This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
The '''OpenSTLinux BSP''' encompasses the following components: | The '''OpenSTLinux BSP''' encompasses the following components: | ||
* The '''boot chain''' based on '''TF-A''' and '''U-Boot''' | * The '''boot chain''' based on '''TF-A''' and '''U-Boot''' | ||
Line 13: | Line 6: | ||
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.<br> | The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.<br> | ||
[[File: OpenSTLinux architecture overview.png|link=OpenSTLinux architecture overview|thumb|Zoom out to OpenSTLinux distribution]] | [[File: OpenSTLinux architecture overview.png|link=OpenSTLinux architecture overview|thumb|Zoom out to OpenSTLinux distribution]] | ||
{{ImageMap|Image:OpenSTLinux_BSP_SW_Overview.png{{!}} frame {{!}} center {{!}} OpenSTLinux BSP architecture overview | {{ImageMap|Image:OpenSTLinux_BSP_SW_Overview.png{{!}} frame {{!}} center {{!}} OpenSTLinux BSP architecture overview | ||
rect 16 37 111 95 [[OP-TEE overview]] | rect 16 37 111 95 [[OP-TEE overview]] | ||
rect 119 37 216 95 [[TF-A overview]] | rect 119 37 216 95 [[TF-A overview]] | ||
Line 20: | Line 13: | ||
poly 230 11 334 11 334 98 114 98 114 32 230 32 [[Boot_chains_overview#STM32MP_boot_chains|Boot chains overview]] | poly 230 11 334 11 334 98 114 98 114 32 230 32 [[Boot_chains_overview#STM32MP_boot_chains|Boot chains overview]] | ||
}} | }} | ||
<noinclude> | |||
{{PublicationRequestId | 5965 | 2018-01-25 | AlainF}} | |||
[[Category:Architecture overview|03]] | |||
</noinclude> |
Latest revision as of 11:41, 15 October 2019
The OpenSTLinux BSP encompasses the following components:
- The boot chain based on TF-A and U-Boot
- The OP-TEE secure OS running on the Cortex-A in secure mode
- The Linux kernel running on the Cortex-A in non-secure mode
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.