Registered User |
Registered User No edit summary |
||
(5 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
More information can be found in the detailed release notes referenced later in this article. | More information can be found in the detailed release notes referenced later in this article. | ||
== SW4TM32 - System Workbench for STM32 2. | == SW4TM32 - System Workbench for STM32 2.9.0 - ''STM32-CoPro-MPU plugin''== | ||
The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>®</sup>-M core contained in the STM32MP1 Family. <br> | The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>®</sup>-M core contained in the STM32MP1 Family. <br> | ||
It is included in '''System Workbench for STM32''' from version 2. | It is included in '''System Workbench for STM32''' from version 2.9.0. <br> | ||
It provides:<br> | It provides:<br> | ||
* the target status widget, | * the target status widget, | ||
Line 43: | Line 26: | ||
<onlyinclude> | <onlyinclude> | ||
{| class=" | {| class="st-table" width=98% | ||
|- | |- | ||
! !! IDE for Linux<sup>®</sup> host PC!! IDE for Windows<sup>®</sup> host PC | ! !! style="text-align:center;"|IDE for Linux<sup>®</sup> host PC!!style="text-align:center;"| IDE for Windows<sup>®</sup> host PC | ||
|- | |- | ||
| '''Download''' | | '''Download''' | ||
|| | || | ||
''' | '''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 ''' | ||
*Download the all-in-one Linux installer 2. | *Download the all-in-one Linux installer 2.9 '''install_sw4stm32_linux_64bits-v2.9.run''' from [http://www.openstm32.org/HomePage openstm32.org] | ||
|| | || | ||
''' | '''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 ''' | ||
*Download the all-in-one Windows installer 2. | *Download the all-in-one Windows installer 2.9 '''install_sw4stm32_win_64bits-v2.9.exe''' from [http://www.openstm32.org/HomePage openstm32.org] | ||
|- | |- | ||
| '''Installation''' | | '''Installation''' | ||
|| | || | ||
* Run the installation script | * Run the installation script | ||
$ chmod +x install_sw4stm32_linux_64bits-v2. | $ chmod +x install_sw4stm32_linux_64bits-v2.9.run | ||
$ ./install_sw4stm32_linux_64bits-v2. | $ ./install_sw4stm32_linux_64bits-v2.9.run | ||
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org] | *Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org] | ||
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. | * '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. | ||
|| | || | ||
* Run the installation exe | * Run the installation exe | ||
$ install_sw4stm32_win_64bits-v2. | $ install_sw4stm32_win_64bits-v2.9.exe | ||
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org] | *Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org] | ||
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. | * '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. | ||
Line 76: | Line 59: | ||
<noinclude> | <noinclude> | ||
{{PublicationRequestId | 8349 | 2018-08-14 | AlainF}} | |||
[[Category:Release notes|5]] | |||
[[Category:SW4STM32 IDE]] | |||
{{UpdateNeededForNewRelease| | |||
* Copy the current release (first chapter) in the "Archives" chapter | |||
* Change the version of the tool | |||
* Change the name of the archive file | |||
* Change the download URLs | |||
}} | |||
</noinclude> |
Latest revision as of 15:18, 10 October 2019
More information can be found in the detailed release notes referenced later in this article.
1. SW4TM32 - System Workbench for STM32 2.9.0 - STM32-CoPro-MPU plugin[edit source]
The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It is included in System Workbench for STM32 from version 2.9.0.
It provides:
- the target status widget,
- the console management,
- the project creation, compilation and debug in two modes:
- Engineering Mode,
- Production Mode, with Cortex®-M firmware download :
- via Ethernet Network (LAN or Point-to-Point)
- via Ethernet over USB
- the remote system explorer configuration
It is available on Linux® and Windows® platforms.
Upgrading your System Workbench, STM32-CoPro-MPU plugin can be installed using the System Workbench for STM32 - Updates
in menu Windows > Preferences > Install/Update > Available Software Site.
The installation is then the standard Eclipse one: Help > Install New Software...
In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in Windows > Preferences > General > Network Connections; Active Provider set to Manual.
Then after selecting HTTP proxy entry, click Edit... and enter your proxy setup.
IDE for Linux® host PC | IDE for Windows® host PC | |
---|---|---|
Download |
STM32-CoPro-MPU plugin in SW4STM32 2.9.0
|
STM32-CoPro-MPU plugin in SW4STM32 2.9.0
|
Installation |
$ chmod +x install_sw4stm32_linux_64bits-v2.9.run
$ ./install_sw4stm32_linux_64bits-v2.9.run
|
$ install_sw4stm32_win_64bits-v2.9.exe
|
Detailed release notes | Details about the content of this tool version are available on openstm32.org |
Details about the content of this tool version are available on openstm32.org |