This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
Coming soon |
This article explain what is sleep/stop and standby low power mode and provide code examples !
1. Low power mode
By default, the microcontroller is in Run mode after a system or a power-on reset. Several low-power modes are available to save power when the CPU does not need to be kept running, for example when waiting for an external event. It is up to the user to select the mode that gives the best compromise between low-power consumption, short startup time and available wakeup sources. The main three low-power modes:
- Sleep mode (Cortex core stopped, peripherals kept running)
- Stop mode (all clocks are stopped)
- Standby mode (only backup domain is powered)
2. SLEEP Mode
2.1. Definition
2.1.1. Use SLEEP mode with EXTI
2.1.1.1. Objective
- We use the EXTI setup from EXTI_overview
- Learn how to setup SLEEP in HAL
- Create simple project with SLEEP mode with wake up on pin press
2.1.1.2. Goal
- Use project from EXTI_overview
- Learn how to setup the SLEEP in HAL, and which events can wake up MCU
- Verify the correct functionality by measuring consumption
2.1.1.3. HAL Library workflow summary
2.1.1.4. Open the project from EXTI_overview
- Open the main.c
- Add function suspend the Systick ( as we wakeup on any interrupt)
- Add function to enter in SLEEP mode
- Add function to resume the Systick on wakeup
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_SuspendTick();
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON,PWR_SLEEPENTRY_WFI);
HAL_ResumeTick();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
2.1.1.5. Compile and flash
2.1.1.6. Measure consumption
- Stop any debug session and do a full power cycle
- Use an ampermeter on IDD connector (JP5 on NucleoF429ZI, for other board check User Manual)
- Check consumption while in SLEEP mode
- Press the button of the Nucleo, you can see the consumption variation
3. STOP Mode
3.1. Definition
3.1.1. Use STOP mode with EXTI
3.1.1.1. Objective
- We use the EXTI setup from EXTI_overview
- Learn how to setup STOP in HAL
- Create simple project with STOP mode with wake up on pin press
3.1.1.2. Goal
- Use project from EXTI_overview
- Learn how to setup the STOP in HAL, and which events can wake up MCU
- Verify the correct functionality by measuring consumption
3.1.1.3. HAL Library workflow summary
3.1.1.4. Open the project from EXTI_overview
- Open the main.c
- Add function to enter in STOP mode
- Reconfiguration of the clocking
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_SuspendTick();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFI);
SystemClock_Config();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
3.1.1.5. Compile and flash
3.1.1.6. Measure consumption
- Stop any debug session and do a full power cycle
- Use an ampermeter on IDD connector (JP5 on NucleoF429ZI, for other board check User Manual)
- Check consumption while in STOP mode
- Press the button of the Nucleo, you can see the consumption variation
4. STANBY Mode
4.1. Definition
4.1.1. Use STANBY mode
4.1.1.1. Objective
- For this lab create CubeMX project
- For testing purpose enable LED PG14 on NucleoF429ZI(for other board check User Manual)
- Learn how to setup STANDBY in HAL
- Create simple project with STANDBY mode with wake up on pin
4.1.1.2. Goal
- Learn how to setup the STANDBY in HAL, which events can wake up you
- Verify the correct functionality by measuring consumption
4.1.1.3. HAL Library workflow summary
4.1.1.4. Open the project from EXTI_overview
- Open the main.c
- Add the clear of the wakeup flag ( without it, you will go in StandBy only once)
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
_HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* USER CODE END 2 */
- Light on the LED
- Wait 2 second
- Enable the wakeup pin ( which is PA0 and connected to the blue button on NucleoF429ZI)
- Add function to enter in STANDBY mode
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_14);
HAL_Delay(2000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_PWR_EnterSTANDBYMode();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
4.1.1.5. Compile and flash
4.1.1.6. Measure consumption
- Stop any debug session and do a full power cycle
- Use an ampermeter on IDD connector (JP5 on NucleoF429ZI, for other board check User Manual)
- Check consumption while in STANDBY mode
- Press the button of the Nucleo, you can see the consumption variation