This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:=:
Displayed 100 items.
- Strace (transclusion) (← links)
- Netstat (transclusion) (← links)
- Perf (transclusion) (← links)
- Sysstat tool suite (transclusion) (← links)
- LTTng (transclusion) (← links)
- Menuconfig or how to configure kernel (transclusion) (← links)
- Ftrace (transclusion) (← links)
- CAN overview (transclusion) (← links)
- Crypto API overview (transclusion) (← links)
- CEC overview (transclusion) (← links)
- U-Boot overview (transclusion) (← links)
- How to debug Weston (transclusion) (← links)
- How to launch Khronos OpenGLES conformance tests (transclusion) (← links)
- How to launch glmark2 benchmark (transclusion) (← links)
- Serial TTY overview (transclusion) (← links)
- How to use TTY with User Terminal (transclusion) (← links)
- Pinctrl overview (transclusion) (← links)
- GPIOLib overview (transclusion) (← links)
- How to control a GPIO in userspace (transclusion) (← links)
- How to control a GPIO in kernel space (transclusion) (← links)
- STM32MP15 V4L2 camera overview (transclusion) (← links)
- STM32MP15 Evaluation boards - starting for the first time (transclusion) (← links)
- STM32MP15 Evaluation boards - required material (transclusion) (← links)
- STM32CubeProgrammer (transclusion) (← links)
- How to use the kernel dynamic debug (transclusion) (← links)
- Watchdog overview (transclusion) (← links)
- Regulator overview (transclusion) (← links)
- PWM overview (transclusion) (← links)
- U-Boot - How to debug (transclusion) (← links)
- STM32MP15 U-Boot (transclusion) (← links)
- Pseudo filesystem (transclusion) (← links)
- How to populate the SD card with dd command (transclusion) (← links)
- How to cross-compile with the Developer Package (transclusion) (← links)
- STM32MP157x-EV1 - board connections (transclusion) (← links)
- STM32MP157x-EV1 - board assembly (transclusion) (← links)
- STM32MP157x-EV1 - hardware description (transclusion) (← links)
- How to configure TF-A BL2 (transclusion) (← links)
- How to create an SDK for OpenSTLinux distribution (transclusion) (← links)
- How to debug TF-A BL2 (transclusion) (← links)
- Weston keyboard shortcuts (transclusion) (← links)
- Power overview (transclusion) (← links)
- Clock overview (transclusion) (← links)
- How to transfer a file over serial console (transclusion) (← links)
- STM32CubeProgrammer flashlayout (transclusion) (← links)
- Dmesg and Linux kernel log (transclusion) (← links)
- V4l2-ctl (transclusion) (← links)
- How to use USB mass storage in U-Boot (transclusion) (← links)
- Gst-play (transclusion) (← links)
- STM32 MPU OpenSTLinux release note (transclusion) (← links)
- STM32CubeProgrammer release note (transclusion) (← links)
- Example of directory structure for Packages (transclusion) (← links)
- Netdata (transclusion) (← links)
- Gdbgui (transclusion) (← links)
- Gst-typefind (transclusion) (← links)
- STM32MP1 Distribution Package - OpenSTLinux distribution (transclusion) (← links)
- Ethernet overview (transclusion) (← links)
- GDB commands (transclusion) (← links)
- Kmemleak (transclusion) (← links)
- Sysprof (transclusion) (← links)
- Valgrind (transclusion) (← links)
- How to transfer a file over network (transclusion) (← links)
- ADC OpenSTLinux drivers (transclusion) (← links)
- How to find Linux kernel driver associated to a device (transclusion) (← links)
- Gst-discoverer (transclusion) (← links)
- Core dump (transclusion) (← links)
- Trace-cmd and kernelshark trace viewer (transclusion) (← links)
- Subpart - STM32MP1 - Starter Package (transclusion) (← links)
- MB1272 (transclusion) (← links)
- STM32MP157x-DKx - board connections (transclusion) (← links)
- STM32MP15 Discovery kits - starting for the first time (transclusion) (← links)
- STM32MP157x-DKx - board assembly (transclusion) (← links)
- STM32MP157x-DKx - hardware description (transclusion) (← links)
- STM32MP15 Discovery kits - required material (transclusion) (← links)
- How to display on HDMI (transclusion) (← links)
- How to create your own distribution (transclusion) (← links)
- DAC Linux driver (transclusion) (← links)
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- Hardware random overview (transclusion) (← links)
- GStreamer troubleshooting grid (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- How to customize the Linux kernel (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- Ethernet device tree configuration (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to integrate an external software package (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- How to perform ssh connection (transclusion) (← links)
- How to perform ping test (transclusion) (← links)
- Configfs (transclusion) (← links)