![]() |
Coming soon |
1. First Capturing sound and recording it
45min
Target description
This tutorial enables you to:
- Use the embedded STM32F769I-Disco microphones
- Capture the sound got from the microphones
- Expose the complete chaine to filter the sound using the DFSDM functionality
- Record the sound and re-listen to them on the ouptut line of the STM32F769I-Disco using an earphone
Prerequisites
- Computer with Windows 7 (or higher)
Hardware
- STM3232F769IDISCOVERY
- Headphones \ Earphones
Software
- STM32CubeIDE
- STM32CubeMX
Literature
- STM32F769NI MCU User Manual
- STM32 DFSDM
- STM32F769xx Datasheet
Getting started with STM32F769NI discovery kit.
- STM32F769I-DISCO schematics
1.1. Installation of the software tools
In this part, the software we will be working on are STM32CubeIDE and STM32CubeMX.
To follow the installation instructions, please refer to our wiki page Tools installation.
1.2. Launching the project
To create the project, please launch STM32CubeMX, and on the home page, click on Access to board selector
Later, in the search bar write STM32F769 in order to search for the board we will be working with, later choose the STM32F769I-Disc1 as presented in the following image.
1.3. Configuring the board
Now, the next step is to set the right parameters in order to create the first recording and listening to the sound got from the embedded STM32F769I-Disco microphones.
Let's start configuring the DFSDM channels and filters.
In the Channel 1, in the Mode section please set the following parameters :
- input from ch1 and internal clock as entry
- right bit shift 2
- Oversampling 10
- Output clock: Selection audio clock and Divider = 4
In the Channel 0, in the Mode section please set the following parameters :
- Mode : input from ch1 and internal clock
- Right bit shift: 2
- Oversampling: 10
- Type SPI: falling
- Output clock: Selection audio clock and Divider = 4
Now it is time to configure the SAI.
For the SAI configuration, make sure the following parameters are set properly:
- Audio frequency = 44
- Slot size = datasize
- Slot active = user setting: 0&1
2. SecondAnalog App
45min
Target description
Hardware
- STM3232F769IDISCOVERY
- Headphones\Earphones
Literature