![]() |
Coming soon |
1. Characterize your first motor by means of ST Motor Profiler
25min
Target description
This tutorial enables you to use ST Motor Profiler and after applying it you will be able to :
- Connect the motor control pack to your computer.
- Start the motor and monitor its speed.
Prerequisites
- Computer with Windows 7 (or higher)
- ST-Link utility installed
Hardware
- P-Nucleo-IHM03 pack
- Standard-A -to- Mini-B USB cable + power source
Software
- ST Motor Profiler
Literature
- P-Nucleo-IHM03 user manual
- UM2374 STM32 motor control SDK.user manual.
1.1. Install ST Motor Profiler
To install the Motor Profiler, the STM32 Motor Control Software Development Kit should be installed on your computer, using the following link
It will get installed automatically with the MotorControl Workbench while following the installation steps.
1.2. Connect the package to the computer
In this tutorial we will be working the P-NUCLEO-IHM03 Motor Control package and to start our application we should contact our pack to the computer.
After setting up the boards and motor properly, let us launch the Motor Profiler application.
- The first step to do is to select the boards we are using by clicking on Select Boards button
- By referring to the user manual, the following parameters regarding the motor characteristics can be defined: Pole Pairs, Max Speed, Max Current, VBus.
- After defining the values, the next step is to click on “Connect” button and check the motor working correctly.
Please make sure to upgrade the ST-Link version so to not have problems with launching the application.
1.3. Start the test
After finishing the connection between the boards and the computer, it is now the time to start the test.
- Click on Start Profile button.
When clicking, the motor will start rotating in a high speed and the electrical as well as the mechanical models will get established as shown in the following photo.
1.4. Monitor the speed
After checking that the motor is connected and working properly, the next step is to make it work while controlling its speed.
- Click on Play button and the following window appears.
- By moving the cursor, the speed can be monitored
Now you are able to:
- Start your own motor application
- Use properly the ST Motor Control pack
2. Start the motor using ST Motor Control Workbench
45min
Target description
This tutorial enables you to use ST Motor Control Workbench and after applying it you will be able to :
- Connect the motor control pack to your computer.
- Start the motor
Prerequisites
- Computer with Windows 7 (or higher)
- ST-Link utility installed
Hardware
- P-Nucleo-IHM03 pack
- Standard-A -to- Mini-B USB cable + power source
Software
Literature
- P-Nucleo-IHM03 data brief
- UM2374 STM32 motor control SDK.user manual.
2.1. Install Motor Control Workbench
2.2. Start the first application
Since the pack used is the P-Nucleo-IHM03 it is mandatory to select the appropriate boards used.
First step to do so is to click on New Project and to select the NUCLEO-G431RB as control board & X-NUCLEO-IHM16M1 as power board and later click on ok as enumerated in the next photo:
After finishing selecting the pack's boards, another window appears that allows the user to check the details and set the values of the different caracteristics.
It is recommended to check some of the different values and try to use the user manual of the power control as well as the control board in order to understand them.
Later, just click on the generate file button presented in the photo below, and save the project in the appropriate directory.
Then a window that allows to choose the IDE to use, and the drive type appears. Just click on Generate and after the software finishes generating the .ioc file click on Run STM32CubeMX.
The .ioc file is open now and the next step is to simply generate the code in the STM32CubeIDE.
Once STM32CubeIDE is generated, before generating the code, do not forget to update the project information in the Project Manager section.