Build an IOT system30min
Target description
This tutorial shows how to program and use the Bluetooth interface to perform data communication between the STM32L4 Discovery kit IoT node (B-L475E-IOT01A) and an Android application running on a mobile device.
After this tutorial, you will be able to build an IoT system, control it from your mobile monitoring sensors and collect data.
Prerequisites
You have gone through:
Hardware
- STM32L4 Discovery kit IoT node (B-L475E-IOT01A )
- USB cable Type-A to Mini-B
Literature
- UM2153 Discovery kit for IoT node, multi-channel communication with STM32L4
- UM1873 Getting started with the X-CUBE-BLE1 Bluetooth® Low Energy software expansion for STM32Cube4
Getting starting with STM32L4 Discovery kit IoT node
The purpose of this section is to explain step-by-step how to reuse one of the applications that are part of the STM32CubeL4 MCU package to create a communication channel between the IoT board emulating a heart rate monitor and a mobile device on which the data is displayed via an Android application.
1. Import and convert the HeartRate project from the STM32Cube package
- In STM32CubeIDE, import the HeartRate example located in: C:\Users\user_name\STM32Cube\Repository\STM32Cube_FW_L4_Vx.xx.x\Projects\B-L475E-IOT01A\Applications\BLE\HeartRate
- The project must be converted and the following message is displayed:
- Click on OK and a new message confirms the success of the conversion
- Click on OK and the STM32CubeIDE workspace opens
2. Build and execute the HeartRate Project
- Select the STM32L4_IOT_HR project
- Click on the Build button
to rebuild the project.
- Click on the Debug button
arrow and select Debug Configurations… and make sure the Debug probe parameter is set to ST-LINK. Otherwise the code is not properly downloaded on the board.
- Click on the Debug button
to run the software.
- STM32CubeIDE opens the Debug perspective. Click on the Resume button
to execute the code.
3. Install the Android application on a mobile device
To interact with the IoT board, an Android application has to be installed on a mobile device.
The STM32 BLE Profile application is a companion tool to show in a human readable form all notifications coming from Bluetooth Low Energy (BLE) devices implementing some peripheral profiles.
4. Connect to the IoT node
- Go to Google Play store and install the “STM32 BLE Profiles” application on your mobile device.
- Once installed, simply launch the STM32 BLE Profiles application. The application scans the network and displays a list of discovered BLE devices (Here the HeartRateSensor device).
- Establish a Bluetooth connection with the B-L475E-IOT1A board selecting the HR_L475_IoT device from the discovered devices list. It can take a while to get the connection established.
- The following screenshot shows the successful pairing with a health thermometer sensor:
- Once connected, select the Heart Rate profile among the BLE profiles proposed.
The application starts to display the heart rate data sent by the IoT connected device, which acts as a peripheral. In this example, the data is generated on the B-L475E-IOT1A board via a formula and does not reflect the data from a real sensor.
Now you are able to:
- Build your own IoT system to get values from a peripheral device and display them on your mobile device
- Regenerate a project from one of the various applications available in the STM32Cube package.