This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Coming soon |
This article explain what is sleep/stop and standby low power mode and provide code examples !
1. Low power mode
By default, the microcontroller is in Run mode after a system or a power-on reset. Several low-power modes are available to save power when the CPU does not need to be kept running, for example when waiting for an external event. It is up to the user to select the mode that gives the best compromise between low-power consumption, short startup time and available wakeup sources. The main three low-power modes:
- Sleep mode (Cortex core stopped, peripherals kept running)
- Stop mode (all clocks are stopped)
- Standby mode (only backup domain is powered)
2. SLEEP Mode
2.1. Definition
2.1.1. Use SLEEP mode with EXTI
2.1.1.1. Objective
- We use the EXTI setup from EXTI_overview
- Learn how to setup SLEEP in HAL
- Create simple project with SLEEP mode with wake up on pin press
2.1.1.2. Goal
- Use project from EXTI_overview
- Learn how to setup the SLEEP in HAL, and which events can wake up MCU
- Verify the correct functionality by measuring consumption
2.1.1.3. HAL Library workflow summary
2.1.1.4. Open the project from EXTI_overview
- Open the main.c
- Add the function to enter in SLEEP mode