Getting started with WDG

Revision as of 15:19, 21 December 2022 by Registered User
Under construction.png Coming soon

This article explains what WDOG is and how to use it through examples

1. What is watchdog (WDOG)

WDOG stands for Watch DOG. The main goal of this IP is to detect and resolve malfunctions due to software failures. The principle is to periodically refresh the WDG (or pet the dog), if the counter isn't refreshed, a system reset is generated. Also, the WDG acts as a protection since it avoids to stay stuck in a particular stage of processing. The configuration using option bytes can launch the WDG by hardware or software. Once started, it cannot be disabled.

Info white.png Information
The WDG (or the dog) needs to be refreshed (pet) or the system will be reset (bark)

2. WDOG type

There are two types of WDOG :

  • WWDG : Window watchdog
  • IWDG : Independent watchdog

2.1. WWDG : Window watchdog

2.1.1. Definition

The window watchdog is based on a 7-bit downcounter that can be set as free running. It can be used as a watchdog to reset the device when a problem occurs. It is clocked from the main clock. It has an early warning interrupt capability and the counter can be frozen in debug mode.

2.1.2. Application benefits

  • Best suited for applications which require the watchdog to react within an accurate time window.
  • Configurable time-window thanks to the prescaler value (For example, the STM32L476xx have a programmable timeout range from 51.2 us to 28.2ms)
  • Selectable hardware or software start
  • Early Wakeup Interrupt (EWI) available before reset happens

2.1.3. How does it work ?

The diagram below illustrates how the WWDG operates. If the downcounter is reloaded too early or too late, the window watchdog will initiate a reset.

WWDG Refresh.png

As we can see on the following block diagram, the counter value and the window value are compared in order to evaluate the time to refresh the downcounter in the configurable window.

WWDG.png

2.2. IWDG : Independent WatchDoG

2.2.1. Definition

The independent watchdog is based on a 12-bit downcounter and 8-bit prescaler. It is clocked from an independent 32 kHz internal RC (LSI) and as it operates independently from the main clock, it can operate in Stop and Standby modes. It can be used either as a watchdog to reset the device when a problem occurs, or as a free running timer for application timeout management. It is hardware or software configurable through the option bytes. The counter can be frozen in debug mode.

2.2.2. Application benefits

  • Totally independent process outside the main application
  • Configurable timeout period thanks to the prescaler value (For example, the STM32L476xx have a programmable timeout range from 125us to 32.7s)
  • Selectable hardware or software start
  • Selectable low-power freeze in Standbye or Stop modes

2.2.3. How does it work ?

The IWDG architecture is represented below : IWDG.png

As we can see on the block diagram above, IWDG registers are located in the CORE voltage domain while its functions are in the VDD voltage domain. The 8-bit prescaler is used to divide the LSI oscillator frequency. When the IWDG is started, the 12-bit counter starts counting down from the reset value of 0xFFF. To refresh the IWDG counter, the Key value (0xAAAA) must be written in the Key register to reload the counter value. If the downcounter reaches the end of the count value (0x000), a system reset is generated.

Info white.png Information
Additional options such as custom reload value and time window might be available

3. Configure WWDOG with LED indication

3.1. Objective

  • In this project, you will learn how to setup WWDG in STM32CubeIDE
  • How to Generate Code in STM32CubeIDE and use HAL functions
  • Create a simple application to test WWDG

3.2. How

  • Configure WWDG in STM32CubeIDE and Generate Code
  • Learn how to activate and refresh WWDG
  • Add into the project the HAL_Delay function and HAL_GPIO_Toggle function
  • Verify the correct functionality on toggling LED

3.3. Create the project in STM32ubeIDE

File > New > STM32 Project in main panel.
create STM32CubeIDE project.png

In this example the NUCLEO-L476RG board is used.

  • Select NUCLEO-L476RG in board Selector.

Select NUCLEO-L476RG board.png

  • Save the project.

WWDG name.png

3.4. GPIO Configuration

  • In the Pinout & Configuration window, select GPIO and define PA5 as a GPIO_Output
  • Keep the same configuration as following
    • Low
    • Output Push Pull
    • No pull-up and pull-down
    • Low
    • LD2

GPIO Config.png

LedPinGPIO.png LED UM GPIO.png

Info white.png Information
The user label is defined to have a more meaningful name
Info white.png Information
For more information on GPIO, please refer to the Getting started with GPIO page

3.5. WWDG Configuration

  • In the same window, select WWDG and click on Activated
  • Then go to Parameter Settings, and enter the following configuration

WWDG param.png

Info white.png Information
Refer to the 2.1 chapter WWDG : Window watchdog for more information on the parameters

3.6. Clock Configuration

  • In the Clock Configuration window, in the HCLK box, enter the maximum value for frequency : 80MHz

CLK Config.png

3.7. Set the project details for generation

The easiest way to generate the code is to save your current project : Ctrl + S
The code is generated so you can see it in the left side of the screen in the project explorer

File tree GPIO.png

3.8. Open the main.c in our IDE

Now, open the main.c file which is the main source file for this application

  • The LED toggling is done with a HAL function inside main.c
Info white.png Information
Between /* USER CODE BEGIN 3 */ and /* USER CODE END 3 */ tags
  • You can calculate the delay with this formula:

Formula.png

Info white.png Information
Try other delays such as 10 or 30 and then conclude
 /* USER CODE BEGIN 3 */
  /* Infinite loop */
  {
    HAL_Delay(20);  // because (1/80000000)*4096*8*(127-80+1)) ~ 20ms
    HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
    if (HAL_WWDG_Refresh(&hwwdg) != HAL_OK)
    {
        Error_Handler();
    }
  }
  /* USER CODE END 3 */
Info white.png Information
Make sure to keep User Code when re-generating !

Code genreation panel.png

3.9. Compile and flash

  • Click on Build button Built.png
  • Click on Debug button (to run step by step) Debug.png
  • Or on Run button (to execute) Run.png

Every 500 ms the green LED state changes.

Warning white.png Warning
All GPIOs are able to drive 5 V and 3.3 V in input mode, but they are only able to generate 3.3V in output push-pull mode

ST10543 NUCLEO L476RG top D2Blink.png

4. Configure IWDOG with LED indication

4.1. Objective

  • In this project, you will learn how to setup IWDG in STM32CubeIDE
  • How to Generate Code in STM32CubeIDE and use HAL functions
  • Create a simple application to test IWDG

4.2. How

  • Configure IWDG in STM32CubeIDE and Generate Code
  • Learn how to activate and refresh IWDG
  • Add into the project the HAL_Delay function and HAL_GPIO_Toggle function
  • Verify the correct functionality on toggling LED

4.3. Create the project in CSTM32ubeIDE

File > New > STM32 Project in main panel.
create STM32CubeIDE project.png

In this example the NUCLEO-L476RG board is used.

  • Select NUCLEO-L476RG in board Selector.

Select NUCLEO-L476RG board.png

  • Save the project.

IWDG name.png

4.4. GPIO Configuration

  • In the Pinout & Configuration window, select GPIO and define PA5 as a GPIO_Output
  • Keep the same configuration as following
    • Low
    • Output Push Pull
    • No pull-up and pull-down
    • Low
    • LD2

GPIO Config.png

LedPinGPIO.png LED UM GPIO.png

Info white.png Information
The user label is defined to have a more meaningful name
Info white.png Information
For more information on GPIO, please refer to the Getting started with GPIO page

4.5. IWDG Configuration

  • In the same window, select IWDG and click on Activated
  • Then go to Parameter Settings, and enter the following configuration

IWDG Param.png

Info white.png Information
Refer to the 2.2 chapter IWDG : Independant WatchDoG for more information on the parameters

4.6. Set the project details for generation

The easiest way to generate the code is to save your current project : Ctrl + S
The code is generated so you can see it in the left side of the screen in the project explorer

IWDG Toggle.png

4.7. Open the main.c in our IDE

Now, open the main.c file which is the main source file for this application

  • The LED toggling is done with a HAL function inside main.c
Info white.png Information
Between /* USER CODE BEGIN 3 */ and /* USER CODE END 3 */ tags
Info white.png Information
Try other delays such as 50, 200 or 450 and then conclude
 /* USER CODE BEGIN 3 */
  /* Infinite loop */
  {
	HAL_Delay(300);  // because (1/32000)*128*100 so max ~400ms
	HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
	if (HAL_IWDG_Refresh(&hiwdg) != HAL_OK)
	{
		Error_Handler();
	}
  }
  /* USER CODE END 3 */
Info white.png Information
Make sure to keep User Code when re-generating !

Code genreation panel.png

4.8. Compile and flash

  • Click on Build button Built.png
  • Click on Debug button (to run step by step) Debug.png
  • Or on Run button (to execute) Run.png

Every 500 ms the green LED state changes.

Warning white.png Warning
All GPIOs are able to drive 5 V and 3.3 V in input mode, but they are only able to generate 3.3V in output push-pull mode

ST10543 NUCLEO L476RG top D2Blink.png



[[category:Getting_started_with_STM32_system_peripherals | 60]]