This article explains Sleep, Stop, Standby and Low-power modes, and provides code examples.
1. Low-power modes Introduction
By default, the microcontroller is in Run mode after a system or power reset. Several low-power modes are available to save power when the CPU does not need to be kept running, for example when waiting for an external event. It is up to the user to select the mode that gives the best compromise between low-power consumption, short startup time and available wakeup sources.
The ultra-low-power STM32L476xx supports 7 low-power modes to achieve the best compromise between low-power consumption, short startup time, available peripherals and available wakeup sources.
- Sleep mode
- Low power run mode
- Low power sleep mode
- Stop 0, Stop1, Stop2 modes
- Standby mode
- Shutdown mode
2. Sleep mode
2.1. Definition
In sleep mode, the CPU clocks are OFF and there is no effect on other clocks or analog clock sources. All peripherals continue to operate and can wake up the CPU when an interrupt/event occurs
2.1.1. Using Sleep mode with EXTI
2.1.1.1. Objective
- Learn how to set up Sleep mode in the HAL
- Create a simple project with Sleep mode and wakeup when a button (configured in the EXTI setup) is pressed.
- Verify the correct functionality by measuring the current consumption.
2.1.1.2. How
- Use the project from EXTI overview
2.1.1.3. HAL library workflow summary
Besides the APIs, HAL peripheral drivers include:
• HAL_PPP_IRQHandler() peripheral interrupt handler that should be called from stm32l4xx_it.c
• User callback functions.
After using the WFI and entering Stop0, Stop1 or Stop 2 mode, the code in the handler will be executed
2.1.1.4. Open the project from EXTI overview
- Open main.c
- Add a function to suspend the Systick (as we wakeup on any interrupt)
- Add a function to enter Sleep mode
- Add a function to resume the Systick on wakeup.
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_SuspendTick();
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON,PWR_SLEEPENTRY_WFI);
HAL_ResumeTick();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
2.1.1.5. Compile and flash
Compile the above code, then load it to the board flash memory.
2.1.1.6. Measure consumption
- Stop any debug session and do a full-power cycle
- Use an ammeter on the IDD connector (JP5 on NucleoF429ZI - for other boards check their user manual)
- Check the consumption while in Sleep mode
- Press the configured button on the Nucleo board to see the current consumption variation.
3. Stop0, Stop1 and Stop2 modes
3.1. Definition
Stop mode achieves the lowest power consumption while retaining the content oSRAM and registers. All clocks in the VCORE domain are stopped, the PLL, the MSI RC, the HSI16 RC and the HSE crystal oscillators are disabled. The LSE or LSI can be kept running. File:Stop mode.jpg
3.1.1. Use Stop modes with EXTI
3.1.1.1. Objective
- Create a simple project with Stop modes with wakeup when a button (configured in the EXTI setup) is pressed.
- Verify the correct functionality by measuring the current consumption.
3.1.1.2. How
- Use the project from EXTI overview
3.1.1.3. HAL library workflow summary
Besides the APIs, HAL peripheral drivers include: • HAL_PPP_IRQHandler() peripheral interrupt handler that should be called from stm32l4xx_it.c • User callback functions. When using WFI and entering Stop0, Stop1 and Stop2, the code in the Handler will be executed. File:Stop HAL.png
3.1.1.4. Open the project from EXTI overview
- Open main.c
- Add a function to enter Stop mode
- Reconfiguration of the clocking
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_SuspendTick();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFI);
SystemClock_Config();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
3.1.1.5. Compile and flash
Compile the above code, then load it to the board flash memory.
3.1.1.6. Measure consumption
- Stop any debug session and do a full-power cycle
- Use an ammeter on the IDD connector (JP5 on NucleoF429ZI - for other boards check their user manual)
- Check the current consumption while in Stop mode
- Press the configured button on the Nucleo board to see the consumption variation.
4. Standby mode
4.1. Definition
4.1.1. Use Standby mode
4.1.1.1. Objective
- For this lab, create an STM32CubeMX project
- For testing purposes, enable LED PG14 on the NucleoF429ZI (for other boards check their user manual)
- Learn how to set up Standby mode in the HAL
- Create a simple project with Standby mode and wakeup when the associated button is pressed.
4.1.1.2. Goals
- Learn how to set up Standby mode in the HAL, and which events can wake up you
- Verify the correct functionality by measuring the current consumption.
4.1.1.3. HAL library workflow summary
4.1.1.4. Open the project from EXTI overview
- Open main.c
- Add the wakeup flag clear (without this, Standby mode is only entered once)
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* USER CODE END 2 */
- Turn on the LED
- Wait 2 seconds
- Enable the wakeup pin (which is PA0 and is connected to the blue button on the NucleoF429ZI)
- Add a function to enter Standby mode.
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_14);
HAL_Delay(2000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_PWR_EnterSTANDBYMode();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
4.1.1.5. Compile and flash
Compile the above code, then load it to the board flash memory.
4.1.1.6. Measure consumption
- Stop any debug session and do a full-power cycle
- Use an ammeter on the IDD connector (JP5 on NucleoF429ZI - for other boards check their user manual)
- Check the current consumption while in Standby mode
- Press the blue Nucleo button to see the consumption variation.
5. Useful power monitoring tool
A dedicated tool exists for power consumption measurement : STM32CubeMonPwr