Getting started with WDG

Revision as of 12:24, 15 November 2022 by Registered User
Under construction.png Coming soon

This article explains what WDOG is and how to use it through examples

1. Introduction of WDOG

WDOG stands for Watch DOG. The main goal of this IP is to detect and resolve malfunctions due to software failures. The principle is to refresh periodically the WDG, if the timer isn't refreshed, a system reset is generated. Also, the WDG act as a protection because it avoid to stay stuck in a particular stage of processing that it performs. The configuration using option bytes can launch the WDG by hardware or software. Once start, it cannot be disabled.

2. WDOG type

There are two types of WDOG :

2.1. WWDG : Window WatchDoG

The window watchdog is based on a 7-bit downcounter that can be set as free running. It can be used as a watchdog to reset the device when a problem occurs. It is clocked from the main clock. It has an early warning interrupt capability and the counter can be frozen in debug mode.

Application benefits :

  • Best suited for applications which require the watchdog to react within an accurate time window.
  • Configurable time-window
  • Selectable hardware or software start
  • Early Wakeup Interrupt (EWI) available before reset happens

2.2. IWDG : Independent WatchDoG

The independent watchdog is based on a 12-bit downcounter and 8-bit prescaler. It is clocked from an independent 32 kHz internal RC (LSI) and as it operates independently from the main clock, it can operate in Stop and Standby modes. It can be used either as a watchdog to reset the device when a problem occurs, or as a free running timer for application timeout management. It is hardware or software configurable through the option bytes. The counter can be frozen in debug mode.

Application benefits :

  • Totally Independent process outside the main application
  • Selectable hardware or software start
  • Selectable low-power freeze in Standbye or Stop modes

3. Configure WWDOG with LED indication

3.1. Definition

3.2. Objective

  • In this project, you will learn how to setup WWDG in STM32CubeIDE
  • How to Generate Code in STM32CubeIDE and use HAL functions
  • Create simple application to test WWDG

3.3. How

  • Configure WWDG in STM32CubeIDE and Generate Code
  • Learn how to activate and refresh WWDG
  • Add into the project the HAL_Delay function and HAL_GPIO_Toggle function
  • Verify the correct functionality on toggling LED

3.4. Create the project in CSTM32ubeIDE

4. Configure IWDOG with LED indication

4.1. Objective

  • In this project, you will learn how to setup IWDG in STM32CubeIDE
  • How to Generate Code in STM32CubeIDE and use HAL functions
  • Create simple application to test IWDG

4.2. How

  • Configure IWDG in STM32CubeIDE and Generate Code
  • Learn how to activate and refresh IWDG
  • Add into the project the HAL_Delay function and HAL_GPIO_Toggle function
  • Verify the correct functionality on toggling LED

4.3. Create the project in CSTM32ubeIDE

5. Conclusion

Keep in mind this :



[[category:Getting_started_with_STM32_system_peripherals | 15]]