Getting started with I2C

Revision as of 10:37, 20 October 2022 by Registered User (→‎=STM32 I2C Mode selectio)

This article explains what is the I2C and how to use it through examples


Objectives
Following this tutorial, you will:

  • Get familiar with the STM32L476RG Nucleo board,
  • Learn how to program and use a I2C

Hardware
The hardware requirements to start the application are the following:

  • 2 boards STM32L476RG [1]


1. I2C

I²C (Inter-Integrated Circuit) is a two-wire serial communication system used between integrated circuits which was originally created by Philips Semiconductors back in 1982.
The I2C is a multi-master, multi-slave, synchronous, bidirectional, half-duplex serial communication bus.

1.1. I2C Overview

  • SDA (Serial Data) is the line where master and slave send or receive the information (sequence of bit).
  • SCL (Serial Clock) is the line dedicated to the clock to synchronize the data flow.

i2c buq.png
SDA and SCL lines need to be pulled up with resistors. The value of these resistors depends on the bus length (the bus capacitance) and the transmission speed. The common value is 4.7kO. In any case, there are many guides to size them and we refer their reading to the more attentive reader.

1.2. I2C Modes

  • Standard-Mode (Sm) with a bit rate up to 100 kbit/s
  • Fast-Mode (Fm) with a bit rate up to 400 kbit/s
  • Fast-Mode Plus (Fm+) with a bit rate up to 1 Mbit/s

1.3. I2C Frame

i2c trame.png
-Start Condition (S)
-Stop Condition (P)
-Repeated Start (Restart) Condition (Sr)
-Acknowledge ACK (A)
-Not Acknowledge NACK (/A)

2. STM32 I2C Mode selectio

The interface can operate in one of the four following modes:

  • Slave transmitter
  • Slave receiver
  • Master transmitter
  • Master receiver

I2C in STM32 can be done in 3 methods.
1. Blocking Mode 2. Interrupt Mode 3. DMA Mode

- Blocking mode : The communication is performed in the polling mode.

           The status of all data processing is returned by the same function
           after finishing transfer.br>

- No-Blocking mode : The communication is performed using Interrupts

           or DMA. These functions return the status of the transfer startup.
           The end of the data processing will be indicated through the
           dedicated I2C IRQ when using Interrupt mode or the DMA IRQ when
           using DMA mode.

3. Create the project in STM32CubeMX


[[category:Getting_started_with_STM32_system_peripherals | 15]]

No categories assignedEdit