Revision as of 17:54, 18 September 2020 by Registered User
Under construction.png Coming soon

Target description

  • This tutorial's first part enables you to:
    • Use the embedded STM32F769I-Disco microphones
    • Capture the sound got from the microphones
    • Expose the complete chaine to filter the sound using the DFSDM functionality
    • Record the sound and re-listen to them on the ouptut line of the STM32F769I-Disco using an earphone
  • This tutorial's second part enables you to:
    • Apply the cross correlation algorithm in order to estimate the direction of the sound

Prerequisites

  • Computer with Windows 7 (or higher)

Hardware

Software

Literature

1. First Capturing sound and recording it

Clock.png 45min

1.1. Installation of the software tools

In this part, the software we will be working on are STM32CubeIDE and STM32CubeMX.
To follow the installation instructions, please refer to our wiki page Tools installation.

1.2. Launching the project

To create the project, please launch STM32CubeMX, and on the home page, click on Access to board selector
anacubemx.png
Later, in the search bar write STM32F769 in order to search for the board we will be working with, later choose the STM32F769I-Disc1 as presented in the following image.
anaselect.png

1.3. Configuring the board

Now, the next step is to set the right parameters in order to create the first recording and listening to the sound got from the embedded STM32F769I-Disco microphones.
Let's start configuring the DFSDM channels and filters.

Info white.png Information
DFSDM is Digital Filter for Sigma-Delta Modulators that performs a digital signal processing from external data, in our tutorial, it is the external data detected by the microphones.

For the Channel 1, please set the following parameters :

  • Mode: Input from ch1 and internal clock as entry
  • Channel 1 parameters:
    • Right bit shift: 2
  • Analog watchdog parameters:
    • Oversampling 10
  • Output clock:
    • Selection : Source for output clock is audio clock
    • Divider = 4

For the Channel 0, please set the following parameters :

  • Mode : input from CH0 and Internal Clock
  • Channel 0 parameters:
    • Type SPI with falling edge
    • SPI Clock: Internal SPI clock
    • Right bit shift: 2
  • Analog watchdog parameters:
    • Oversampling: 10
  • Output clock:
    • Selection : audio clock
    • Divider = 4

dfsdm.png
Later, let's configure the filters used.
For the filter 0, please set the following parameters:

  • Regular channel selection:
    • Regular channel section: Channel1
    • Trigger to start regular conversion: Software trigger
    • Fast mode: Enable
  • Injected channel selection:
    • Channel1 as injected channel: Enable
    • Trigger to start injected conversion: Software trigger
  • Filter parameters:
    • Sinc Order: Sinc 3 filter type
    • Fosr: 64

For the filter 1, please set the following parameters:

  • Regular channel selection:
    • Regular channel section: Channel1
    • Trigger to start regular conversion: Synchronous with DFSDM0
    • Fast mode: Enable
  • Injected channel selection:
    • Channel0 as injected channel: Enable
    • Trigger to start injected conversion: Software trigger
    • Scan Mode: Enable
  • Filter parameters:
    • Sinc Order: Sinc 3 filter type
    • Fosr: 64

Now it is time to configure the SAI.

Info white.png Information
SAI is Serial Audio Interface that provides an interface allowing the microcontroller to communicate with external audio devices such as amplifiers, ADCs, DACs, or audio processors.

For the SAI configuration, make sure the following parameters are set properly:

  • Audio frequency = 44
  • Slot size = datasize
  • Slot active = user setting: 0&1

sai.png

Now go to the project manager, rename the application, choose STM32CubeIDE as toolchain and click on generate code.

Once launching the project, follow these steps in order to create the application:

  • Create a new folder in the project's directory in the Drivers folder and name it BSP.
  • From the Cube Package F7 downloaded from STM32CubeMX, copy the Components folder placed in the directory: C:\Users\UserName\STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Drivers\BSP and paste it in the BSP folder in the project's directory.
  • Create a new folder in the BSP one named STM32F769I-Discovery and copy the two files : stm32f769i_discovery.c and its header file stm32f769i_discovery.h from the directory: C:\Users\UserName\STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Drivers\BSP\STM32F769I-Discovery and place them in the STM32F769I-Discovery folder.
  • From Project menu or File menu, go to Properties > C/C++ Build > Settings > Tool Settings > MCU GCC Compiler > Include paths

options1.png

  • Add the following includes as presented in the following photo :

include.png

  • In the main.h file add the following includes:
#include "stm32f7xx_hal.h"
#include "stm32f769i_discovery.h"
#include "../Components/Common/audio.h"
#include "../Components/wm8994/wm8994.h"

In the main.c file add the following declarations:

#define SaturaLH(N, L, H) (((N)<(L))?(L):(((N)>(H))?(H):(N)))

int32_t                      LeftRecBuff[2048];
int32_t                      RightRecBuff[2048];
int16_t                      PlayBuff[4096];
uint32_t                     DmaLeftRecHalfBuffCplt  = 0;
uint32_t                     DmaLeftRecBuffCplt      = 0;
uint32_t                     DmaRightRecHalfBuffCplt = 0;
uint32_t                     DmaRightRecBuffCplt     = 0;
uint32_t                     PlaybackStarted         = 0;
AUDIO_DrvTypeDef            *audio_drv;
  • Add the following function code:
void HAL_DFSDM_FilterRegConvHalfCpltCallback(DFSDM_Filter_HandleTypeDef *hdfsdm_filter)
{
  if(hdfsdm_filter == &hdfsdm1_filter0)
  {
    DmaLeftRecHalfBuffCplt = 1;
  }
  else
  {
    DmaRightRecHalfBuffCplt = 1;
  }
}

In the initialization function of the SAI, add the following code that reads the signal from the microphone device; WM899, initialize audio driver */

 if(WM8994_ID != wm8994_drv.ReadID(AUDIO_I2C_ADDRESS))
    {
      Error_Handler();
    }

    audio_drv = &wm8994_drv;
    audio_drv->Reset(AUDIO_I2C_ADDRESS);
    if(0 != audio_drv->Init(AUDIO_I2C_ADDRESS, OUTPUT_DEVICE_HEADPHONE, 100, AUDIO_FREQUENCY_22K))
    {
      Error_Handler();
    }
  • After declaring i as uint32_t, in the While loop, add the following code:
if((DmaLeftRecHalfBuffCplt == 1) && (DmaRightRecHalfBuffCplt == 1))
	    {
	    	for(i = 0; i < 1024; i++)
	    	{
	    		PlayBuff[2*i]     = SaturaLH((LeftRecBuff[i] >> 8), -32768, 32767);
	    		PlayBuff[(2*i)+1] = SaturaLH((RightRecBuff[i] >> 8), -32768, 32767);
	    	}
	    	if(PlaybackStarted == 0)
	    	{
	    		if(0 != audio_drv->Play(AUDIO_I2C_ADDRESS, (uint16_t *) &PlayBuff[0], 4096))
	    		{
	    			Error_Handler();
	    		}
	    		if(HAL_OK != HAL_SAI_Transmit_DMA(&hsai_BlockA1, (uint8_t *) &PlayBuff[0], 4096))
	    		{
	    			Error_Handler();
	    		}
	    		PlaybackStarted = 1;
	    	}
	    	DmaLeftRecHalfBuffCplt  = 0;
	    	DmaRightRecHalfBuffCplt = 0;
	    }
	    if((DmaLeftRecBuffCplt == 1) && (DmaRightRecBuffCplt == 1))
	    {
	    	for(i = 1024; i < 2048; i++)
	    	{
	    		PlayBuff[2*i]     = SaturaLH((LeftRecBuff[i] >> 8), -32768, 32767);
	    		PlayBuff[(2*i)+1] = SaturaLH((RightRecBuff[i] >> 8), -32768, 32767);
	    	}
	    	DmaLeftRecBuffCplt  = 0;
	    	DmaRightRecBuffCplt = 0;
	    }

2. SecondAnalog App

Clock.png 45min