This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Coming soon |
This article explain what is and how to use GPIO through examplesl
1. GPIO definition
Stands for General Purpose Input/Output. GPIO is a type of pin found on an integrated circuit that does not have a specific function. While most pins have a dedicated purpose, such as sending a signal to a certain component, the function of a GPIO pin is customizable and can be controlled by software.
1.1. Configure GPIO for LED toggling
1.1.1. Objective
- Learn how to setup pin and GPIO port in STM32CubeMX
- Modify code generated by STM32CubeMX and use HAL functions
1.1.2. Goal
- Configure GPIO pin in STM32CubeMX and Generate Code
- Add in to project HAL_Delay function and HAL_GPIO_Toggle function
- Verify the correct functionality on toggling LED
1.1.3. Create project in STM32CubeMX
- New project > Access to board selector on main panel or Menu > File > New Project
- Select NUCLEO-L476RG
- if you have chosen to start the project with a board LED pin is already setted ( PA5 on NucleoL476RG, for other board check User Manual)
Note : whenever you download a firmware package with STM32CubeMX you have existing examples. You can find them for example here :
c:\Users\YourUserName\STM32Cube\Repository\STM32Cube_FW_G0_V1.3.0\Projects\NUCLEO-G071RB\Examples\GPIO\GPIO_IOToggle\GPIO_IOToggle.ioc
and open them with STM32CubeMX.
1.1.3.1. GPIO Configuration
- Select Push Pull mode
- No pull-up and pull-down
- Output speed to VERY HIGH is important for faster peripheries like SPI, USART
1.1.3.2. GPIO(Pin) output speed configuration
- Change the rising and falling edge when pin change state from high to low or low to high
- Higher GPIO speed increase EMI noise from STM32 and increase STM32 consumption
- It is good to adapt GPIO speed with periphery speed. Ex.: Toggling GPIO on 1Hz is LOW optimal settings, but SPI on 45MHz the VERY HIGH must be set
1.1.3.3. Set the project details for generation
1.1.3.4. Open the main.c in our IDE
- We will do the LED toggling in a function inside main.c
/* USER CODE BEGIN 3 */
/* Infinite loop */
while (1)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, GPIO_PIN_SET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_Delay(500);
}
/* USER CODE END 3 */
1.1.4. Compile and flash
- Every 500ms the green LED state change.