SFI Step-by-step on B-U585I-IOT02A

Revision as of 14:59, 16 June 2023 by Registered User

SFI Step-by-step on B-U585I-IOT02AClock.png75min

Target description

This tutorial shows how to use SFI for installing a simple LED Blink example to B-U585I-IOT02A.

The process goes through three 'steps' at the Original Equipment Manufacturer (OEM) and Contract Manufacturer (CM) sites.

  • Development @ OEM: the application code that runs on STM32 is generated.
  • Secure Room @ OEM: code prepared during the development is encrypted and packaged to be sent for manufacturing. The Secure Room is isolated, and its resources are not visible outside of it.
  • Manufacturing @ CM: the encrypted code received by the OEM Secure Room is installed using SFI tools.


Prerequisites

Hardware

  • B-U585I-IOT02A[1] Discovery kit for IoT node with STM32U5 series
  • STM32-HSM[2] SAM for Secure Firmware Installation
  • Smartcard Reader
    • Laptop Built-in
    • External
  • STLINK-V3[3] modular in-circuit debugger and programmer for STM32/STM8
  • 2 x USB cable Type-A to Micro-B
  • Jump wires

Software

  • STM32CubeProgrammer[4] Software programming tool for STM32 (v2.90 min)
    • Including STM32TrustedPackageCreator
  • STM32CubeU5[5] STM32Cube MCU Package for STM32U5 series
  • STM32CubeIDE[6] Integrated Development Environment for STM32

Literature

  • AN4992 STM32 MCUs secure firmware install (SFI) overview
  • UM2237 STM32CubeProgrammer software description
  • UM2238 STM32 Trusted Package Creator tool software description
  • AN5054 Secure programming using STM32CubeProgrammer
  • AN2606 STM32 microcontroller system memory boot mode
  • RM0456 STM32U575/585 Arm®-based 32-bit MCUs
  • UM2839 Discovery kit for IoT node with STM32U5 Serie
  • UM2448 STLINK-V3SET debugger/programmer for STM8 and STM32



1. Environment setup

Before starting, the first step is to prepare the environment to be able to go through the SFI process.

You can refer to this article.

2. Development @ OEM

The first step of the process is to create a demo LED Blink application for B-U585I-IOT02A.
You can use the example project developed in xcube-sfi, or create a new project.
These two options are described in this section of the following article: SFI Step-by-step on STM32 boards.
The Third option is to use an example from the STM32CubeU5 firmware package. We took GPIO_IOToggle_TrustZone as an example (description in the next paragraph).


Info white.png Information
In this page, we use STM32CubeIDE, but the process is valid for any other compatible toolchain
Info white.png Information
You could use your working application binary for B-U585I-IOT02A instead.
Warning white.png Warning
Note: the STM32 SFI process can only perform secure programming in user Flash memory

firmware using Arm® TrustZone® - the application code must be TrustZone compatible.


3. Download STM32CubeU5 Firmware package

Clock.png 10min
For this step, we use the GPIO_IOToggle_TrustZone project example included in STM32CubeU5 [5] MCU package. STM32CubeU5 MCU Package includes the STM32Cube hardware abstraction layer (HAL) and the low-layer (LL) APIs, plus a consistent set of middleware components (Azure RTOS USBX, FileX/LevelX, ThreadX, NetX Duo, USB Power Delivery, TF‑M, mbed-crypto, Touch library, Network library, and OpenBootloader). All embedded software utilities are delivered with a full set of examples running on STMicroelectronics boards.

  • Open STM32CubeMX
  • Click Manage embedded software packages in Help
  • In the STM32Cube MCU Packages tab, check the last STM32CubeU5 release version
  • Click Install (it may take a long time)
Download STM32CubeU5.png


STM32CubeU5 MCU package is now installed on your computer (typical location C:\Users\myname\STM32Cube\Repository\STM32Cube_FW_U5_Vx.xx.x).

3.1. Configure the GPIO_IOToggle_TrustZone Project included in STM32CubeU5

Clock.png 5min
Open the .project included in <STM32CubeU5 FOLDER>\Projects\B-U585I-IOT02A\Examples\GPIO\GPIO_IOToggle_TrustZone\STM32CubeIDE\ with STM32CubeIDE.

  • From Project explorer, click on GPIO_IOToggle_TrustZone_NonSecure , then right click and select Properties.
  • Navigate to C/C++ Build > Settings > Tool Settings > MCU Post build output.
  • Make sure Convert to binary file (-O binary) is checked
  • Click Apply and Close.
cubeIDE convert to binary

3.2. Build the project

Clock.png 2min
From Project explorer, click on GPIO_IOToggle_TrustZone_NonSecure , then right click and select Build Project. This triggers the compilation of both GPIO_IOToggle_TrustZone_Secure and GPIO_IOToggle_TrustZone_NonSecure projects (in this order).

Copy the Secure and NonSecure binaries to the 'ROOT_FOLDER' - in this example, the binaries are available in:

  • Projects\B-U585I-IOT02A\Examples\GPIO\GPIO_IOToggle_TrustZone\STM32CubeIDE\NonSecure\Debug\GPIO_IOToggle_TrustZone_NonSecure.bin
  • Projects\B-U585I-IOT02A\Examples\GPIO\GPIO_IOToggle_TrustZone\STM32CubeIDE\Secure\Debug\GPIO_IOToggle_TrustZone_Secure.bin

4. Secure Room @ OEM

In the Secure Room, the following two steps are performed:

  • SFI package generation: the code prepared during the development is encrypted and packaged to be sent for manufacturing.
  • HSM Provisioning: the HSM is provisioned with the keys used for encryption and with the max license counter.
Warning white.png Warning
The assumption is that the Secure Room is isolated and its resources are not accessible from the outside world.


4.1. SFI package generation

Clock.png10min

In this step, the application binary file (including S and NS applications) and the option byte configuration are encrypted in an SFI package.

The following inputs are needed:

  • Secure and Non-Secure Application Binary files (created in the previous step) and download addresses in FLASH.
  • AES Key
  • Nonce
  • Option bytes

4.1.1. Download address

Each binary composing the OEM application is designed to be executed from a specific address in FLASH. The SFI process ensures that each binary is downloaded at the address specified as an input parameter.

  • For this example, we use:
    • 0x0C000000 for GPIO_IOToggle_TrustZone_Secure
    • 0x08100000 for GPIO_IOToggle_TrustZone_NonSecure

4.1.2. Key generation

The first step is to create secret keys and the nonce that is used by STM32TrustedPackageCreator to encrypt the firmware image in the SFI package which is programmed in the STM32-HSM.

Info white.png Information
In this page, we use dummy values, the OEM can create its keys with arbitrary values
4.1.2.1. AES Key

To create the encryption key file you can refer to: Encryption key file creation

4.1.2.2. AES Nonce

To create the AES nonce file you can refer to: Nonce key file creation

4.1.3. Option bytes

Together with installing the application binary, the SFI process can be used to specify the OB values to be configured at the end of the installation process.

  1. Create a new text file
  2. Paste the following text
  3. OPTR,0x9DA9F9DC
    NSBOOTADD0R,0x0800007F
    NSBOOTADD1R,0x0BF9007F
    SECBOOTADD0R,0x0C00007C
    SECWM1R1,0xFFFFFF80
    SECWM1R2,0x7F807F80
    WRP1AR,0xFF80FFFF
    WRP1BR,0xFF80FFFF
    SECWM2R1,0xFF80FFFF
    SECWM2R2,0x7F807F80
    WRP2AR,0xFF80FFFF
    WRP2BR,0xFF80FFFF
    OEM1KEYR1,0x00000000
    OEM1KEYR2,0x00000000
    OEM2KEYR1,0x00000000
    OEM2KEYR2,0x00000000
    
  4. Save it as ob.csv.

This example of an OB file configures the option bytes as described below:

  • FOPTSR_PRG,0x9DA9F955
    • TZEN: 0x1 (Global TrustZone security enabled)
    • IO_VDDIO2_HSLV: 0x0 (High-speed IO at low VDDIO2 voltage feature disabled (VDDIO2 can exceed 2.5 V))
    • IO_VDD_HSLV: 0x0 (High-speed IO at low VDD voltage feature disabled (VDD can exceed 2.5 V))
    • PA15_PUPEN: 0x1 (USB power delivery dead-battery disabled/ TDI pull-up activated)
    • nBOOT0: 0x1 (nBOOT0 = 1)
    • nSWBOOT0: 0x1 (BOOT0 taken from PH3/BOOT0 pin)
    • SRAM2_RST: 0x0 (SRAM2 erased when a system reset occurs)
    • SRAM2_ECC: 0x1 (SRAM2 ECC check disabled)
    • SRAM3_ECC: 0x1 (SRAM3 ECC check disabled)
    • BKPRAM_ECC: 0x0 (Backup RAM ECC check enabled)
    • DBANK: 0x1 (Dual bank mode with 64 bits data)
    • SWAP_BANK: 0x0 (Bank 1 and bank 2 address are not swapped)
    • WWDG_SW: 0x1 (Software window watchdog)
    • IWDG_STDBY: 0x0 (Freeze IWDG counter in standby mode)
    • IWDG_STOP: 0x0 (Freeze IWDG counter in stop mode)
    • IWDG_SW: 0x1 (Software independent watchdog)
    • SRAM134_RST: 0x1 (SRAM1, SRAM3 and SRAM4 not erased when a system reset occurs)
    • nRST_SHDW: 0x1 (No reset generated when entering the Shutdown mode)
    • nRST_STDBY: 0x1 (No reset generated when entering Standby mode)
    • nRST_STOP: 0x1 (No reset generated when entering Stop mode)
    • SRAM2_PE: 0x1 (SRAM2 parity check disable)
    • BOR_LEV: 0x1 (BOR Level 1, reset level threshold is around 2.0 V)
    • RDP: 0x55 (Level 0.5)


  • NSBOOTADD0R,0x0800007F
    • NSBOOTADD0: 0x100000(0x8000000)
  • NSBOOTADD1R,0x0BF9007F
    • NSBOOTADD1: 0x17F200(0xBF90000)
  • SECBOOTADD0R,0x0C00007C
    • SECBOOTADD0: 0x1800C0 (0xC006000)
    • BOOT_LOCK: 0x0 (Boot based on the pad/option bit configuration)
  • SECWM1R1,0xFFFFFF80
    • SECWM1_PSTRT: 0x0 (0x8000000)
    • SECWM1_PEND: 0xFF (0x81FE000)
  • SECWM1R2,0x7F807F80
    • HDP1_PEND: 0x0 (0xC001FFF)
    • HDP1EN: 0x0 (No HDP area 1)
  • WRP1AR,0xFF80FFFF
    • WRP1A_PSTRT: 0x7F (0x80FE000)
    • WRP1A_PEND: 0x0 (0x8000000)
    • UNLOCK_1A: 0x1 (WRP1A starts and ends pages unlocked)
  • WRP1BR,0xFF80FFFF
    • WRP1B_PSTRT: 0x7F (0x80FE000)
    • WRP1B_PEND: 0x0 (0x8000000)
    • UNLOCK_1B: 0x1 (WRP1B start and end pages unlocked)
  • SECWM2R1,0xFF80FFFF
    • SECWM2_PSTRT: 0x7F (0x81FE000)
    • SECWM2_PEND: 0x0 (0x8100000)
  • SECWM2R2,0x7F807F80
    • HDP2_PEND: 0x0 (0xC101FFF)
    • HDP2EN: 0x0 (No HDP area 2)
  • WRP2AR,0xFF80FFFF
    • WRP2A_PSTRT: 0x7F (0x81FE000)
    • WRP2A_PEND: 0x0 (0x8100000)
    • UNLOCK_2A: 0x1 (WRP2A start and end pages unlocked)
  • WRP2BR,0xFF80FFFF
    • WRP2B_PSTRT: 0x7F (0x81FE000)
    • WRP2B_PEND: 0x0 (0x8100000)
    • UNLOCK_2B: 0x1 (WRP2B start and end pages unlocked)
  • OEM1KEYR1,0x00000000
  • OEM1KEYR2,0x00000000
  • OEM2KEYR1,0x00000000
  • OEM2KEYR2,0x00000000
Info white.png Information
You can find OB files for each supported MCU under the following installation path C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\SFI_OB_CSV_FILES
Info white.png Information
You can refer to RM0456 for details on OB register values.

4.1.4. Output generation

Now we have all the parameters needed for the creation of the SFI package with the following command.

STM32TrustedPackageCreator_CLI.exe -sfi -fir GPIO_IOToggle_TrustZone_Secure.bin 0x0C000000 -fir GPIO_IOToggle_TrustZone_NonSecure.bin 0x08100000 -k aeskey.bin -n nonce.bin -ob ob.csv -v 1 --ramsize 0x55500 --token 0x80F0000 -hash 1 -o U585_LedBlink.sfi

The command creates the U585_LedBlink.sfi package (you can change the verbose level of the command with the parameter -v 1,2,3)

SFI cmd generation U585


4.2. HSM programming

Clock.png10min

To program the HSM, you can follow the same steps described in this section of the SFI article using the B-U585I-IOT02A board: HSM programming.

After programming the HSM, it is now ready to be shipped to the CM together with the U585_LedBlink.sfi package created before.

5. Manufacturing @ CM

Clock.png6min

In this step, the CM receives from the OEM the HSM card provisioned with the secret key and initialized with a max counter of licenses, and the .sfi package to be installed (including the firmware in encrypted form and the option bytes configuration).

The SFI process could be performed through a regular JTAG/SWD interface or the system bootloader interface (you can refer to AN2606 for details on the supported interface for each microcontroller). The following section covers JTAG/SWD, USART, and SPI interfaces - each section includes the following sections:

  • Hardware connection
  • Option Bytes regression (optional)
  • Secure Firmware Install
Info white.png Information
The Option Bytes regression step configures the OB to their default state (this operation may not be needed if the CM runs the SFI process on a virgin part).


5.1. Hardware connection

Plug a micro-USB cable into CN8 and make sure that JP4 is in the STLINK position.

5.2. Option bytes regression

The following steps configure the device to regress the option bytes configuration to a default state:

STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob RDP=0xAA TZEN=1 nSWBOOT0=1 nBOOT0=1 SECBOOTADD0=0x180000 SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 DBANK=0x01 -e all -ob displ

After this step, the device is ready for the SFI process.

5.3. Firmware install

This command starts the SFI process and proceeds with the installation.

STM32_Programmer_CLI.exe -vb 1 -log U585_LedBlink.log -c port=SWD mode=HOTPLUG -sfi protocol=static U585_LedBlink.sfi hsm=1 slot=1 -rsse C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\RSSe\U5\enc_signed_RSSe_sfi.bin
Info white.png Information
You can refer to AN5054 for details on hsm and slot parameters.
SFI cmd installation U585

After the installation of the multiple chunks of the code, the SFI process completes successfully

SFI cmd installationU585 - 2.png

After this step, the device is programmed with the OEM application code.

Info white.png Information
You can check the log of the process saved in the file U585_LedBlink.log.


6. References