![]() |
Coming soon |
This article explains what the I3C is and it describes how to set up an I3C controller based on STM32H5 microcontroller and a shield board IKS01A3 (LSM6DSO accelerometer/gyroscope and LPS22HH barometer) as an I3C target.
1. What is inter-integrated circuit (I3C)?
MIPI I3C is a serial communication interface specification that improves upon the features, performance, and power use of I²C, while maintaining backward compatibility for most devices.
An I3C bus Controller device drives the push-pull SCL line at the communication bus speed, up to 12.5 MHz.
I3C supports several communication formats, all sharing a two-wire interface. The two wires are designated SDA and SCL:
- SDA (Serial Data) is a bidirectional data pin, the line on which master and slave send or receive the information (sequence of bits).
- SCL (Serial Clock) is the clock-dedicated line for data flow synchronization.
The main purpose of MIPI I3C is threefold:
1. To standardize communication inside embedded systems with a reconfigurable bus,
2. To reduce the number of physical pins used,
3. To support low-power, high-speed data transfer, up to 33 Mbps.
1.1. I3C Bus Configuration
I3C bus can be configured with multiple devices. There are four main types of devices:
• I3C main controller
• I3C secondary controller
• I3C target
• Legacy I2C target
1.2. Features
The I3C bus supports different modes and operations of various message types:
• Broadcast and direct common command code CCC messages to communicate with multiple devices or a specific one.
• Dynamic addressing: assigns a dynamic address unlike I2C, which has a static address.
• Private read/write transfers.
• Legacy I2C messages: the I3C controller can communicate with I2C devices on the I3C bus.
• In Band interrupt IBI: the target device, which is connected on the bus can send an interrupt to the controller over the two-wire (SCL / SDA)
• Hot-Join request: the target can join the I3C bus after the initialization.
• Controller role request
1.3. I2C vs. I3C: What are the differences?
The I3C SDR mode allows only for legacy I2C target devices to coexist with I3C devices on the same I3C bus.
The following table compares I2C versus I3C interface types and mentions difference between I2C and I3C:
2. Setup & demo examples
2.1. Hardware prerequisites
• 1x STM32 Nucleo development board (NUCLEO-H503RB)
• 1x Motion MEMS and environmental sensor expansion board (X-NUCLEO-IKS01A3):
The X-NUCLEO-IKS01A3 is compatible with the Arduino UNO R3 connector layout and features the LSM6DSO 3-axis accelerometer + 3-axis gyroscope, the LIS2MDL 3-axis magnetometer, the LIS2DW12 3-axis accelerometer, the HTS221 humidity and temperature sensor, the LPS22HH pressure sensor, and the STTS751 temperature sensor. The X-NUCLEO-IKS01A3 interfaces with the STM32 microcontroller via the I2C/I3C pin, and it is possible to change the default I2C/I3C port.
X-NUCLEO-IKS01A3 plugged on an STM32 Nucleo board
2.2. Examples
Example 1: Assign a dynamic address to the LSM6DSO using ENTDAA CCC (Enter Dynamic Address Assignment) Keep only JP2.
Example 2: Assign a dynamic address to the LPS22HH using SETDASA CCC (Set Dynamic Address from Static Address) Keep only JP4.
3. Configure the I3C Controller to communicate with the I3C Targets (LSM6DSO and LPS22HH):
3.1. Objective
Assign a dynamic address using NUCLEO-H503RB as I3C controller and LSM6DSO & LPS22HH as Targets with two different modes.
3.2. Create a project in STM32CubeIDE
- File > New > STM32 Project in main panel.
- Select NUCLEO-H503RB board using Board Selector and click Next as shown in the figure below.
- Save the project.
- Initialize all peripherals with their default settings.
Answer “Yes” to initialize all peripherals with their default mode? Popup as below:
In case you haven't downloaded the STM32H5Cube library, it will be downloaded automatically. This however may take some time.
3.3. Configure I3C
Open the STM32CubeMX project from the workspace
- Under Connectivity, select I3C1
- Select PB6: SCL and PB7: SDA for I3C1
- Select Controller mode.
- Set the I3C frequency at 3000 KHz
- Select I3C pure bus (Only I3C devices on the bus)
NVIC settings
In the NVIC settings tab :
- Enable event interrupt and error interrupt in the NVIC tab
Clock configuration
Select the system Clock at 250MHz :
- Select HSI from PLL1 Source Mux
- Select PLLCLK from System Clock Mux
- Set HCLK at 250MHz.
- Select PCLK from the I3C1 Clock Mux
Verify : PLLM = 4, PLLN = 31, PLLP = 2, PLLQ = 2, PLLR = 2, APB1 Prescaler =1.
3.4. Generate source code and edit main.c
- Click "Ctrl+S" to generate the project.
4. Software settings
4.1. Dynamic addressing using ENTDAA CCC (LSM6DSO)
4.1.1. Blocking Mode
- Open main.c in Project Explorer / project_name / Src / main.c :
/* USER CODE BEGIN 2 */
/* Buffer that contain payload data, mean PID, BCR, DCR */
uint64_t payload [64];
uint8_t dynamic_adr = 0x32;
HAL_StatusTypeDef status = HAL_OK;
/* Assign dynamic address processus */
do
{
status = HAL_I3C_Ctrl_DynAddrAssign(&hi3c1, &payload[1], I3C_ONLY_ENTDAA, 5000);
if (status == HAL_BUSY)
{
HAL_I3C_Ctrl_SetDynAddr(&hi3c1, dynamic_adr);
}
TargetDesc1.TARGET_BCR_DCR_PID = (uint64_t) payload;
} while (status == HAL_BUSY);
/* USER CODE END 2 */
4.1.2. Interrupt Mode
- Open main.h in Project Explorer / project_name / Inc / main.h.
/* USER CODE BEGIN ET */
typedef struct {
char * TARGET_NAME; /*!< Marketing Target reference */
uint32_t TARGET_ID; /*!< Target Identifier on the Bus */
uint64_t TARGET_BCR_DCR_PID; /*!< Concatenation value of PID, BCR and DCR of the target */
uint8_t STATIC_ADDR; /*!< Static Address of the target, value found in the datasheet of the device */
uint8_t DYNAMIC_ADDR; /*!< Dynamic Address of the target preset by software/application */
} TargetDesc_TypeDef;
/* USER CODE END ET */
Insert the following line also :
/* USER CODE BEGIN Private defines */
/* Define Target Identifier */
#define DEVICE_ID1 0U
- Create target.h in Project Explorer / project_name / Inc / target.h :
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __STM32_I3C_DESC_TARGET1_H
#define __STM32_I3C_DESC_TARGET1_H
/* Includes ------------------------------------------------------------------*/
/* Exported types ------------------------------------------------------------*/
/* Exported constants --------------------------------------------------------*/
#define TARGET1_DYN_ADDR 0x32
/********************/
/* Target Descriptor */
/********************/
TargetDesc_TypeDef TargetDesc1 =
{
"TARGET_ID1",
DEVICE_ID1,
0x0000000000000000,
0x00,
TARGET1_DYN_ADDR,
};
#endif /* __STM32_I3C_DESC_TARGET1_H */
- Open main.c in Project Explorer / project_name / Src / main.c :
Include the Target lib into the project :
/* USER CODE BEGIN Includes */
#include "target.h"
/* USER CODE END Includes */
Add the target descriptor :
/* USER CODE BEGIN PV */
/* Array contain targets descriptor */
TargetDesc_TypeDef *aTargetDesc[1] = \
{
&TargetDesc1, /* DEVICE_ID1 */
};
/* Buffer that contain payload data, mean PID, BCR, DCR */
uint8_t aPayloadBuffer[64];
/* USER CODE END PV */
/* USER CODE BEGIN 2 */
/* Assign dynamic address processus ## Initiate a RSTDAA before a ENTDAA procedure ##*/
if (HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, I3C_RSTDAA_THEN_ENTDAA) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END 2 */
Callback
/* USER CODE BEGIN 4 */
void HAL_I3C_TgtReqDynamicAddrCallback(I3C_HandleTypeDef *hi3c, uint64_t targetPayload)
{
TargetDesc1.TARGET_BCR_DCR_PID = targetPayload;
HAL_I3C_Ctrl_SetDynAddr(hi3c, TargetDesc1.DYNAMIC_ADDR);
}
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
/* USER CODE END 4 */
4.2. Dynamic addressing using SETDASA CCC (LPS22HH)
- Open main.c in Project Explorer / project_name / Src / main.c :
/* USER CODE BEGIN PTD */
#define Unicast_SETDASA 0x87
#define Brodacast_DISEC 0x01
#define Brodacast_RST 0x06
#define SETNEWDA 0x88
#define LPS22HH_DYNAMIC_ADDR 0x32
/* USER CODE END PTD */
/* USER CODE BEGIN PD */
#define I3C_IDX_FRAME_1 0U /* Index of Frame 1 */
#define I3C_IDX_FRAME_2 1U /* Index of Frame 2 */
/* USER CODE END PD */
/* USER CODE BEGIN PV */
uint8_t aSETDASA_LPS22HH_data[1] = {(LPS22HH_DYNAMIC_ADDR << 1)};
uint8_t aDISEC_data[1] = {0x08};
/* Buffer used for transmission */
uint8_t aTxBuffer[0x0F];
/* Buffer used by HAL to compute control data for the Private Communication */
uint32_t aControlBuffer[0xF];
/* Context buffer related to Frame context, contain different buffer value for a communication */
I3C_XferTypeDef aContextBuffers[2];
I3C_XferTypeDef ContextBuffers[2];
/* Descriptor for direct write SETDASA CCC */
I3C_CCCTypeDef aSET_DASA_LPS22HH[] =
{
/*Target Addr CCC Value CCC data + defbyte pointer CCC size + defbyte Direction */
{0x5D,Unicast_SETDASA,{aSETDASA_LPS22HH_data,1},HAL_I3C_DIRECTION_WRITE},
};
/* Descriptor for direct write DISEC CCC */
I3C_CCCTypeDef aSET_CCC_DISEC[] =
{
{0x5D,Brodacast_DISEC, {aDISEC_data,1},LL_I3C_DIRECTION_WRITE},
};
/* Descriptor for direct write RST CCC */
I3C_CCCTypeDef aSET_CCC_RST[] =
{
{0x5D,Brodacast_RST, {NULL,0},LL_I3C_DIRECTION_WRITE},
};
/* USER CODE END PV */
/* USER CODE BEGIN 2 */
/* Send a DISEC to disable target HotJoin */
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.pBuffer = aControlBuffer;
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.Size = COUNTOF(aControlBuffer);
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.pBuffer = aTxBuffer;
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.Size = 1;
/* Add context buffer Set CCC frame in Frame context */
if (HAL_I3C_AddDescToFrame(&hi3c1,
aSET_CCC_DISEC,
NULL,
aContextBuffers,
COUNTOF(aSET_CCC_DISEC),
I3C_BROADCAST_WITHOUT_DEFBYTE_RESTART) != HAL_OK)
{
Error_Handler();
}
if (HAL_I3C_Ctrl_TransmitCCC(&hi3c1, aContextBuffers, 1000) != HAL_OK)
{
Error_Handler();
}
while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY)
{
}
/* Send a RSTDAA to reset all the dynamic addresses of the targets */
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.pBuffer = aControlBuffer;
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.Size = COUNTOF(aControlBuffer);
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.pBuffer = aTxBuffer;
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.Size = 1;
/*Add context buffer Set CCC frame in Frame context */
if (HAL_I3C_AddDescToFrame(&hi3c1,
aSET_CCC_RST,
NULL,
aContextBuffers,
COUNTOF(aSET_CCC_RST),
I3C_BROADCAST_WITHOUT_DEFBYTE_RESTART) != HAL_OK)
{
Error_Handler();
}
if (HAL_I3C_Ctrl_TransmitCCC(&hi3c1, aContextBuffers, 1000) != HAL_OK)
{
Error_Handler();
}
while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY)
{
}
/* Send a SETDASA to set the dynamic on LPS22HH using his static address */
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.pBuffer = aControlBuffer;
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.Size = COUNTOF(aControlBuffer);
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.pBuffer = aTxBuffer;
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.Size = 1;
/* Add context buffer Set CCC frame in Frame context */
if (HAL_I3C_AddDescToFrame(&hi3c1,
aSET_DASA_LPS22HH,
NULL,
&aContextBuffers[I3C_IDX_FRAME_1],
1,
I3C_DIRECT_WITHOUT_DEFBYTE_RESTART) != HAL_OK)
{
Error_Handler();
}
if (HAL_I3C_Ctrl_TransmitCCC_IT(&hi3c1, &aContextBuffers[I3C_IDX_FRAME_1]) != HAL_OK)
{
Error_Handler();
}
while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY)
{
}
/* After a dynamic address has been assigned, the sensor is recognized as an I3C device */
/* Check if the LPS22HH sensor is ready to communicate in I3C */
if (HAL_I3C_Ctrl_IsDeviceI3C_Ready(&hi3c1, LPS22HH_DYNAMIC_ADDR, 300, 1000) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END 2 */
4.3. Compile and flash
4.4. Results
After running the project :
4.4.1. Example 1 result (LSM6DSO as target)
We can check this example by verifying the SDA and SCL behavior with the oscilloscope as shown below (LSM6DSO using ENTDAA CCC):
From LSM6DSO datasheet :
Device ID register PID : 0x0208006C100B
Bus characteristics register BCR : 0x07
Device Characteristic Register DCR : 0x44
4.4.2. Example 2 result (LPS22HH as target)
We can check this example by verifying the SDA and SCL behavior with the oscilloscope as shown below (LPS22HH using SETDASA CCC):
- Broadcast DISEC CCC : 0x01 (0x08 : Disable IBI interrupt )
- Reset a previous Dynamic address : Broadcast RSTDAA 0x06
5. References
- AN5879 : Introduction to I3C for STM32H5 series MCU
- RM0492 : STM32H503xx Reference manual
- DS12140 : LSM6DSO Datasheet