Getting started with DAC

Revision as of 14:58, 2 January 2023 by Registered User
Under construction.png Coming soon

This article explains what DAC is and how to use it through examples

1. What is a digital to analog converter (DAC)?

A digital to analog converter is a system that converts a digital input signal or a value into an analog signal. It takes in a digital number or value as an input and converts it into an analog voltage. The voltage level corresponds to the binary number in the DAC output register.

To better understand DACs, we will take a look at the STM32L4 DAC in this article.

1.1. Simplified Block Diagram

simplified block diagram

1.2. DAC main features

  • 8 or 12 bit mode: The DAC can support different input formats:
    • 8-bit right aligned data format.
      For dual mode (to provide input data for 2 DACs): 8-bit + 8-bit
    • 12-bit mode: either a right or left aligned mode

DAC data format5.png

  • Buffered output: the DAC output can have a low impedance buffer to drive external loads
  • Sample and Hold mode to reduce power consumption
  • Synchronized update capability
  • DMA capability to offload CPU
  • Several trigger inputs: The DAC output data can be updated by a timer, an external trigger or a software trigger
  • Signal generation: DAC integrates small logic to generate noise waves as well as triangle waves

2. Configure DAC to generate a wave

2.1. Objectives

  • Learn how to setup the DAC as wave generator in STM32CubeMX
  • Generate code in STM32CubeMX and use HAL functions
  • Create a simple application to test the DAC

2.2. Create the project in STM32CubeIDE

  • File > New > STM32 Project in main panel.

create STM32CubeIDE project.png.

This example uses the NUCLEO-L476RG board.

  • Select NUCLEO-L476RG board using Board Selector as shown in the figure below:

Select NUCLEO-L476RG board.png

In case you haven't downloaded the STM32L476 Cube library, it will be downloaded automatically. This however may take some time.

  • Save the project

DAC.png

2.3. Configure DAC

  • Search for DAC1 in the left search field

We will use PA5 as the DAC's output. However, we need to reset it first, as it is configured as GPIO Output by default.

Info white.png Information
For more information on GPIO, please refer to the Getting started with GPIO page
  • Search for PA5 in the bottom right search field, then click Reset_State

Pinout2.png

  • Set OUT2 to connected to: only to external pin. Notice how PA5 is automatically set to DAC1_OUT2 on the pinout view
  • Parameter Settings should be as below: normal mode, buffer enabled and no trigger

DAC Output Config.PNG

2.4. Generate project and edit main.c

  • Click "Ctrl+S" to generate the project

Generate project.png

  • Edit main.c
Info white.png Information
Insert your code between /* USER CODE BEGIN PV */ and /* USER CODE END PV */ tags
/* USER CODE BEGIN PV */
uint16_t dac_value=0;
/* USER CODE END PV */
Info white.png Information
Start the DAC by inserting the required code between /* USER CODE BEGIN 2*/ and /* USER CODE END 2 */ tags
/* USER CODE BEGIN 2 */
HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);
/* USER CODE END 2 */
Info white.png Information
Set the DAC output value by inserting the required code between /* USER CODE BEGIN 3 */ and /* USER CODE END 3 */ tags
/* USER CODE BEGIN 3 */
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_12B_R, dac_value);
if (dac_value < 4095) {
	dac_value++;
} else {
	dac_value=0;
}
HAL_Delay(1);
/* USER CODE END 3 */
  • Explanation

Inside the if conditional statement, we check if dac_value is lower than 4095 (0xFFF) which is the maximum output value for a 12-bit resolution DAC:

  • If the value is lower than the maximum value, it is incremented
  • If not, it is reset back to zero
  • Then, we add a 1ms delay in order to have a stable output value

This will be running in the infinite loop. Therefore, the code will sweep through all the possible DAC output values, and then reset it to zero restarting the process all over again.

2.5. Compile and flash

  • Click on Build button Built.png
  • Click on Debug button (to run step by step) Debug.png
  • Or on Run button (to execute) Run.png

2.6. Build a simple signal generator

  • On NUCLEO-L476RG, PA5 is connected to the user LED LD2. As a consequence, the DAC's output voltage is driving LD2. Notice how it progressively lights up before being switched off when the DAC's output is reset to 0
  • Connect your multimeter or oscilloscope to the PA5 pin, the DAC output gradually increases up to a maximum output value which is 3V. Then, it is reset to 0, drawing a sawtooth wave

File:Swatooth.jpg

  • Explore further possibilities such as :
  • Audio and waveform generation [1]
  • Extending the DAC performance [2]

3. References

The following documents and more are available on ST's website [3]



[[category:Getting_started_with_STM32_system_peripherals | 65]]

  1. AN3126 - Audio and waveform generation using the DAC in STM32 products[1]
  2. AN4566 - Extending the DAC performance of STM32 microcontrollers[2]
  3. https://www.st.com