![]() |
Coming soon |
This article explains what SPI is and uses examples to demonstrate how to use it.
1. What is Serial Peripheral Interface (SPI)?
Serial Peripheral Interface (SPI) is a synchronous serial communication interface specification used for short-distance communication, primarily in embedded systems. The interface was developed by Motorola in the mid-1980s and has become a de facto standard. SPI devices can communicate in full duplex mode using a master-slave architecture, with most often a single master. The master (controller) device originates the frame for reading and writing. Multiple slave devices may be supported through selection with individual chip select (CS), sometimes called slave select (SS), lines.
In full duplex mode with multiple slaves, SPI uses four buses:
- SCK (Serial Clock) bus, controlled by the master device
- MISO (Master Input Slave Output) bus
- MOSI (Master Output Slave Input) bus
- SS (Slave Select) bus, useful in the case of a multiple-slave configuration
1.1. STM32 SPI Modes
The SPI interface is highly configurable to support many standard protocols and can operate in various modes.
- Full-Duplex
- Half-Duplex
- Receive Only
- Transmit Only
1.2. STM32 SPI Parameters
Basic parameters:
- Frame format: Motorola or TI
- Data size: 4 to 16 bits depending on STM32
- First bit: MSB or LSB
Clock parameters:
- Prescaler: from 2 to 256. Note that SPI clock speed cannot exceed half of the internal bus frequency.
- Clock polarity (CPOL): Low or high
- Clock Phase (CPHA): 1 or 2 Edge
1.3. Main SPI HAL functions
Based on STM32Cube HAL functions, SPI data transfer can be performed in 3 modes: Blocking Mode, Interrupt Mode or DMA Mode.
- Blocking Mode:
- The communication is performed in polling mode. The status of all data processing is returned by the same function after finishing transfer.
- HAL_SPI_Transmit()
- HAL_SPI_Receive()
- HAL_SPI_TransmitReceive()
- HAL_SPI_Transmit()
- Non-blocking modes
- The communication is performed using Interrupts or DMA. These functions return the status of the transfer startup.
- The end of the data processing will be indicated through the dedicated SPI IRQ when using Interrupt mode or the DMA IRQ when using DMA mode.
- Interrupt Mode:
- HAL_SPI_Transmit_IT()
- HAL_SPI_Receive_IT()
- HAL_SPI_TransmitReceive_IT()
- HAL_SPI_Transmit_IT()
- DMA Mode:
- HAL_SPI_Transmit_DMA()
- HAL_SPI_Receive_DMA()
- HAL_SPI_TransmitReceive_DMA()
- HAL_SPI_Transmit_DMA()
2. Configure the SPI to communicate between 2 boards
2.1. Objective
In this example, the objective is to set up communication through SPI between two NUCLEO-L476RG. Here data is transmitted by master and received by slave.
2.2. Master board project
2.2.1. Create master project in STM32CubeIDE
- The NUCLEO-L476RG pinout is helpful to set the wiring between the boards in the project.
- File>New>STM32 Project in main panel.
- Select NUCLEO-L476RG board using Board Selector as shown in the below figure.
In case you haven't downloaded the STM32CubeL4 firmware package, it will be downloaded automatically, it may take some time.
- Save the project.
2.2.2. Configure SPI on master board
- Open the STM32CubeMX project from the workspace.
2.2.2.1. SPI settings
- Under Connectivity, select SPI1.
- Select Full-Duplex Master mode:
- Pin PA5 as SCK
- Pin PA6 as MISO
- Pin PA7 as MOSI
- Pin PA5 as SCK
- Leave SPI parameters settings in default configuration.
2.2.2.2. GIPO settings
- Leave GPIO settings in default configuration.
2.2.2.3. NVIC and DMA settings
- Interrupt Mode only
- In the NVIC settings tab
- Enable interrupt
- In the NVIC settings tab
- DMA Mode only
- In the DMA settings tab
- In the DMA settings tab
- Add SPI1_TX for Master
2.2.3. Generate source code and edit main.c
- Click "Ctrl+S" to generate the project.
- Open main.c in Project Explorer / myproject / Src / main.c.
/* USER CODE BEGIN PV */
/* Private variables */
uint8_t TX_Buffer [] = "A" ; // DATA to send
/* USER CODE END PV */
- Blocking Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Transmit(&hspi1, TX_Buffer, 1, 1000); //Sending in Blocking mode
HAL_Delay(100);
/* USER CODE END 2 */
- Interrupt Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Transmit_IT(&hspi1, TX_Buffer, 1); //Sending in Interrupt mode
HAL_Delay(100);
/* USER CODE END 2 */
- DMA Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Transmit_DMA(&hspi1, TX_Buffer, 1);; //Sending in DMA mode
HAL_Delay(100);
/* USER CODE END 2 */
2.2.4. Compile and flash on master board
2.3. Slave board project
2.3.1. Create slave project in STM32CubeIDE
- Create a new project as discribed in section #Create master project in STM32CubeIDE.
2.3.2. Configure SPI on slave board
- Open the STM32CubeMX project from the workspace.
2.3.2.1. SPI settings
- Under Connectivity, select SPI1.
- Select Full-Duplex Slave mode:
- Pin PA5 as SCK
- Pin PA6 as MISO
- Pin PA7 as MOSI
- Pin PA5 as SCK
- Leave SPI parameters settings in default configuration.
2.3.2.2. GIPO settings
- Leave GPIO settings in default configuration.
2.3.2.3. NVIC and DMA settings
- Interrupt Mode only
- In the NVIC settings tab
- Enable interrupt
- In the NVIC settings tab
- DMA Mode only
- In the DMA settings tab
- In the DMA settings tab
- Add SPI1_RX for Master
2.3.3. Generate source code and edit main.c
- Click "Ctrl+S" to generate the project.
- Open main.c in Project Explorer / myproject / Src / main.c.
/* USER CODE BEGIN PV */
/* Private variables */
uint8_t RX_Buffer [1] ; // DATA to receive
/* USER CODE END PV */
- Blocking Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Receive(&hspi1, RX_Buffer, 1, 1000); //Receiving in Blocking mode
HAL_Delay(100);
/* USER CODE END 2 */
- Interrupt Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Receive_IT(&hspi1, RX_Buffer, 1); //Receiving in Interrupt mode
HAL_Delay(100);
/* USER CODE END 2 */
- DMA Mode
/* USER CODE BEGIN 2 */
HAL_SPI_Receive_DMA(&hspi1, RX_Buffer, 1); //Receiving in DMA mode
HAL_Delay(100);
/* USER CODE END 2 */
2.3.4. Compile and flash on slave board
2.4. Project workspace
The following table shows the connection between 2 Nucleo-L474RG boards for using SPI bus. It requires only three wires.
NUCLEO-L476RG MASTER | NUCLEO-L476RG SLAVE | Pin description |
---|---|---|
PA5 | PA5 | SCK |
PA6 | PA6 | MISO |
PA7 | PA7 | MOSI |
[[category:Getting_started_with_STM32_system_peripherals | 40]]