This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains what WDG is and how to use it through examples.
1. What is a HRTIM ?
HRTIM stands for High Resolution Timer. HRTIM is a highly accurate timer which can generate the complex waveform with highly very fine timing resolution.
1.1. HRTIM modes
1.2. Block diagram overview
As we can see on the figure below, the HRTIM have a modular architecture. Let's have a look at each block : - Block Timer : - Block Crossbar : - Block Output : - Block Input : - Block Interface :
2. Configure the HRTIM to generate multiple PWMs
2.1. Objective
2.2. Creating the project in STM32CubeIDE
2.3. Configure HRTIM
2.4. Generate project and edit main.c
2.5. Compile and flash
3. Configure the HRTIM to generate arbitrary waveform
3.1. Objective
3.2. Creating the project in STM32CubeIDE
3.3. Configure HRTIM
3.4. Generate project and edit main.c
3.5. Compile and flash
4. Configure the HRTIM to generate arbitrary waveform
4.1. Objective
4.2. Creating the project in STM32CubeIDE
4.3. Configure HRTIM
4.4. Generate project and edit main.c
4.5. Compile and flash
5. References