Getting started with DAC

Revision as of 17:46, 2 November 2022 by Registered User
Under construction.png Coming soon

This article explains what is DAC and how to use it through examples

1. DAC definition

Provide digital data to analog output conversion

1.1. Objective

• Learn how to setup DAC as wave generator in CubeMX • Generate Code in CubeMX and use HAL functions

1.2. How

Follow step by step work instructions:

Menu > File > New Project

Open Board Selector On Initialize all peripherals with their default Mode? > Select No Select Nucleo-L476RG

2. DAC Overview

2.1. What is DAC

2.2. Simplified Diagram

The DAC output can be buffered for low impedance loads Raw output from R-2R type resistor ladder DAC When unbuffered, the output is directly connected to the R 2-R resistor ladder network type of DAC The DAC support different input format: • 8-bit mode: Right aligned data input (on 16 bit data register) 8-bit + 8-bit data input for Dual channel mode

• 12-bit mode: Right aligned data input (on 16-bit data register) Left aligned data input (on 16-bit data register)

insert diagram

2.3. Low Power Mode

This is a feature available for extremely low power requirements.

insert figure []

3. Let's get started

3.1. Start a new project

File:step2.png

Note: After downloading the firmware package with STM32CubeMX, existing examples could be found at the following relative path : \STM32Cube\Repository\STM32Cube_FW_L4_V1.17.2\Projects\NUCLEO-L476RG\Examples\DAC and open them with STM32CubeMX. insert fig [] Search for DAC1 in the left search field Search for PA5 then click Reset_State Insert fig [] • If you want to start the project with a board, the LED pin is already selected (PA5 on NucleoL476RG. For other boards refer to the user manual), we can measure the output waveform on this pin. [] insert fig []


4. Test


[[category:Getting_started_with_STM32_system_peripherals | 15]] </noinclude