Getting started with I2C

Revision as of 17:14, 24 October 2022 by Registered User

This article explains what is the I2C and how to use it through examples


Objectives
Following this tutorial, you will:

  • Get familiar with the STM32L476RG Nucleo board,
  • Learn how to program and use a I2C

Hardware
The hardware requirements to start the application are the following:

  • 2 boards STM32L476RG [1]


1. I2C

I²C (Inter-Integrated Circuit) is a two-wire serial communication system used between integrated circuits which was originally created by Philips Semiconductors back in 1982.
The I2C is a multi-master, multi-slave, synchronous, bidirectional, half-duplex serial communication bus.

1.1. I2C Overview

  • SDA (Serial Data) is the line where master and slave send or receive the information (sequence of bit).
  • SCL (Serial Clock) is the line dedicated to the clock to synchronize the data flow.

i2c buq.png
SDA and SCL lines need to be pulled up with resistors. The value of these resistors depends on the bus length (the bus capacitance) and the transmission speed. The common value is 4.7kO. In any case, there are many guides to size them and we refer their reading to the more attentive reader.

1.2. I2C Modes

  • Standard-Mode (Sm) with a bit rate up to 100 kbit/s
  • Fast-Mode (Fm) with a bit rate up to 400 kbit/s
  • Fast-Mode Plus (Fm+) with a bit rate up to 1 Mbit/s

1.3. I2C Frame

i2c trame.png

-Start Condition (S)
-Stop Condition (P)
-Repeated Start (Restart) Condition (Sr)
-Acknowledge ACK (A)
-Not Acknowledge NACK (/A)

1.4. STM32 I2C Mode selectio

The interface can operate in one of the four following modes:

  • Slave transmitter
  • Slave receiver
  • Master transmitter
  • Master receiver

1.5. Examples I2C HAL functions

I2C in STM32 can be done in 3 methods.
1. Blocking Mode
2. Interrupt Mode
3. DMA Mode

Blocking mode :
The communication is performed in the polling mode.The status of all data processing is returned by the same function after finishing transfer.
No-Blocking mode :
The communication is performed using Interrupts or DMA. These functions return the status of the transfer startup.
The end of the data processing will be indicated through the dedicated I2C IRQ when using Interrupt mode or the DMA IRQ when using DMA mode.

- Blocking Mode:

HAL_I2C_Master_Transmit()
HAL_I2C_Master_Receive()
HAL_I2C_Slave_Transmit()
HAL_I2C_Slave_Receive()
HAL_I2C_Mem_Write()
HAL_I2C_Mem_Read()

- Interrupt Mode:

HAL_I2C_Master_Transmit_IT()
HAL_I2C_Master_Receive_IT()
HAL_I2C_Slave_Transmit_IT()
HAL_I2C_Slave_Receive_IT()
HAL_I2C_Mem_Write_IT()
HAL_I2C_Mem_Read_IT()


- DMA Mode:

HAL_I2C_Master_Transmit_DMA()
HAL_I2C_Master_Receive_DMA()
HAL_I2C_Slave_Transmit_DMA()
HAL_I2C_Slave_Receive_DMA()
HAL_I2C_Mem_Write_DMA()
HAL_I2C_Mem_Read_DMA()

2. Create the project in STM32CubeMX

NUCLEO-L476RG Board

  • STM32L476RG board Pinout

File:pinout.png

Create NUCLEO-L476RG UART project using STM32CubeMX

  • Create a new project using STM32CubeMX.
  • Select NUCLEO-L476RG MCU Selector.

File:mcu selector.png

  • Select I2C1
  • Select PB8: SCL and PB9: SDA for I2C1 if weren't selected

File:i2cinstance.PNG

CubeMX I2C configuration
Parameter Settings
File:parameterset.PNG - Set the I2C Mode Standard Mode and the I2C Frequency 100 KHz

  • GPIO Settings

- Tab>GPIO Settings

- Check Pull-UP

GPIO.PNG


- Check GPIO speed

Interrupt Mode only
- Tab>NVIC settings
- Enable interrupt
nvic.png

Project Manager

Set the project details for generation
- Menu > Project > Project Settings
- Set the project name
- Project location
- Type of toolchain
File:project.png




[[category:Getting_started_with_STM32_system_peripherals | 15]]