This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Board$:
Displayed 100 items.
- How to get Terminal (transclusion) (← links)
- Blktrace (transclusion) (← links)
- Ethtool (transclusion) (← links)
- Ifconfig (transclusion) (← links)
- Ltrace (transclusion) (← links)
- Tcpdump (transclusion) (← links)
- How to setup a WLAN connection (transclusion) (← links)
- IP Linux command line (transclusion) (← links)
- Wayland Weston overview (transclusion) (← links)
- I2C overview (transclusion) (← links)
- I2C i2c-tools (transclusion) (← links)
- IIO overview (transclusion) (← links)
- GDB (transclusion) (← links)
- WLAN overview (transclusion) (← links)
- How to use the IIO user space interface (transclusion) (← links)
- Strace (transclusion) (← links)
- Netstat (transclusion) (← links)
- Perf (transclusion) (← links)
- Sysstat tool suite (transclusion) (← links)
- LTTng (transclusion) (← links)
- Menuconfig or how to configure kernel (transclusion) (← links)
- Ftrace (transclusion) (← links)
- CAN overview (transclusion) (← links)
- Crypto API overview (transclusion) (← links)
- CEC overview (transclusion) (← links)
- How to debug Weston (transclusion) (← links)
- How to launch Khronos OpenGLES conformance tests (transclusion) (← links)
- How to launch glmark2 benchmark (transclusion) (← links)
- Serial TTY overview (transclusion) (← links)
- How to use TTY with User Terminal (transclusion) (← links)
- Pinctrl overview (transclusion) (← links)
- GPIOLib overview (transclusion) (← links)
- How to control a GPIO in userspace (transclusion) (← links)
- How to control a GPIO in kernel space (transclusion) (← links)
- STM32MP15 V4L2 camera overview (transclusion) (← links)
- STM32MP15 Evaluation boards - Starter Package (transclusion) (← links)
- How to use the kernel dynamic debug (transclusion) (← links)
- Watchdog overview (transclusion) (← links)
- Regulator overview (transclusion) (← links)
- PWM overview (transclusion) (← links)
- Pseudo filesystem (transclusion) (← links)
- How to cross-compile with the Developer Package (transclusion) (← links)
- Weston keyboard shortcuts (transclusion) (← links)
- Power overview (transclusion) (← links)
- Clock overview (transclusion) (← links)
- Dmesg and Linux kernel log (transclusion) (← links)
- V4l2-ctl (transclusion) (← links)
- Gst-play (transclusion) (← links)
- Netdata (transclusion) (← links)
- Gdbgui (transclusion) (← links)
- Gst-typefind (transclusion) (← links)
- Ethernet overview (transclusion) (← links)
- Kmemleak (transclusion) (← links)
- Sysprof (transclusion) (← links)
- Valgrind (transclusion) (← links)
- How to transfer a file over network (transclusion) (← links)
- ADC OpenSTLinux drivers (transclusion) (← links)
- How to find Linux kernel driver associated to a device (transclusion) (← links)
- Gst-discoverer (transclusion) (← links)
- Core dump (transclusion) (← links)
- Trace-cmd and kernelshark trace viewer (transclusion) (← links)
- Subpart - STM32MP1 - Starter Package (transclusion) (← links)
- STM32MP15 Discovery kits - Starter Package (transclusion) (← links)
- How to display on HDMI (transclusion) (← links)
- DAC Linux driver (transclusion) (← links)
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- Hardware random overview (transclusion) (← links)
- GStreamer troubleshooting grid (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- Configfs (transclusion) (← links)
- How to configure a WLAN interface on hotspot mode (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- How to set up a Bluetooth connection (transclusion) (← links)
- How to scan Bluetooth devices (transclusion) (← links)
- How to scan BLE devices (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- How to monitor the display framerate (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to control a RNG in userspace (transclusion) (← links)
- How to retrieve Cortex-M4 logs after crash (transclusion) (← links)
- How to monitor the GCNANO GPU load (transclusion) (← links)
- DRM KMS troubleshooting grid (transclusion) (← links)
- How to play audio (transclusion) (← links)
- Reading tips (transclusion) (← links)
- Debugfs (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)