- Last edited 8 months ago ago
Modify, rebuild and reload the Linux® kernel
![]() | ||||||
Develop on Arm® Cortex®-A7 | Develop on Arm® Cortex®-M4 | |||||
![]() |
Install the SDK | ![]() |
Create a simple hello-world application | ![]() |
Modify, rebuild and reload the Linux® kernel | ![]() |
1 Overview[edit]
This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then you will execute step by step procedures to modify, rebuild and reload the Linux® kernel.
2 Download OpenSTLinux BSP that includes the Linux® kernel source code[edit]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
- The OpenSTLinux BSP package is delivered through a tarball file named SOURCES-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.tar.xz for STM32MP157x-EV1
, STM32MP157x-DKx
and STM32MP135x-DK
boards.
- Download and install the STM32MP1 OpenSTLinux BSP package
STM32MP1 Developer Package - STM32MP1-Ecosystem-v4.0.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
cd <working directory path>/Developer-Package
tar xvf SOURCES-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.tar.xz |
Release note |
Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note.
|
3 Prepare the Linux® kernel source code[edit]
cd stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.15.24-stm32mp1-r1-r0
Extract the Linux® kernel source
tar xvf linux-5.15.24.tar.xz
Apply ST patches
cd linux-stm32mp-5.15.24-stm32mp1-r1-r0 for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Apply fragments
make ARCH=arm multi_v7_defconfig "fragment*.config" for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done yes '' | make ARCH=arm oldconfig
4 Build the Linux® kernel source code for the first time[edit]
- Build kernel images (uImage and vmlinux) and device tree (dtbs)
make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
- Build kernel module
make ARCH=arm modules
- Generate output build artifacts
mkdir -p $PWD/install_artifact/ make ARCH=arm INSTALL_MOD_PATH="$PWD/install_artifact" modules_install
5 Deploy the Linux® kernel on the board[edit]
5.1 Push the Linux® kernel onto the board[edit]
scp arch/arm/boot/uImage root@<board ip address>:/boot
5.2 Push the devicetree into the board[edit]
scp arch/arm/boot/dts/stm32mp1xx*.dtb root@<board ip address>:/boot
5.3 Push the kernel modules onto the board[edit]
- Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
rm install_artifact/lib/modules/5.15.24/build install_artifact/lib/modules/5.15.24/source
- Optionally, strip kernel modules (to reduce the size of each kernel modules)
find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
- Copy kernel modules
scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
- Using the Linux® console, regenerate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
/sbin/depmod -a
- Synchronize data on disk with memory
sync
5.4 Reboot the board[edit]
reboot
6 Modify a built-in Linux® kernel device driver[edit]
This simple example adds unconditional log information when the display driver is probed.
- Using the Linux® console, check that there is no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the Linux® kernel source directory
cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.15.24-stm32mp1-r1-r0/linux-stm32mp-5.15.24-stm32mp1-r1-r0
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function as follows
static int stm_drm_platform_probe(struct platform_device *pdev)
{
struct device *dev = &pdev->dev;
struct drm_device *ddev;
int ret;
[...]
DRM_INFO("Simple example - %s\n", __func__);
return 0;
[...]
}
- Save the file
- Rebuild the Linux® kernel
make uImage LOADADDR=0xC2000040
- Update the Linux kernel image into board
scp arch/arm/boot/uImage root@<board ip address>:/boot
- Reboot the board
reboot
- Check that log information is now present when the display driver is probed
dmesg | grep -i stm_drm_platform_probe [ 2.764080] [drm] Simple example - stm_drm_platform_probe
![]() |
![]() |
![]() |