Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
<bookshelf src="Book:Getting started" /> | <bookshelf src="Book:Getting started" /> | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
{| class="st-table" style="text-align:center; margin: auto" | {| class="st-table" style="text-align:center; margin: auto" | ||
| colspan="7" style="border-style: hidden;" | [[Image:STM32MP157C-EV1.png | 65px | link=]] | | colspan="7" style="border-style: hidden;" | [[Image:STM32MP157C-EV1.png | 65px | link=]] | ||
Line 16: | Line 20: | ||
<br> | <br> | ||
{{:Modify, rebuild and reload the Linux® kernel}} | {{#lst:Modify, rebuild and reload the Linux® kernel|STM32MP1}} | ||
<br> | <br> | ||
Line 29: | Line 33: | ||
__NOTOC__ | __NOTOC__ | ||
[[Category:STM32MP157x-EV1 - develop on A7 | 03]] | [[Category:STM32MP157x-EV1 - develop on A7 | 03]] | ||
{{PublicationRequestId | | {{PublicationRequestId |19661|2021-04-20}} | ||
</noinclude> | </noinclude> |
Latest revision as of 17:47, 14 December 2023
1. Overview[edit | edit source]
This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then you will execute step by step procedures to modify, rebuild and reload the Linux® kernel.
2. Download OpenSTLinux BSP that includes the Linux® kernel source code[edit | edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
- The OpenSTLinux BSP package is delivered through a tarball file named SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz applicable for all STM32 microprocessor series.
- Download and install the STM32MPU OpenSTLinux BSP package.
STM32MPU Developer Package - STM32MPU ecosystem v6.1.0 release | |
---|---|
Download |
|
Installation |
<working directory path>/Developer-Packagecd
tar xvf SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz
|
Release note |
Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note.
|
cd stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/linux-stm32mp-6.6.78-stm32mp-r2-r0
3. Prepare the Linux® kernel source code[edit | edit source]
Extract the Linux® kernel source
tar xvf linux-6.6.78.tar.xz
Apply ST patches
cd linux-6.6.78
for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
- Configure build directory
export OUTPUT_BUILD_DIR=$PWD/../build
mkdir -p ${OUTPUT_BUILD_DIR}
- Apply fragments
make O="${OUTPUT_BUILD_DIR}" defconfig fragment*.config
for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O ${OUTPUT_BUILD_DIR} ${OUTPUT_BUILD_DIR}/.config $f; done
(yes '' || true) | make oldconfig O="${OUTPUT_BUILD_DIR}"
4. Build the Linux® kernel source code for the first time[edit | edit source]
![]() |
Building the kernel for the first time can take several minutes. |
Build kernel images (uImage and vmlinux) and device tree (dtbs):
make uImage vmlinux dtbs LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
export IMAGE_KERNEL="uImage"
- Build kernel module
make modules O="${OUTPUT_BUILD_DIR}"
- Generate output build artifacts
make INSTALL_MOD_PATH="${OUTPUT_BUILD_DIR}/install_artifact" modules_install O="${OUTPUT_BUILD_DIR}"
mkdir -p ${OUTPUT_BUILD_DIR}/install_artifact/boot/
cp ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/${IMAGE_KERNEL} ${OUTPUT_BUILD_DIR}/install_artifact/boot/
find ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/dts/ -name 'st*.dtb' -exec cp '{}' ${OUTPUT_BUILD_DIR}/install_artifact/boot/ \;
5. Deploy the Linux® kernel on the board[edit | edit source]
5.1. Push the Linux® kernel and the devicetree onto the board[edit | edit source]
cd ${OUTPUT_BUILD_DIR}/install_artifact
scp -r boot/* root@<ip of board>:/boot/
5.2. Push the kernel modules onto the board[edit | edit source]
- Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
rm lib/modules/6.6.78/build
- Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
- Copy kernel modules
scp -r lib/modules/* root@<ip of board>:/lib/modules
- Using the Linux® console, regenerate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
/sbin/depmod -a
- Synchronize data on disk with memory
sync
5.3. Reboot the board[edit | edit source]
reboot
6. Modify a built-in Linux® kernel device driver[edit | edit source]
This simple example adds unconditional log information when the display driver is probed.
- Using the Linux® console, check that there is no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the Linux® kernel source directory
cd $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/linux-stm32mp-6.6.78-stm32mp-r2-r0/linux-6.6.78
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function as follows
DRM_INFO("Simple example - %s\n", __func__); return 0; [...] }static int stm_drm_platform_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct drm_device *ddev; int ret; [...]
- Save the file
- Rebuild the Linux® kernel
make uImage LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
- Update the Linux kernel image into board
scp ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/uImage root@<board ip address>:/boot
- Reboot the board
reboot
- Check that log information is now present when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
[ 2.764080] [drm] Simple example - stm_drm_platform_probe