Registered User m (Assignment tables reviewed with architects) |
Registered User mNo edit summary Tag: 2017 source edit |
||
(9 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x | |MPUs list=STM32MP13x, STM32MP25x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |MPUs checklist=STM32MP13x,STM32MP15x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
Line 30: | Line 30: | ||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | | <span title="assigned peripheral" style="font-size:21px">☑</span> | ||
| | | | ||
| | | ROM code allocation is managed with the [[STM32MP13_OTP_mapping|bit 7 in OTP 9]] | ||
|- | |- | ||
<section end=stm32mp13_boottime /> | <section end=stm32mp13_boottime /> | ||
|} | |||
====On {{MicroprocessorDevice | device=25}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | |||
<section begin=stm32mp25_a35_boottime /> | |||
| rowspan="1" | Security | |||
| rowspan="1" | [[SAES internal peripheral | SAES]] | |||
| SAES | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | |||
| ROM code allocation is managed with the [[STM32MP25_OTP_mapping|bit 8 in OTP 16]] | |||
|- | |||
<section end=stm32mp25_a35_boottime /> | |||
|} | |} | ||
Line 46: | Line 60: | ||
| Assignment (single choice) | | Assignment (single choice) | ||
|-<section end=stm32mp13_runtime /> | |-<section end=stm32mp13_runtime /> | ||
|} | |||
====On {{MicroprocessorDevice | device=25}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp25_runtime}} | |||
<section begin=stm32mp25_a35_runtime /> | |||
| rowspan="1" | Security | |||
| rowspan="1" | [[SAES internal peripheral | SAES]] | |||
| SAES | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span><sup>OP-TEE</sup> | |||
| <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | |||
| | |||
| | |||
|- | |||
<section end=stm32mp25_a35_runtime /> | |||
|} | |} | ||
Line 52: | Line 82: | ||
* '''Linux<sup>®</sup>''': [[Crypto_API_overview|crypto framework]] | * '''Linux<sup>®</sup>''': [[Crypto_API_overview|crypto framework]] | ||
* '''OP-TEE''': [[OP-TEE_overview|SAES driver]] and {{CodeSource | OP-TEE_OS | core/include/crypto/crypto.h | Cryptographic Provider API (CP API)}} | * '''OP-TEE''': [[STM32 MPU OP-TEE_overview|SAES driver]] and {{CodeSource | OP-TEE_OS | core/include/crypto/crypto.h | Cryptographic Provider API (CP API)}} | ||
* '''TF-A BL2''': [[TF-A_overview|SAES driver]] | * '''TF-A BL2''': [[TF-A_overview|SAES driver]] | ||
Latest revision as of 16:12, 25 July 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the SAES peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The SAES peripheral provides hardware acceleration to encrypt or decrypt data using the AES[1] algorithms. It supports two key sizes (128 bits and 256 bits) and different chaining modes. It incorporates protections against differential power analysis (DPA) and the related side-channel attacks.
Refer to the STM32MP13 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP13x lines
[edit | edit source]
The SAES instance is used to decrypt the firmware.
Click on the right to expand the legend...
Domain | Peripheral | Boot time allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Security | SAES | SAES | ☐ | ☑ | ROM code allocation is managed with the bit 7 in OTP 9 |
3.1.2. On STM32MP25 unknown microprocessor device[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Security | SAES | SAES | ☐ | ☑ | ⬚ | ROM code allocation is managed with the bit 8 in OTP 16 |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Security | SAES | SAES | ☐ | ⬚ | Assignment (single choice) |
3.2.2. On STM32MP25 unknown microprocessor device[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Security | SAES | SAES | ☐OP-TEE | ⬚ | ☐ | ⬚ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the SAES peripheral for the embedded software components listed in the above tables.
- Linux®: crypto framework
- OP-TEE: SAES driver and Cryptographic Provider API (CP API)
- TF-A BL2: SAES driver
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
6. References[edit | edit source]