Last edited 2 years ago

X-LINUX-AI OpenSTLinux Expansion Package



cente

X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). It is composed of an OpenEmbedded meta layer, named meta-st-stm32mpu-ai, to be added on top of the STM32MP1 Distribution Package. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices.

AI Expansion Package In STM32MPU Embedded Software.png

1. X-LINUX-AI v3.0.0[edit source]

1.1. Contents[edit source]

  • Application support for the 720p, 480p, and 272p display configurations
  • New.png Python application camera pipeline update to use GtkWaylandsink and achieve better performance
  • X-LINUX-AI SDK add-on extending the OpenSTLinux SDK with AI functionality to develop and build an AI application easily. The X-LINUX-AI SDK add-on provides support for all the above frameworks. It is available from the X-LINUX-AI product page

1.2. Validated hardware[edit source]

As any software expansion package, the X-LINUX-AI is supported on all STM32MP1 Series and it has been validated on the following boards:

  • STM32MP157F-DK2[6]
  • STM32MP157F-EV1[7]

1.3. Software structure[edit source]

X-LINUX-AI v2.1.0 Expansion Package Software structure

2. Starter package: install from the OpenSTLinux AI package repository[edit source]

All the generated X-LINUX-AI packages are available from the OpenSTLinux AI package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AI.

This repository contains AI packages that can be simply installed using apt-* utilities, which the same as those used on a Debian system:

  • the main group contains the selection of AI packages whose installation is automatically tested by STMicroelectronics
  • the updates group is reserved for future uses such as package revision update.

You can install them individually or by package group.

2.1. Prerequisites[edit source]

  • Flash the Starter Package on your SDCard
For OpenSTLinux ecosystem release v4.1.0 More info.png :
STM32MP157x-DKx Starter Package procedure
or
STM32MP157x-EV1 Starter Package procedure
  • Your board has an internet connection either through the network cable or through a WiFi connection.

2.2. Configure the AI OpenSTLinux package repository[edit source]

Once the board is booted, execute the following command in the console in order to configure the AI OpenSTLinux package repository:


For ecosystem release   v4.1.0 More info.png :
 wget http://extra.packages.openstlinux.st.com/AI/4.1/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb
 dpkg -i apt-openstlinux-ai_1.0_armhf.deb 

Then synchronize the AI OpenSTLinux package repository.

 apt-get update

2.3. Install AI packages[edit source]

2.3.1. Install all X-LINUX-AI packages[edit source]

Command Description
apt-get install packagegroup-x-linux-ai
Install all the X-LINUX-AI packages (TensorFlow™ Lite, Edge TPU™, application samples and tools)

2.3.2. Install AI framework related packages[edit source]

2.3.3. Install individual packages[edit source]

3. Developer package: build AI application from the X-LINUX-AI add-on SDK[edit source]

In order to easily develop and build an AI application without using the Yocto build system, X-LINUX-AI comes with a SDK add-on extending the OpenSTLinux SDK with AI functionality.

All the needed information to install and use the X-LINUX-AI SDK add-on can be found in the following article : How to install and use the X-LINUX-AI SDK add-on

4. Distribution package: re-generate X-LINUX-AI OpenSTLinux distribution[edit source]

With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.
This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.

4.1. Download the STM32MP1 Distribution Package[edit source]

For ecosystem release v4.1.0 More info.png :
Install the STM32MP1 Distribution Package v4.1.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).

4.2. Install X-LINUX-AI environment[edit source]

  • Clone the meta-st-stm32mpu-ai git repositories
For X-LINUX-AI v3.0.0:
 cd <Distribution Package installation directory>/layers/meta-st
 git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-ai.git -b v3.0.0
  • For a new environment
  • For an already installed environment

4.3. Build the image[edit source]

 bitbake st-image-ai

4.4. Flash the built image[edit source]

Follow this link to see how to flash the built image.

5. How to use the X-LINUX-AI Expansion Package[edit source]

5.1. Material needed[edit source]

To use the X-LINUX-AI OpenSTLinux Expansion Package, choose one of the following materials:

  • STM32MP157F-DK2[6] + an UVC USB WebCam
  • STM32MP157F-EV1[7] with the built in OV5640 parallel camera

Optional:

  • Coral USB Edge TPU™[3] accelerator

5.2. Boot the OpenSTlinux Starter Package[edit source]

At the end of the boot sequence, the demo launcher application appears on the screen.

Demo launcher appearance when X-LINUX-AI is not installed

5.3. Install the X-LINUX-AI[edit source]

After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.

 apt-get install packagegroup-x-linux-ai

And restart the demo launcher:

 systemctl restart weston-launch

Check that X-LINUX-AI is properly installed:

 x-linux-ai -v
X-LINUX-AI version: v3.0.0

5.4. Launch an AI application sample[edit source]

Once the demo launcher is restarted, notice that it is slightly different because new AI application samples have been installed.
The demo launcher has the following appearance, and you can navigate into the different screens by using the NEXT or BACK buttons.

Demo launcher appearance when X-LINUX-AI is installed

The demo launcher now contain AI application samples that are described within dedicated article available in the X-LINUX-AI application samples zoo page.

5.5. Enjoy running your own NN models[edit source]

The above examples provide application samples to demonstrate how to execute models easily on the STM32MP1.

You are free to update the C/C++ application or Python scripts for your own purposes, using your own NN models.

Source code locations are provided in application sample pages.

6. References[edit source]


7. Archives Archive box.png[edit source]

X-LINUX-AI release Release note
X-LINUX-AI v2.2.0 X-LINUX-AI_OpenSTLinux_Expansion_Package_-_v2.2.0#X-LINUX-AI_v2-2-0
X-LINUX-AI v2.1.1 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-1 page for the v3 ecosystem releases (in archived wiki)
X-LINUX-AI v2.1.0 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-0 page for the v2 ecosystem releases (in archived wiki)
X-LINUX-AI v2.0.0 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-0-0 page for the v2 ecosystem releases (in archived wiki)