This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. STM32PRGFW-UTIL overview[edit source]
This article describes STM32PRGFW-UTIL, an official STMicroelectronics firmware package for One-time Programmable (OTP) management.
1.1. Applicability[edit source]
The STM32PRGFW-UTIL applies to STM32MP13x linesĀ and STM32MP15x linesĀ
.
1.2. Package overview[edit source]
STM32PROGFW-UTIL provides multiple applications to manage the One-time Programmable (OTP) memories.
- Functionalities are available through 4 applications
- STM32CubeProgrammer based application
- Standalone STM32CubeIDE based application
- 2 other applications for development purpose
- UART configuration for the Standalone application
- Run mode for STM32CubeProgrammer application
- Features
- STM32CubeProgrammer based application (in Serial boot mode)
- OTP v2 structure
- STM32CubeProgrammer UART interface and USB DFU
- OTP Console based application (in Dev boot mode)
- OTP CLI implemented based on STM32CubeProgrammer OTP CLI with OTP v2 structure
- UART and STM32CubeIDE Semihosting interface
- STM32CubeProgrammer based application (in Serial boot mode)
1.3. README.md[edit source]
The README.md, included in the package, is a complete document that describes:
- the Software architecture and design of STM32PRGFW-UTIL.
- how to use the STM32PRGFW-UTIL firmware package
2. How to get STM32PRGFW-UTIL[edit source]
Refer to the following link to find STM32PRGFW-UTIL firmware package.