This article describes the content of OpenSTLinux distribution software release version openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23, which is part of the STM32 MPU ecosystem release note - v4.1.0.
1. Intended audience[edit source]
The targeted audience is STM32MP13x lines and STM32MP15x lines
customers or partners.
2. Delivery scope and purpose[edit source]
The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution. This delivery of OpenSTLinux distribution is part of STM32 MPU Ecosystem v4.1.0 (see the STM32 MPU ecosystem release note - v4.1.0).
3. Licensing[edit source]
This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).
All packages use the same source components. All components and their respective licenses are listed here.
4. Supported hardware[edit source]
This software delivery is compatible with the following boards:
STM32MP13 boards | |||
---|---|---|---|
Boards | PCBs list | Main features | Ordering |
![]() STM32MP135F-DK Discovery kit |
|
STM32MP15 boards | |||
---|---|---|---|
Boards | PCBs list | Main features | Ordering |
![]() STM32MP157D-DK1 Discovery kit |
|
||
![]() STM32MP157F-DK2 Discovery kit |
|
||
![]() STM32MP157D-EV1 Evaluation board |
|
||
![]() STM32MP157F-EV1 Evaluation board |
|
||
![]() STM32MP157A-DK1 Discovery kit |
|
Out of production | |
![]() STM32MP157C-DK2 Discovery kit |
|
Out of production | |
![]() STM32MP157A-EV1 Evaluation board |
|
Out of production | |
![]() STM32MP157C-EV1 Evaluation board |
|
Out of production |
5. Release content[edit source]
5.1. Main software components[edit source]
- Build process
- OpenEmbedded v4.0.4 (Kirkstone) - Updated
- GCC version v11.3.0 - Updated
- Embedded software components
- Applicative components
- Weston version v10.0.2 - Updated
- Wayland version 1.20.0
- GStreamer version v1.20.3 - Updated
- GCnano version v6.4.9 - Updated
5.2. Changes[edit source]
5.2.1. OpenSTLinux layers[edit source]
Changes are:
- Rebase on Yocto LTS Release 4.0.4 (Kirkstone)
- Add support of Firmware Update feature for NAND memory
- Add Arm® Cortex®-A7 and Arm® Cortex®-M4 examples in Starter Package for STM32MP157D-DK1
- Move Arm® Cortex®-A7 and Arm® Cortex®-M4 examples from STM32MP157C-DK2
to STM32MP157F-DK2
- Increase default rootfs ext4 partition size: 3GB for eMMC and 4GB for Micro SD Card
- Minor fixes
5.2.2. Linux® kernel[edit source]
New component release tag 5.15-stm32mp-r2 is available, rebased on official Linux® kernel v5.15.67.
Changes are:
- Real Time ready drivers (RT-Linux)
- SPI slave support
- ADC oversampling support
- SPI master driver with dual-qspi mode support
- DMA support for CRYP IP (Crypto performance improvement)
- STM32MP13x lines
:
- New wake up sources
- USB OTG wake up via STM32G0
- Ethernet PHY Wakeup on LAN
- New wake up sources
- Minor fixes
5.2.3. U-Boot[edit source]
New component release tag 2021.10-stm32mp-r2 is available, rebased on official U-Boot v2021.10.
Changes are:
- Fix support of STM32MP13x Rev.Y
- Device tree alignment with Linux Kernel v5.15-stm32mp-r2
- Remove tests on CONFIG_DM_REGULATOR
- Fix invalid clock name references in SCMI driver
- Make usage of clock/reset bulk() API in USB EHCI driver
- Fix the display of protected GPIO in gpio and pinmux command
- Display label for gpio in alternate mode in gpio status command
- Fixes for stm32prog command:
- Several fixes for STM32MP13 clock
- Use correct compatible string to add MTD partitions int ft_board_setup()
- Check fdtcontroladdr in label_boot for pxe command parsing, used on extlinux.conf for GENERIC DISTRO support
- Use RGB565 for BMP blitting, as panel configuration
- Several STM32 I2C corrections
- Other minor updates
5.2.4. TF-A[edit source]
New component release tag 2.6-stm32mp-r2 is available, rebased on official TF-A v2.6.
Changes are:
- Firmware update on NAND devices
- Improve FIP management on NAND devices
- Add GPIO regulators driver
- Use FCONF to manage the Chain of Trust
- Allow support of non-paged OP-TEE
- Skip boot devices initialization when returning from Standby (only with OP-TEE)
- Minor fixes
5.2.5. OP-TEE[edit source]
New component release tag 3.16.0-stm32mp-r2 is available, rebased on official OP_TEE OS 3.16.0.
Changes are:
- ADC driver implementation
- IRQ forwarding
- Update regulator IO management
- Hardware unique key (HUK) implementation:
- Minor Fixes
6. Release change notification[edit source]
OpenSTLinux attention points to switch from ecosystem release v4.0.0 to ecosystem release v4.1.0
are documented in STM32 MPU OpenSTLinux release changes notification – v4.1.0 article.
7. Recommendations for use[edit source]
7.1. Safe use[edit source]
- Flash programming and boot from all supported flash devices: SDCard, eMMC, ONFI NAND and NOR flash memories.
- Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery.
- Develop coprocessor Cube applications based on STM32CubeMP1 delivery.
- Develop boards based on STM32MP1 Series.
- Prototype applications based on ST boards.
7.2. Non-recommended use[edit source]
- None
8. Restrictions[edit source]
- If Firmware Update is not enabled, and the flashlayout partition is not needed anymore, but the storage mapping is hardcoded in U-Boot; either the flashlayout keeps the partitions for Firmware Update feature or U-Boot needs to be updated.
9. Minor release updates[edit source]
STMicroelectronics regularly delivers corrections through github® components which are U-Boot, OP-TEE, TF-A, Linux kernel.
The corrections can be incorporated into the Developer Package (refer to STM32MP1 Developer Package) or Distribution Package (see below).
Two possibilities exist to update a Distribution Package:
- Update your existing Distribution Package:
- Switch your Distribution Package to # github® mode .
- Use the devtool modify <recipe name> command to set up an environment. It fetches and unpacks the source code.
- In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
- More rarely STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MP1 Distribution Package environment. See below the github® links of the quoted layers :
- Get a new Distribution Package:
- Refer to Installing_the_OpenSTLinux_distribution page for install instructions, and use the repo command given for the minor version below, if it exists.
9.1. v4.1.2[edit source]
- Update to Yocto Project 4.0.19 (2022-04.19-kirkstone)
- Update to Linux Kernel 5.15.145
- BSP maturation with an amount of 17 fixes delivered BSP components (TF-A, u-Boot, OP-TEE and Linux Kernel)
- BSP update:
Layer name | github® commit SHA1 reference |
---|---|
meta-st-stm32mp | b7accec80a2903c75d4129cf2b3bf6e15f5410c0 |
meta-st-openstlinux | 613b158e6ee5b575e7de1251eae389c72e376043 |
- Component update:
Component | Recipe name | new github® release |
---|---|---|
tf-a | tf-a-stm32mp | v2.6-stm32mp-r2.2 |
u-boot | u-boot-stm32mp | v2021.10-stm32mp-r2.2 |
kernel | linux-stm32mp | v5.15-stm32mp-r2.2 |
optee-os | optee-os-stm32mp | 3.16.0-stm32mp-r2.2 |
- New manifest tag available to get the release: openstlinux-5.15-yocto-kirkstone-mp1-v24.07.17
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v24.07.17 repo sync
9.2. v4.1.1[edit source]
- Update to Yocto Project 4.0.11 (2022-04.11-kirkstone)
- Update to Linux Kernel 5.15.118
- BSP maturation with an amount of 49 fixes delivered BSP components (TF-A, u-Boot, OP-TEE and Linux Kernel)
- BSP update:
Layer name | github® commit SHA1 reference |
---|---|
meta-st-stm32mp | ef4a6a785d17b4370cd20402b351a17ed34cd74d |
meta-st-openstlinux | 03daeb62ccffa2e29c20ee97154dc18dda4fbd60 |
- Component update:
Component | Recipe name | new github® release |
---|---|---|
tf-a | tf-a-stm32mp | v2.6-stm32mp-r2.1 |
u-boot | u-boot-stm32mp | v2021.10-stm32mp-r2.1 |
kernel | linux-stm32mp | v5.15-stm32mp-r2.1 |
optee-os | optee-os-stm32mp | 3.16.0-stm32mp-r2.1" |
- New manifest tag available to get the release: openstlinux-5.15-yocto-kirkstone-mp1-v23.07.26
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v23.07.26 repo sync
10. How to get started with openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23[edit source]
Refer to How to download the software and start with this release?
11. Associated tools[edit source]
Refer to the Referenced tools release notes .
12. Yocto features enabled in the delivery[edit source]
OpenEmbedded[3] build framework engine is named OE-Core.
OpenSTLinux distribution is based on the build framework OpenEmbedded, and can be configured thanks to a mechanism named "features" (machine features, distribution features, ...).
Depending on the features enabled, the resulting distribution can have more capabilities or software embedded.
For example, if the wifi is enabled then the wifi software and drivers are present on the filesystem and the wifi can be used.
12.1. Machine features[edit source]
The variable MACHINE_FEATURES specifies the list of hardware features the machine is capable of supporting.
These features (MACHINE_FEATURES) are defined inside the machine configuration .
Machine feature | Purpose |
---|---|
alsa | Include ALSA support (OSS compatibility kernel modules installed if available). |
autoresize | Add support of autoresize through InitRD |
bluetooth | Add Broadcom43430 (Bluetooth) firmware to the filesystem (STM32MP135x-DK Discovery kit ![]() ![]() |
ext2 | Add Second Extended File System support |
fip | Enable Firmware In Package (FIP) packaging format |
fw-update | Enable Firmware update feature |
gpu | Add GPU support (if EULA is accepted) (STM32MP157 line ![]() |
initrd | Enable Intial ramdisk building |
m4copro | Add m4projects to userfs (STM32MP15x lines ![]() |
optee | Add OP-TEE Secure part |
pci | Add Peripheral Component Interconnect peripheral support |
rtc | Add Real Time Clock peripheral support |
screen | Add display screen peripheral support |
splashscreen | Add splashscreen to U-Boot |
tpm2 | Add Trusted Platform Module peripheral support |
usbg0 | Add G0 Firmware for USB support |
usbgadget | Enable USB Gadget feature |
usbhost | Enable USB Host feature |
watchdog | Add watchdog support and binaries |
wifi | Add Broadcom43430 (wifi) firmware to the filesystem (STM32MP135x-DK Discovery kit ![]() ![]() |
12.2. Distribution features[edit source]
The variable DISTRO_FEATURES specifies the list of software features present in the distribution.
These features (DISTRO_FEATURES) are defined inside the distribution configuration .
Distribution feature | Purpose |
---|---|
alsa | Include ALSA support (OSS compatibility kernel modules installed if available). |
argp | |
autoresize | Add support of userfs auto resize feature in OpenSTLinux |
bluetooth | Include Bluetooth support |
bluez5 | Add Bluetooth stack |
efi | Add userland EFI tools |
ext2 | Add Second Extended File System support |
ext4 | Add Fourth Extended File System support |
gobject-introspection-data | Enable GObject Introspection, project for providing machine readable introspection data of the API of C libraries. |
gplv3 | Add gplv3 binaries in OpenSTLinux |
gstreamer | Add gstreamer tools in filesystem |
initrd | Add ramdisk |
ipv4 | Add ipv4 support |
ipv6 | Add ipv6 support |
kde | Add several tools (e.g. cups, fontconfig, ...) to the filesystem |
largefile | Enable large file support |
ldconfig | Include support for ldconfig and ld.so.conf on the target |
multiarch | Enable 64 bits BFD (Binary File Descriptor) |
nfs | Include NFS client support (for mounting NFS exports on device). |
opengl | Include the Open Graphics Library |
optee | Install tee service on the filesystem |
pam | Enable Pluggable Authentication Module |
pci | Add pci support |
polkit | Enable PolicyKit for controlling system-wide privileges |
pulseaudio | Network-capable sound server program |
splashscreen | Add U-Boot splashscreen |
systemd | Use systemd as init service |
usbgadget | USB Gadget Device support (for USB networking/serial/storage) |
usbhost | USB Host support (allows to connect external keyboard, mouse, storage, network etc) |
wayland | Add Wayland support |
wifi | WiFi support |
xattr | Add "Extended Attributes" support for filesystem |
zeroconf | Add zeroconf package to set up a ad-hoc network |
12.3. Bootscheme labels[edit source]
The variable BOOTSCHEME_LABELS defines which kind of boot is supported on the board.
These settings (BOOTSCHEME_LABELS) are defined inside the machine configuration .
Bootscheme label | Purpose |
---|---|
optee | Add optee in bootscheme |
trusted | Add trusted in bootscheme |
12.4. Bootdevice labels[edit source]
The variable BOOTDEVICE_LABELS defines which kind of mass storage OpenSTLinux can programmed.
These settings (BOOTDEVICE_LABELS ) are defined inside the machine configuration .
Bootdevice label | Purpose |
---|---|
emmc | Add boot on emmc device |
nand-4-256 | Add boot on NAND device |
nor-sdcard | Add boot stage on NOR device and the filesystem on SD-Card |
sdcard | Add boot on SD-Card |