This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The embedded software distributions[1] supported for the STM32MP135x-DK Discovery kits are listed below.
For each distribution, up to three software Packages are delivered:
- the Starter Package (software image)
- the Developer Package (SDK for cross-development, source code for the BSP of the distribution)
- the Distribution Package (build framework on Linux® host PC, source code for the whole distribution)
![]() | ||
![]() Linux Yocto-based Starter Package for STM32MP13 Discovery kits |
![]() Linux Yocto-based Developer Package for STM32MP1 Series |
![]() Linux Yocto-based Distribution Package for STM32MP1 Series |
![]() | ||
![]() Linux Buildroot-based Distribution Package for STM32MP1 Series |
- ↑ The STM32 MPU ecosystem release note details the latest delivered embedded software distributions
- ↑ The Which STM32MPU Embedded Software Package better suits your needs article provides hints for selecting the most appropriate Package.