This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Wayland logs
To get the logs of the wayland protocol messages, set this environment variable:
export WAYLAND_DEBUG=1
2. Saving Weston logs in a file
Standard Weston logs are available in the /home/weston/weston.log file when Weston is started with the "weston user" using the systemd service.
cat /home/weston/weston.log
3. Displaying Weston logs on a console
Start Weston with the following command:
weston --tty=1 &
All Weston logs are then displayed on the console.