1. Article purpose[edit source]
The purpose of this article is to explain how to perform a secure boot on a STM32MP device with the Distribution package.
To perform this use-case you need to:
- Create signature key with KeyGen tool (if not already done)
- Put signature key on STM32MP (if not already done)
- Compile a Distribution package with signed FIP
- Sign first stage bootloader binaries with Signing tool
- Create FlashLayout for signed binaries
- Program and test
- Close the device (if not already done)
You must proceed step-by-step (you cannot roll back).
2. Creating signature key[edit source]
To perform the Secure Boot, you need to have binaries signed with a specific signature key.
If this signature key is already present on the STM32MP device, go directly to Distribution package with signed FIP.
To create the signature key, you must use the STM32MP KeyGen CLI Tool.
See KeyGen tool page for installation and command-line options.
The minimal command to use is:
-abs <output directory> -pwd <password> -n <number of key>STM32MP_KeyGen_CLI
With:
- <output directory> = patch to the generated private and public key files (privateKey.pem and publicKey*.pem)
- <password> = Password of the private key. The password must contain 4 characters at least.
- <number of key> = number of key pairs, 1 for STM32MP15 or 8 for stm32MP13
2.1. Creating signature key for STM32MP15x lines
[edit source]
STM32MP15x lines device supports only one signature key pair (Public key / Private Key)
Example:
AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 0 generated successfully. + public key: /tmp/key/publicKey00.pem + private key: /tmp/key/privateKey00.pem + public hash key: /tmp/key/publicKeyHash00.bin ------------------------------------------------------------ Hash of table of Hash of {algorithm + public Key} file generated successfully. + Hash Hash: /tmp/key/publicKeysHashHashes.binSTM32MP_KeyGen_CLI -abs stm32mp15-key/ -pwd azerty -n 1 ------------------------------------------------------------------- STM32MP Key Generator v1.0.0 ------------------------------------------------------------------- Prime256v1 curve is selected.
2.2. Creating signature key for STM32MP13x lines
[edit source]
STM32MP13x lines device supports up to 8 signature key pairs (Public key / Private Key)
Example:
STM32MP_KeyGen_CLI -abs stm32mp13-key/ -pwd azerty -n 8
AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 0 generated successfully. + public key: /tmp/key/publicKey00.pem + private key: /tmp/key/privateKey00.pem + public hash key: /tmp/key/publicKeyHash00.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 1 generated successfully. + public key: /tmp/key/publicKey01.pem + private key: /tmp/key/privateKey01.pem + public hash key: /tmp/key/publicKeyHash01.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 2 generated successfully. + public key: /tmp/key/publicKey02.pem + private key: /tmp/key/privateKey02.pem + public hash key: /tmp/key/publicKeyHash02.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created must be signed with Keys packet 3 generated successfully. + public key: /tmp/key/publicKey03.pem + private key: /tmp/key/privateKey03.pem + public hash key: /tmp/key/publicKeyHash03.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 4 generated successfully. + public key: /tmp/key/publicKey04.pem + private key: /tmp/key/privateKey04.pem + public hash key: /tmp/key/publicKeyHash04.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 5 generated successfully. + public key: /tmp/key/publicKey05.pem + private key: /tmp/key/privateKey05.pem + public hash key: /tmp/key/publicKeyHash05.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 6 generated successfully. + public key: /tmp/key/publicKey06.pemsoc + private key: /tmp/key/privateKey06.pem + public hash key: /tmp/key/publicKeyHash06.bin ------------------------------------------------------------ AES_256_cbc algorithm is selected for private key encryption Generating Prime256v1 keys... Private key PEM file created Public key PEM file created public key hash file created Keys packet 7 generated successfully. + public key: /tmp/key/publicKey07.pem + private key: /tmp/key/privateKey07.pem + public hash key: /tmp/key/publicKeyHash07.bin ------------------------------------------------------------ Hash of table of Hash of {algorithm + public Key} file generated successfully. + Hash Hash: /tmp/key/publicKeysHashHashes.bin------------------------------------------------------------------- STM32MP Key Generator v1.0.0 ------------------------------------------------------------------- Prime256v1 curve is selected.
3. Creating encryption key[edit source]
3.1. Creating encryption key for STM32MP13x lines
[edit source]
To perform Secure Boot with encrypted binaries, you must have binaries encrypted with a specific encryption key.
If this signature key is already present on the STM32MP device, go directly to Distribution package with signed FIP.
To create an encryption key, you must generate a random key of 16 bytes'.
On Linux PC:
dd if=/dev/random of=stm32mp13_encryption_key.bin bs=1 count=16
On Linux with STM32MP_KeyGen_CLI:
STM32MP_KeyGen_CLI.exe -rand 16 stm32mp13_encryption_key.bin
On Windows with STM32MP_KeyGen_CLI:
STM32MP_KeyGen_CLI.exe -rand 16 stm32mp13_encryption_key.bin
4. Put signature key on STM32MP[edit source]
4.1. Put the hash key on the device for STM32MP15x lines
[edit source]
To manually put the public key hash (PKH) on the STM32MP device with a U-Boot stm32key command, you need to:
- Put the Public Key Hash' file (publicKeyhash.bin), generated in the previous section, on bootfs partition
- Boot the board and stop it on th U-Boot console
- Load the public key hash in DDR
for example, the hash key file is located on 8th partition of the SD card:
load mmc 0:8 0xc0000000 publicKeyhash.bin
- Register public key hash
stm32key fuse 0xc0000000
For more information, see How to use U-Boot stm32key command.
4.2. Put hash key on device for STM32MP13x lines
[edit source]
To manually put the public key hash (PKH) on STM32MP device with U-Boot stm32key command, you need to:
- Put the 'Public Key Hash file (publicKeysHashHashes.bin), generated on previous section, on bootfs partition
- Boot the board and stop on U-Boot console
- Load public key hash in DDR
for example, the hash key file is located on 8th partition of sdcard:
load mmc 0:8 0xc0000000 publicKeysHashHashes.bin
- Register public key hash
stm32key fuse 0xc0000000
For more information, see How to use U-Boot stm32key command.
5. Put encryption key on STM32MP[edit source]
5.1. Put an encryption key on the device for STM32MP13x lines
[edit source]
To manually put the key on the STM32MP device with a U-Boot stm32key command, you need to:
- Put the encryption key file (stm32mp13_encryption_key.bin), generated in the previous section, on the bootfs partition
- Boot the board and stop it on the U-Boot console
- Load a hash public key in DDR
for example, the hash key file is located on 8th partition of the SD card:
load mmc 0:8 0xc0000000 stm32mp13_encryption_key.bin
- Select the EDMK key (How to use U-Boot stm32key command|)
EDMKstm32key select
- Register encryption key
stm32key fuse 0xc0000000
- Verify that the key is registered
stm32key read
For more information, see How to use U-Boot stm32key command.
6. Distribution package with signed FIP[edit source]
6.1. Pre-requisites[edit source]
- Having the Signature Key (Public Key(s), Private Key(s), Hash key file, password)
- Having obtained the STM32MP1 Distribution Package
6.2. Generate Distribution package with signed binaries[edit source]
- Source the environment of the Distribution package
source layers/meta-st/scripts/envsetup.sh
Select your DISTRO and your machine
- Indicate where to find your Signature key
(in this example we put the signature key on meta-st-stm32mp layer on key directory)
Add the following lines on your local.conf (on build directory)
For ST32MP15:
FIP_SIGN_KEY = "key/stm32mp15/privateKey.pem" ' >> conf/local.conf echo 'FIP_SIGN_KEY_stm32mp15 = "key/stm32mp15/privateKey.pem" ' >> conf/local.conf echo 'FIP_SIGN_KEY_EXTERNAL = "1" ' >> conf/local.conf echo 'FIP_SIGN_KEY_PASS = "<password of signature key>" ' >> conf/local.conf echo 'TF_A_SIGN_ENABLE = "1" ' >> conf/local.confecho '
For ST32MP13:
FIP_SIGN_KEY = "key/stm32mp13/privateKey00.pem" ' >> conf/local.conf echo 'FIP_SIGN_KEY_stm32mp13 = "key/stm32mp13/privateKey00.pem" ' >> conf/local.conf echo 'FIP_SIGN_KEY_EXTERNAL = "1" ' >> conf/local.conf echo 'FIP_SIGN_KEY_PASS = "<password of signature key>" ' >> conf/local.conf echo 'TF_A_SIGN_ENABLE = "1" ' >> conf/local.confecho '
Request to sign the FIP file generated:
FIP_SIGN_ENABLE = "1" ' >> conf/local.confecho '
- Compile your binaries
bitbake st-image-weston
On tmp-glibc/deploy/images/<machine name>/fip/ you will found the FIP file signed ready to be programmed on board.
6.3. Generate a Distribution package with encrypted partition binaries for STM32MP13x lines
[edit source]
To enable secure boot with encryption support, you must add DECRYPTION_SUPPORT=aes_gcm with the ENCRYPT_BLx to specify the encrypted binary.
Request encryption support on BL2 TF-A binaries:
echo 'TF_A_ENCRYPTED_ENABLE = "1" ' >> conf/local.conf
7. Sign first stage bootloader binaries[edit source]
The first stage bootloader binaries = TF-A BL2 are generated unsigned; we need to sign them manually with the STM32MP_SigningTool_CLI.
For installation and command-line options, see Signing tool.
These tools are used to sign a binary with STM32 header, with the minimal options to sign the FSBL binary:
-pubk <public key> -prvk <private key> -pwd <password> -t fsbl -of <Option_Flags> -bin FSBL binary not signed>.stm32 -o <FSBL binary signed>.stm32STM32MP_SigningTool_CLI
with:
- <public key>= the path of the Public key file generated by KeyGen: publicKey.pem
- <private key> = the path of the Private key files generated by KeyGen: privateKey*.pem, 1 for STM32MP15 and 8 for STM32MP13
- <password> = pasword used by KeyGen to protect the key files
- <Option_Flags> = the -of option is required only for STM32MP13, with 0x00000001 value
7.1. Signing first stage bootloader binaries for STM32MP15x lines
[edit source]
For SDCARD:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-sdcard.stm32 -o arm-trusted-firmware/tf-a-<board name>-sdcard_Signed.stm32
For EMMC:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-emmc.stm32 -o arm-trusted-firmware/tf-a-<board name>-emmc_Signed.stm32
For NAND:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-nand.stm32 -o arm-trusted-firmware/tf-a-<board name>-nand_Signed.stm32
For NOR:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-nor.stm32 -o arm-trusted-firmware/tf-a-<board name>-nor_Signed.stm32
For USB (used with STM32CubeProgrammer):
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-usb.stm32 -o arm-trusted-firmware/tf-a-<board name>-usb_Signed.stm32
For UART (used with STM32CubeProgrammer):
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp15/publicKey.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey.pem -pwd <password> -t fsbl -bin arm-trusted-firmware/tf-a-<board name>-uart.stm32 -o arm-trusted-firmware/tf-a-<board name>-uart_Signed.stm32
7.2. Signing first stage bootloader binaries for STM32MP13x lines
[edit source]
For SDCARD:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-sdcard.stm32 -o arm-trusted-firmware/tf-a-<board name>-sdcard_Signed.stm32
For EMMC:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp13/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-emmc.stm32 -o arm-trusted-firmware/tf-a-<board name>-emmc_Signed.stm32
For NAND:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp13/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-nand.stm32 -o arm-trusted-firmware/tf-a-<board name>-nand_Signed.stm32
For NOR:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp13/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-nor.stm32 -o arm-trusted-firmware/tf-a-<board name>-nor_Signed.stm32
For USB (used with STM32CubeProgrammer):
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp13/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-usb.stm32 -o arm-trusted-firmware/tf-a-<board name>-usb_Signed.stm32
For UART (used with STM32CubeProgrammer):
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp13/privateKey00.pem -pwd <password> -t fsbl -of 0x00000001 -bin arm-trusted-firmware/tf-a-<board name>-uart.stm32 -o arm-trusted-firmware/tf-a-<board name>-uart_Signed.stm32
7.3. Encrypt first stage bootloader binaries for STM32MP13x lines
[edit source]
For SDCARD:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey00.pem -pwd <password> --enc-key <path to meta-st-stm32mp>key/stm32mp13/stm32mp13_encryption_key.bin -t fsbl --enc-dc 0x0E5F2025 --image-version 0 -of 0x80000003 -bin arm-trusted-firmware/tf-a-<board name>-sdcard.stm32 -o arm-trusted-firmware/tf-a-<board name>-sdcard_Encrypted.stm32
For EMMC:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey00.pem -pwd <password> --enc-key <path to meta-st-stm32mp>key/stm32mp13/stm32mp13_encryption_key.bin -t fsbl --enc-dc 0x0E5F2025 --image-version 0 -of 0x80000003 -bin arm-trusted-firmware/tf-a-<board name>-emmc.stm32 -o arm-trusted-firmware/tf-a-<board name>-emmc_Encrypted.stm32
For NAND:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey00.pem -pwd <password> --enc-key <path to meta-st-stm32mp>key/stm32mp13/stm32mp13_encryption_key.bin -t fsbl --enc-dc 0x0E5F2025 --image-version 0 -of 0x80000003 -bin arm-trusted-firmware/tf-a-<board name>-nand.stm32 -o arm-trusted-firmware/tf-a-<board name>-nand_Encrypted.stm32
For NOR:
STM32MP_SigningTool_CLI -pubk <path to meta-st-stm32mp>key/stm32mp13/publicKey*.pem -prvk <path to meta-st-stm32mp>key/stm32mp15/privateKey00.pem -pwd <password> --enc-key <path to meta-st-stm32mp>key/stm32mp13/stm32mp13_encryption_key.bin -t fsbl --enc-dc 0x0E5F2025 --image-version 0 -of 0x80000003 -bin arm-trusted-firmware/tf-a-<board name>-nor.stm32 -o arm-trusted-firmware/tf-a-<board name>-nor_Encrypted.stm32
8. Create FlashLayout for signed binaries[edit source]
To populate the correct binaries on the board, you need to create a FlashLayout file with the signed binaries:
- FSBL = tf-a-*_Signed.stm32
- FIP = fip-*.bin
Example for FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv:
FIP none 0x0 fip/fip-stm32mp157f-dk2-optee.bin P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-dk2-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-dk2-sdcard.stm32 P 0x06 metadata1 Binary mmc0 0x00084400 arm-trusted-firmware/metadata.bin P 0x07 metadata2 Binary mmc0 0x000C4400 arm-trusted-firmware/metadata.bin P 0x08 fip-a FIP mmc0 0x00104400 fip/fip-stm32mp157f-dk2-optee.bin PED 0x09 fip-b FIP mmc0 0x00504400 none PED 0x0A u-boot-env Binary mmc0 0x00904400 none P 0x10 bootfs System mmc0 0x00984400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04984400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05984400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33984400 st-image-userfs-openstlinux-weston-stm32mp1.ext4#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-dk2-usb.stm32 - 0x03 fip-boot
You need to update the fsbl1-boot, fip-boot, fsbl1, fsbl2 and fip partitions.
Result:
FIP none 0x0 fip/fip-stm32mp157f-dk2-optee_Signed.bin P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-dk2- sdcard_Signed.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-dk2- sdcard_Signed.stm32 P 0x06 metadata1 Binary mmc0 0x00084400 arm-trusted-firmware/metadata.bin P 0x07 metadata2 Binary mmc0 0x000C4400 arm-trusted-firmware/metadata.bin P 0x08 fip-a FIP mmc0 0x00104400 fip/fip-stm32mp157f-dk2-optee_Signed.bin PED 0x09 fip-b FIP mmc0 0x00504400 none PED 0x0A u-boot-env Binary mmc0 0x00904400 none P 0x10 bootfs System mmc0 0x00984400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04984400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05984400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33984400 st-image-userfs-openstlinux-weston-stm32mp1.ext4#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-dk2-usb_Signed.stm32 - 0x03 fip-boot
9. Program and test[edit source]
To populate the correct binaries on the board with STM32CubeProgrammer, you must use the previous FlashLayout file with the signed binaries.
At board boot time, you must check the two level of the secure boot: the ROM code secure boot validation, and the TF-A BL2 trusted board boot validation.
10. Close the device[edit source]
For more information, see How to secure STM32 MPU.
In U-Boot console:
stm32key close
For more information, see the How to use U-Boot stm32key command.
As soon as the device is closed, the operation is irreversible; the user is forced to only use signed images.
11. References[edit source]