This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
OpenSTLinux distribution does not provide the flash memory layout (flashlayout) files required to use a UART as a serial boot device.
Refer to Using_STM32Programmer_over_UART article to see how to modify a flashlayout file to use a UART as serial boot device.
You can use this modified flashlayout as described in STM32CubeProgrammer article.
For example, the provided FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv file can be used on USB with the command:
STM32_Programmer_CLI -c port=usb1 -w FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv
By replacing tf-a-stm32mp157f-dk2-usb.stm32 to tf-a-stm32mp157f-dk2-uart.stm32 in this tsv file, the resulting file FlashLayout_sdcard_stm32mp157c-dk2-optee_uart.tsv can be used on UART port /dev/ttyACM1 with the command:
STM32_Programmer_CLI -c port=/dev/ttyACM1 -w FlashLayout_sdcard_stm32mp157c-dk2-optee_uart.tsv