The purpose of this article is to explain how the Linux® GPIOlib framework manages IOs/pins, how to configure it, and how to use it.
1. Framework purpose[edit source]
As explain in Overview of GPIO pins, the pins are multiplexed between "Alternate function", "ANALOG" and "GPIO" modes. The current article deals with the framework to use in order to manipulate GPIO: the GPIOLib framework. The GPIOLib framework is used when you want to control a pin directly in software, i.e. to set pin as output as a certain level (0/1), or to set pin in input configuration, or to configure the GPIO as an interrupt line. More details about GPIO in the kernel documentation are available in gpio.txt [1]
2. System overview[edit source]
2.1. Component description[edit source]
- GPIOLib:
- Pinctrl: the pinctrl framework core. Its role is:
- to call specific vendor callback for the pin configuration (muxing end setting).
- to create the logical pin mapping and guarantee pin exclusivity for a device. See Pinctrl overview
- Pinctrl-stm32: microprocessor specific pinctrl driver, its role is:
- to register the vendor specific function (callback) in the pinctrl framework.
- to access to hardware registers to configure pins (muxing and all pin capabilities).
- foo_driver: foo_driver could be any driver that needs to control a GPIO.
- debugfs: provides a debug interface available from the user terminal. See How to monitor with debugfs.
- GPIO tools: tools offered by the kernel to manipulate GPIOs. See GPIO tools.
2.2. API description[edit source]
Depending on needs and the caller location (kernel space or user space), several APIs are available to control a pin:
- User space API: the Linux® standard character device driver interface[3] allows applications to manipulate all "system objects" with the standard file API (open, read, write, close, IOctl...). This is used to manipulate GPIO through user space, as gpio devices are seen as files.
- Refer to GNU documentation for file manipulation.
- See example How to control a GPIO in userspace
- Kernel space API: the GPIOLib API provides API to the user driver.
- See in the Kernel documentation "consumer.txt" [4] to know how to obtain and use GPIO in a driver.
- See in the Kernel documentation "board.txt" [5] to know how to assign GPIOs to a consumer device.
- The GPIO descriptor acquisition is linked to a function label declared in the device tree. So there is a direct relationship between the driver and the device tree about this label, and the driver name (see sample code "dummy.c" below (ie "st,dummy" and "redled")).
- See example How to control a GPIO in kernel space
- Debugfs API: provides only information about GPIO configuration. See How to monitor with debugfs.
3. Configuration[edit source]
3.1. Kernel configuration[edit source]
GPIOLib is activated by default in ST deliveries.
3.2. Device tree configuration[edit source]
A detailed device tree configuration is described in GPIO device tree configuration.
4. How to use framework[edit source]
4.1. How to configure a new board[edit source]
If you have to declare a GPIO, please refer first to the hardware block GPIO page: GPIO internal peripheral and your board scematics. Then either you declare your GPIO directly in device tree or you declare it using the STM32CubeMX.
4.2. How to toggle a GPIO in user space[edit source]
How to control a GPIO in userspace
4.3. How to toggle a GPIO in kernel space[edit source]
How_to_control_a_GPIO_in_kernel_space
4.4. Tools[edit source]
5. How to trace and debug the framework[edit source]
5.1. How to monitor[edit source]
5.1.1. How to monitor with debugfs[edit source]
Some information about gpio is available in Debugfs interface.
cat /sys/kernel/debug/gpio
Output:
gpiochip0: GPIOs 0-15, parent: platform/soc:pin-controller@50002000, GPIOA:
...
gpiochip1: GPIOs 16-31, parent: platform/soc:pin-controller@50002000, GPIOB:
...
gpiochip5: GPIOs 80-95, parent: platform/soc:pin-controller@50002000, GPIOF:
gpio-94 ( |? ) out hi
gpio-95 ( |reset ) out hi
...
It provides per gpiochip: requested GPIOs, the state of the GPIO and the gpio-controller parent.
5.1.2. Other ways to monitor[edit source]
You can also get GPIO information by using gpiodetect - gpioinfo tools
5.2. How to trace[edit source]
By default there is no kernel trace to see the activity on GPIOs. However you could enable dynamic debug for the gpiolib and the pinctrl.
dmesg -n8
echo "file drivers/pinctrl/* +p" > /sys/kernel/debug/dynamic_debug/control
echo "file drivers/gio/* +p" > /sys/kernel/debug/dynamic_debug/control
6. Source code location[edit source]
The source files are located inside the Linux kernel.
- STM32 pinctrl vendor part: folder to STM32 dedicated pinctrl functions[12]
7. To go further[edit source]
GPIOLib is the main framework to handle a GPIO at run time. However, dedicated GPIO drivers already exist to control basic features (Leds, regulator, buttons, ...). You can find the list (and more details) inside the Kernel documentation [13]
8. References[edit source]
- ↑ Kernel documentation - gpio.txt, GPIO Kernel documentation
- ↑ Interrupt Management training document, Linux Kernel and Driver Development
- ↑ character device interface, Linux Kernel and Driver Development training document, see Kernel frameworks for device drivers chapter
- ↑ Kernel gpio documentation - consumer.txt,to know how to obtain and use GPIO in a driver
- ↑ Kernel gpio documentation - board.txt, to know how to assign GPIOs to a consumer device and a function
- ↑ GPIOLib source - gpiolib.c Provides GPIOLib API
- ↑ GPIOLib source - gpiolib-of.c Provides OF-GPIOLib API
- ↑ gpio tools folder Provides all sources of GPIO tools
- ↑ Pinctrl framework source - core.c Sources of generic pinctrl framework
- ↑ Pinctrl framework source - pinconf.c Sources of generic pin configuration
- ↑ Pinctrl framework source - pinmux.c Sources of generic pin muxing
- ↑ STM32 vendor specific folder Provides all vendor specifics functions
- ↑ Kernel documentation - drivers-on-gpio.txt List and explain standard kernel drivers used for common GPIO task