This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Configure a wireless gateway[edit source]
A wireless gateway routes packets from a wireless LAN to a wired network (Ethernet)
Prerequisites
For this example of configuration, the setup is :
- wlan0: wireless interface connected to SSID_NETWORK with DHCP
- eth0: this is an ethernet interface with a static IP address, which also includes a DHCP server
- packet forwarding is activated between the two network interfaces.
Apply the same procedure: How_to_setup_a_WLAN_connection#How_to_set_a_wireless_configuration_with_networkd
Add "IPForward=ipv4" rule in the 51-wireless.network file as follows:
cat /lib/systemd/network/51-wireless.network
[Match]
Name=wlan0
[Network]
DHCP=ipv4
IPForward=ipv4
- IPForward
- allows to forward any network packet from a wireless network to another network.