This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Configure a wireless gateway[edit source]
A wireless gateway routes packets from a wireless LAN to wired network (Ethernet)
Prerequisites For this example of configuration, the setup is :
- wlan0: wireless interface connected to SSID_NETWORK with DHCP
- eth0: ethernet interface with static IP which also have a DHCPserver on it
- forward of packet are activated between the two network interfaces.
same procedure of How_to_setup_a_WLAN_connection#How_to_set_a_wireless_configuration_with_networkd }}
Just need to add this rule in 51-wireless.network file:
cat /lib/systemd/network/51-wireless.network
[Match]
Name=wlan0
[Network]
DHCP=ipv4
IPForward=ipv4
- IPForward
- permit to forward all network packet from wireless network to other network.