X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). It is composed of an OpenEmbedded meta layer, named meta-st-stm32mpu-ai, to be added on top of the STM32MP1 Distribution Package. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices.

1. X-LINUX-AI v3.0.0
1.1. Contents
TensorFlow™ Lite[1] 2.11.0
ONNX Runtime[2] 1.11.0
- Coral Edge TPU™[3] accelerator native support
- libedgetpu 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0
- libcoral 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0
- PyCoral 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0
- OpenCV[4] 4.5.x
- Python™[5] 3.10.x (enabling Pillow module)
- Application samples
Python image classification using ONNX™ Runtime based on MobileNet v1 quantized model
- C++ / Python image classification using TensorFlow™ Lite based on MobileNet v1 quantized model
- C++ / Python object detection using TensorFlow™ Lite based on COCO SSD MobileNet v1 quantized model
- C++ / Python image classification using Coral Edge TPU™ based on MobileNet v1 quantized model and compiled for the Coral Edge TPU™
- C++ / Python object detection using Coral Edge TPU™ based on COCO SSD MobileNet v1 quantized model and compiled for the Coral Edge TPU™
- C++ face recognition using TensorFlow™ Lite models capable of recognizing the face of a known (enrolled) user (available on demand)
- Application support for the 720p, 480p, and 272p display configurations
Python application camera pipeline update to use GtkWaylandsink and achieve better performance
- X-LINUX-AI SDK add-on extending the OpenSTLinux SDK with AI functionality to develop and build an AI application easily. The X-LINUX-AI SDK add-on provides support for all the above frameworks. It is available from the X-LINUX-AI product page
1.2. Validated hardware
As any software expansion package, the X-LINUX-AI is supported on all STM32MP1 Series and it has been validated on the following boards:
1.3. Software structure

2. Starter package: install from the OpenSTLinux AI package repository
All the generated X-LINUX-AI packages are available from the OpenSTLinux AI package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AI.
This repository contains AI packages that can be simply installed using apt-* utilities, which the same as those used on a Debian system:
- the main group contains the selection of AI packages whose installation is automatically tested by STMicroelectronics
- the updates group is reserved for future uses such as package revision update.
You can install them individually or by package group.
2.1. Prerequisites
- Flash the Starter Package on your SDCard
- For OpenSTLinux ecosystem release v4.1.0
:
- For OpenSTLinux ecosystem release v4.1.0
- Your board has an internet connection either through the network cable or through a WiFi connection.
2.2. Configure the AI OpenSTLinux package repository
Once the board is booted, execute the following command in the console in order to configure the AI OpenSTLinux package repository:
v4.1.0For ecosystem release: wget http://extra.packages.openstlinux.st.com/AI/4.1/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb dpkg -i apt-openstlinux-ai_1.0_armhf.deb
Then synchronize the AI OpenSTLinux package repository.
apt-get update
2.3. Install AI packages
2.3.1. Install all X-LINUX-AI packages
Command | Description |
---|---|
apt-get install packagegroup-x-linux-ai |
Install all the X-LINUX-AI packages (TensorFlow™ Lite, Edge TPU™, application samples and tools) |
2.3.3. Install individual packages
3. Developer package: build AI application from the X-LINUX-AI add-on SDK
In order to easily develop and build an AI application without using the Yocto build system, X-LINUX-AI comes with a SDK add-on extending the OpenSTLinux SDK with AI functionality.
All the needed information to install and use the X-LINUX-AI SDK add-on can be found in the following article : How to install and use the X-LINUX-AI SDK add-on
4. Distribution package: re-generate X-LINUX-AI OpenSTLinux distribution
With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.
This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.
4.1. Download the STM32MP1 Distribution Package
For ecosystem release v4.1.0 :
Install the STM32MP1 Distribution Package v4.1.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).
4.2. Install X-LINUX-AI environment
- Clone the meta-st-stm32mpu-ai git repositories
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai.git -b v3.0.0For X-LINUX-AI v3.0.0: cd <Distribution Package installation directory>/layers/meta-st git clone
- For a new environment
- For an already installed environment
4.3. Build the image
bitbake st-image-ai
4.4. Flash the built image
Follow this link to see how to flash the built image.
5. How to use the X-LINUX-AI Expansion Package
5.1. Material needed
To use the X-LINUX-AI OpenSTLinux Expansion Package, choose one of the following materials:
Optional:
- Coral USB Edge TPU™[3] accelerator
5.2. Boot the OpenSTlinux Starter Package
At the end of the boot sequence, the demo launcher application appears on the screen.
5.3. Install the X-LINUX-AI
After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.
apt-get install packagegroup-x-linux-ai
And restart the demo launcher:
systemctl restart weston-launch
Check that X-LINUX-AI is properly installed:
x-linux-ai -v
X-LINUX-AI version: v3.0.0
5.4. Launch an AI application sample
Once the demo launcher is restarted, notice that it is slightly different because new AI application samples have been installed.
The demo launcher has the following appearance, and you can navigate into the different screens by using the NEXT or BACK buttons.
The demo launcher now contain AI application samples that are described within dedicated article available in the X-LINUX-AI application samples zoo page.
5.5. Enjoy running your own NN models
The above examples provide application samples to demonstrate how to execute models easily on the STM32MP1.
You are free to update the C/C++ application or Python scripts for your own purposes, using your own NN models.
Source code locations are provided in application sample pages.
6. References
7. Archives 
X-LINUX-AI release | Release note |
---|---|
X-LINUX-AI v2.2.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package_-_v2.2.0#X-LINUX-AI_v2-2-0 |
X-LINUX-AI v2.1.1 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-1 page for the v3 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.1.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-0 page for the v2 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.0.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-0-0 page for the v2 ecosystem releases (in archived wiki) |