This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This section gives an overview of Linux® kernel drivers (UPPERCASE in the figure) implemented for the STM32MP13 support, with their respective software frameworks (lowercase in the figure).
The components are grouped per functional domains.
Each Linux framework is further described in Linux operating system category articles.
Each STM32 MPU peripheral is introduced in peripherals overview articles.
Both those sections are reusing the same functional domain split.
The color code, explained in the legend, allows to see the code origin for each component.


- Documentation/arm/stm32/overview.rst
- PWM overview
- Overview of GPIO pins
- Interrupt overview
- Dmaengine overview
- Watchdog overview
- Linux kernel device tree
- RTC overview
- Reset overview
- Clock overview
- CAN overview
- Ethernet overview
- WLAN overview
- Bluetooth overview
- ALSA overview
- V4L2 camera overview
- DRM KMS overview
- SPI overview
- I2C overview
- Serial TTY overview
- MTD overview
- MMC overview
- Power overview
- Regulator overview
- Thermal overview
- NVMEM overview
- OP-TEE overview
- Crypto API overview
- Hardware random overview
- USB overview
- IIO overview
STM32MP13 Linux kernel overview