How to prevent the year 2038 bug

Revision as of 14:57, 23 November 2022 by Registered User

1. Article purpose[edit source]


2. Introduction[edit source]

The Year 2038 problem is a time formatting bug in computer systems with representing times after 03:14:07 UTC on 19 January 2038. To summarize, this bug will happen on Unix-like system (so on Linux®) because, on 32 bits platforms, the time is coded on a singed 32 bits integer, and at 03:14:07 UTC on 19 January 2038, it will loop and then be understood as 20:45:52 UTC on 13 December 1901.

3. Behavior[edit source]

On OpenSTLinux, in the event of that problem, a watchdog will be fired.

Tue Jan 19 03:14:07 UTC 2038                                                    
[  164.856181] systemd-journald[283]: Assertion 'clock_gettime(map_clock_id(clo.
Thu Jan  1 00:00:01 UTC 1970                                                    
[  165.428314] watchdog: watchdog0: watchdog did not stop!                      
Thu Jan  1 00:00:01 UTC 1970                                                    
Thu Jan  1 00:00:01 UTC 1970                                                    
Thu Jan  1 00:00:01 UTC 1970                                                                                             [  172.837733] systemd-coredump[1036]: Process 283 (systemd-journal) of user 0 .
[  172.844733] systemd-coredump[1036]: Coredump diverted to /var/lib/systemd/coz
Thu Jan  1 00:00:01 UTC 1970
[  183.125664] systemd-coredump[1037]: Failed to log coredump: Connection refusd
Thu Jan  1 00:00:01 UTC 1970                                                    
Thu Jan  1 00:00:01 UTC 1970
INFO:    CPU 0 IT Watchdog 2                                                    
INFO:    CPU : 0       

From this log, we can see the date is now 1970 (and not 1901) and does not change anymore. This is caused by the fact that some executables on the system already support the time on a signed 64 bits integer whereas some others still don't support such format.

4. BSP side[edit source]

4.1. OP-TEE OS[edit source]

OP-TEE OS already supports time on 64 bits instead of 32bits.

4.2. TF-A[edit source]

TF-A already supports time on 64 bits instead of 32bits.

4.3. U-Boot[edit source]

U-Boot already supports time on 64 bits instead of 32bits.

4.4. Linux kernel[edit source]

The Linux kernel already supports time on 64 bits instead of 32 bits.

5. User space[edit source]

There is no universal solution to fix that issue.

5.1. Gnu LibC[edit source]

Since the version 2.34, the support of the time on 64 bits is already implemented. But by default, to keep compatibility, all applications, built with the Gnu LibC, use a time coded on 32 bits. So, to use a time format on 64 bits, two "defines" must be set on build line for application: _TIME_BITS==64 and _FILE_OFFSET_BITS==64.

5.2. User space applications[edit source]

As stated above, to build applications for using a time coded on 64 bits, two defines must be specified.

5.2.1. get_date.c (an example)[edit source]

Let's try with following example:

// Code based on example found here: https://www.blaess.fr/christophe/2038/
#include <stdio.h>
#include <stdlib.h>
#include <time.h>

int main(void)
{
	time_t now;
	struct tm *tm_now;
	char line[1024];

	printf("sizeof(int): %d\n",sizeof(int));
	printf("sizeof(long long int): %d\n",sizeof(long long int));
	printf("sizeof(time_t): %d\n",sizeof(time_t));

	time(&now);
	tm_now = gmtime(&now);
	strftime(line, 1023, "%x %X", tm_now);
	printf("%s\n", line);

	return 0;
}
  • Cross-compile it without the defines
 $CC -Wall get_date.c -o get_date_32b

Execute it on the platform

 ./get_date_32b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 4
01/19/38 03:14:07
 ./get_date_32b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 4
01/01/70 00:00:00
 ./get_date_32b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 4
01/01/70 00:00:00
  • Cross-compile it with the defines
 $CC  -D_TIME_BITS==64 -D_FILE_OFFSET_BITS==64 -Wall get_date.c -o get_date_64b

Execute it on the platform

 ./get_date_64b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 8
01/19/38 03:14:07
 ./get_date_64b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 8
01/19/38 03:14:08
 ./get_date_64b
sizeof(int): 4
sizeof(long long int): 8
sizeof(time_t): 8
01/19/38 03:14:09

The first executable cannot read correctly the time, whereas the second can.

5.3. Other applications[edit source]

When building application with these two defines, behavior can be different:

  • successful if the application does not deal with time or already ported to support time format on 64 bits
  • unsuccessful if the work is not already done.


5.3.1. ioclt alias[edit source]

The glibc added a time64 alias for ioctl but some application can still look for ioctl during the link. A quick patch could be something like that

 libtswrap_la_LDFLAGS = \
-       -export-symbols-regex ^ioctl \
+       -export-symbols-regex ^__ioctl_time64 \

5.3.2. _FILE_OFFSET_BITS[edit source]

When the flag _TIME_BITS is defined, the flag _FILE_OFFSET_BITS must be defined too. But some application disable it. A quick patch could be something like that

-#    undef _FILE_OFFSET_BITS
+/*#    undef _FILE_OFFSET_BITS*/

But sometimes, to remove that undef is not enough and can bring new build issues, like these ones.

| {standard input}: Assembler messages:
| {standard input}:197: Error: symbol `open64' is already defined
| {standard input}:437: Error: symbol `mmap64' is already defined
No categories assignedEdit