Last edited 2 years ago

STM32MP135x-DK - software distributions


The STM32MP135x-DK Discovery kit Warning.png (STM32MP135F-DK Warning.png) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP135 line Warning.png microprocessor devices.

All useful information to start with the STM32MP135x-DK Discovery kit Warning.png is accessible through the links provided below.

1. Supported software distribution[edit source]

Only one software distribution is supported with STM32MP135x-DK Discovery kit Warning.png:

  • The STM32MPU Embedded Software distribution[1].

Take also a look at the latest STM32 MPU ecosystem release note for complementary information.

For this distribution, three software Packages are delivered:

  • the Starter Package
  • the Developer Package
  • the Distribution Package

Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.

These Packages provide you with the software packages (image, source code) and the tools that are needed to start using the STM32MP135x-DK Warning.png Discovery Kits boards.

2. Hardware description[edit source]

The STM32MP135x-DK - hardware description article describes the board, and provides indications on how to:

  • assemble the board
  • configure the hardware switches
  • connect the board to external material

It also contains a short introduction of the board hardware components and connectors.

3. References[edit source]