How to play audio

Revision as of 13:46, 8 June 2022 by Registered User (→‎Audio playback overview)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Article purpose[edit source]

This article explains how to play audio through the ALSA audio framework in Linux® OS context. The examples below, show how to play audio on the different audio hardware interfaces of the STM32MPU boards.

2. Audio playback overview[edit source]

The ALSA framework exposes audio devices associated to the board audio hardware interfaces.

The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface which allows to list audio profiles and to select a profile, to play on a specific audio interface.

Warning white.png Warning
The applications interacting with Weston framework have to be launched as "Weston" user instead of "root" user. The Pulseaudio commands can, for instance, be launched as follows:
su -l "weston" -c "pactl info"

The audio playback examples in following sections are given for ALSA utilities. However, the audio playbacks can be launched by other applications, such as gstreamer multimedia framework.

3. Examples[edit source]

3.1. Audio playback on headset output[edit source]

3.1.1. Playback on ALSA device[edit source]

Run audio playback on 'playback_codec' ALSA device:

Info white.png Information
'playback_codec' is an alias defined in /etc/asound.conf, for headset output device.
 aplay -D playback_codec /usr/share/sounds/alsa/Front_Left.wav

3.1.2. Playback via PulseAudio[edit source]

  • Configure Pulseaudio

Change the Pulseaudio active profile of the sound card, to 'analog-stereo' profile:

Info white.png Information
The Pulseaudio analog-stereo profile is the default profile. So next command is not required after boot.
Info white.png Information
Example below is given for sound card index 0. Check sound cards index with "pactl list cards short" command.
 pactl set-card-profile 0 output:analog-stereo
  • Run audio playback:
 aplay /usr/share/sounds/alsa/Front_Left.wav

3.2. Audio playback on HDMI output[edit source]

Warning white.png Warning
The support of HDMI output is board dependent. Please, check available outputs with "aplay -l" command.

3.2.1. Playback on ALSA device[edit source]

Run audio playback on 'playback_hdmi' ALSA device:

Info white.png Information
'playback_hdmi' is an alias defined in /etc/asound.conf, for hdmi output device.
 aplay -D playback_hdmi /usr/share/sounds/alsa/Front_Left.wav

3.2.2. Playback via PulseAudio[edit source]

  • Configure Pulseaudio

Change the Pulseaudio active profile of the sound card, to 'hdmi-stereo' profile:

Info white.png Information
Example below is given for sound card index 0. Check sound card index with "pactl list cards short" command.
 pactl set-card-profile 0 output:hdmi-stereo
  • Run audio playback:
 aplay /usr/share/sounds/alsa/Front_Left.wav

3.3. Audio playback on S/PDIF output[edit source]

Warning white.png Warning
The support of S/PDIF output is board dependent. Please, check available outputs with "aplay -l" command.
Info white.png Information
S/PDIF ALSA device supports only 32-bit audio streams. As 32-bit wave files are not provided in sample sound files, speaker-test is used instead of aplay, for convenience, here. Speaker-test generates a 440Hz sine wave in following examples.

3.3.1. Set IEC958 status bits[edit source]

Example: set IEC958 mode bit.

 iecset -c STM32MP1EV -n device=0 pro on

3.3.2. Playback on ALSA device[edit source]

Run audio playback on 'playback_spdif' ALSA device:

Info white.png Information
'playback_spdif' is an alias defined in /etc/asound.conf, for S/PDIF output device.
 speaker-test -D playback_spdif -c 2 -F S32_LE -f 440 -t sine -l 1

3.3.3. Playback via PulseAudio[edit source]

  • Configure Pulseaudio

Change the sound card active profile, to S/PDIF 'iec958-stereo' profile.

Info white.png Information
Example below is given for sound card index 0. Check sound card index with "pactl list cards short" command.
 pactl set-card-profile 0 output:iec958-stereo
  • Run audio playback:
 speaker-test -c 2 -F S32_LE -f 440 -t sine -l 1