How to use U-Boot stm32key command

Revision as of 19:07, 3 March 2022 by Registered User (→‎Purpose)
Applicable for STM32MP13x lines, STM32MP15x lines

This page explains how to enable the the secure boot for your board.

1. Purpose[edit source]

The secure boot is a key feature to guarantee a secure platform.

In this article, the stm32key U-Boot command is used to illustrate and experiment the steps needed to activate the associated features: authentication and encryption.

For real secured product, the associated OTPs must be updated directly by customer application or with Secure Secret Provisioning (SSP).

Warning white.png Warning
Make sure that a device with Secure boot enabled is used: this is mentioned in the chip part number, for STM32MP13 and STM32MP15, otherwise the device will become permanently unusable.

2. Prerequisite[edit source]

The needed keys file is generated using STM32 KeyGen tool.

3. U-Boot command stm32key[edit source]

U-Boot in OpenSTLinux embeds a stm32key command that can be called from U-Boot command line interface to manage the keys in OTPs.

  stm32key help
 stm32key - Manage key on STM32
 
 Usage:
 stm32key list : list the supported key with description
 stm32key select [<key>] : Select the key identified by <key> or display the key used for read/fuse command
 stm32key read [<addr> | -a ] : Read the curent key at <addr> or current / all (-a) key in OTP
 stm32key fuse [-y] <addr> : Fuse the current key at addr in OTP
 stm32key close [-y] : Close the device, force use of PKH stored in OTP

The optional option -y is used to skip the confirmation message.

The name of the used <key> is

  • for STM32MP13x lines More info.png: PKHTH for authentication and FEK for encryption
  stm32key list
 PKHTH : Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm)
 	OTP24..32
 FEK : Firmware Encryption Key
 	OTP92..95
  • for STM32MP15x lines More info.png: PKH for authentication
  stm32key list
 PKH : Hash of the ECC Public Key (ECDSA is the authentication algorithm)
 	OTP24..32

4. Authentication steps with U-Boot[edit source]

The steps described in authentication for STM32MP13x and for STM32MP15x are executed with the same sequence of U-Boot stm32keycommands:

4.1. Keys registration with U-Boot[edit source]

The first step to enable the authentication is to burn the keys in OTPs with the output file from STM32 KeyGen.

  • Select keys with U-Boot : with the command sm32key select <key>
    with <key>=
  • PKHTH for STM32MP13x lines More info.png
  sm32key select PKHTH
 PKHTH selected
  • PKH for STM32MP15x lines More info.png
  sm32key select PKH
 PKH selected
  • Load keys file in DDR

The keys file, the output file from STM32 KeyGen, must be available in DDR before proceeding the stm32key command;
this file is loaded at 0xc0000000 in the next examples.

For example loaded from a filesystem partition on a storage device by using the load.

with a file Keys.bin in bootfs (partition 4) on SD card (mmc0):

  load mmc 0:4 0xc0000000 Keys.bin
 32 bytes read in 50 ms (0 Bytes/s)
  • Verify keys file in DDR

Then you can verify the content of keys files loaded in DDR with the command:

  stm32key read 0xc0000000 

Example for STM32MP13x lines More info.png with PKHTH

 stm32key read 0xC0000000
 Read PKHTH at 0xc0000000
 PKHTH OTP 24: [c0000000] 27051956
 PKHTH OTP 25: [c0000004] b56aef2d
 PKHTH OTP 26: [c0000008] 6215263c
 PKHTH OTP 27: [c000000c] 00000439
 PKHTH OTP 28: [c0000010] 00000000
 PKHTH OTP 29: [c0000014] 00000000
 PKHTH OTP 30: [c0000018] 72429173
 PKHTH OTP 31: [c000001c] 05020600

Example for STM32MP15x lines More info.png with PKH

 stm32key read 0xC0000000
 Read PKH at 0xc0000000
 PKH OTP 24: [c0000000] 27051956EDMK
 PKH OTP 25: [c0000004] b56aef2d
 PKH OTP 26: [c0000008] 6215263c
 PKH OTP 27: [c000000c] 00000439
 PKH OTP 28: [c0000010] 00000000
 PKH OTP 29: [c0000014] 00000000
 PKH OTP 30: [c0000018] 72429173
 PKH OTP 31: [c000001c] 05020600
  • Register keys

To write and lock the keys in OTP, you use the command:

  stm32key fuse 0xc0000000 
Warning white.png Warning
Verify keys before to confirm the operation, it is a irreversible operation !
  • Verify keys in OTPs

After the previous command, the device contains the keys to authenticate images and it can be verified with the command:

  stm32key read

Result for STM32MP13x lines More info.png with PKHTH

 stm32key readEDMKEDMKEDMK
 PKHTH OTP 24: 27051956 lock : 50000000
 PKHTH OTP 25: b56aef2d lock : 50000000
 PKHTH OTP 26: 6215263c lock : 50000000
 PKHTH OTP 27: 00000439 lock : 50000000
 PKHTH OTP 28: 00000000 lock : 50000000
 PKHTH OTP 29: 00000000 lock : 50000000
 PKHTH OTP 30: 72429173 lock : 50000000
 PKHTH OTP 31: 05020600 lock : 50000000

Result for STM32MP15x lines More info.png with PKH

 stm32key read
 PKH OTP 24: 27051956 lock : 50000000
 PKH OTP 25: b56aef2d lock : 50000000
 PKH OTP 26: 6215263c lock : 50000000
 PKH OTP 27: 00000439 lock : 50000000
 PKH OTP 28: 00000000 lock : 50000000
 PKH OTP 29: 00000000 lock : 50000000
 PKH OTP 30: 72429173 lock : 50000000
 PKH OTP 31: 05020600 lock : 50000000

4.2. Check authentication[edit source]

Without any other modification, the device is able to perform image authentication but the non-authenticated images can still be used and executed: the device is still opened, let's see this as a kind of test mode to check that the keys is properly set.

To check authentication, the FSBL =TF-A binary must be signed with the STM32 Signing tool.

Once the image is signed, it can be programmed into the flash on the target board with STM32CubeProgrammer.

Using this signed binary, the ROM code compares the keys carried in the STM32 header with the one that was provisioned in OTP and starts the FSBL = TF-A.

The Authentication result to transmit to TF-A and, at boot time on board, you must see the following line in TF-A trace:
NOTICE: Bootrom authentication succeeded

Example:

NOTICE:  CPU: STM32MP157CAA Rev.?
NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
NOTICE:  Board: MB1263 Var1.0 Rev.C-01
NOTICE:  Bootrom authentication succeeded
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    PMIC version = 0x10

4.3. Closing the device with U-Boot[edit source]

As soon as the authentication process is confirmed, the device can be closed and the user is forced to use signed images.

Non-signed binaries will not be supported anymore on the target.

This operation is perform with the U-Boot command:

  stm32key close
Warning white.png Warning
This must not be done on STM32MP13 or STM32MP15 part numbers without Secure boot enabled, otherwise the chip will be bricked and could not be used anymore

On closed device, if the authentication fails, the ROM code enters into a serial boot loop indicated by the blinking Error LED (cf ROM code common debug and error cases).

5. References[edit source]