Arm CoreSight overview

Revision as of 11:06, 27 January 2022 by Registered User (Merge articles)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Article purpose[edit source]

The purpose of this article is to provide information on the Arm® CoreSight hardware subsystem.
It explains what are the principle peripherals of this subsystem.

2. Peripheral overview[edit source]

Arm® CoreSight products include

  • a wide range of trace macrocells for Arm® processors,

To enable the debug and trace of the most complex, multi-core SoCs, Arm® CoreSight products include

  • a system and software instrumentation,
  • and a comprehensive set of IP blocks.

Arm® has defined an open CoreSight architecture to allow SoC designers to add "debug and trace" capabilities for other IP cores in to the CoreSight infrastructure.

Alternate text
CoreSight overview

2.1. Components description[edit source]

The debug features are based on Arm® CoreSight™ components:

  • SWJ-DP: JTAG/Serial-wire debug port
  • AXI-AP: AXI access port
  • AHB-AP: AHB access port
  • APB-AP: APB access port
  • ITM: Instrumentation Trace Macrocell
  • DWT: Data Watchpoint and Trace
  • ETM: Embedded Trace Macrocell
  • ETF: Embedded Trace FIFO
  • TPIU: Trace Port Interface Unit
  • SWO: Serial Wire Output
  • CTI: Cross Trigger Interface
  • CTM: Cross Trigger Matrix
  • TSGEN: Timestamp Generator
  • STM: System Trace Macrocell

More information about these components can be found in the Arm® website [1]

2.2. Features[edit source]

Refer to the Debug support (DBG) chapter of

for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

3. References[edit source]