This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Article purpose[edit source]
The Reserved-memory mechanism[1] allows reserving memory regions in the kernel. This mechanism is used by drivers to allocate buffers in specific memory regions (such as internal SRAM[2][3]) or to get a dedicated memory pool that will not be managed by Linux® conventionnal memory allocator (in DDR).
2. Use cases[edit source]
In OpenSTLinux, the reserved-memory is used:
- On STM32MP1 Series by:
- the dmaengine driver to reserve the region where DMA buffers are allocated, typically internal SRAM[2][3].
- the remoteproc driver to reserve the regions in RETRAM and MCU SRAM where the coprocessor firmware will be loaded.
- the RPMsg driver to reserve the region where RPMsg buffers used for interprocess communication with the coprocessor, are allocated, typically MCU SRAM.
- the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the DDR.
3. References[edit source]