1. Article purpose[edit source]
The purpose of this article is to
- briefly introduce the QUADSPI peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when needed, how to configure the QUADSPI peripheral.
2. Peripheral overview[edit source]
The Quad-SPI interface (QUADSPI peripheral) is used to interface the processor with serial NOR Flash and serial NAND Flash memories.
It supports:
- Single, dual or quad SPI Flash memories
- A dual-flash mode, allowing to agregate two Flash memories into a virtual single one
- Dual data rate and memory-mapped modes.
2.1. Features[edit source]
Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.
2.2. Security support[edit source]
2.2.1. On STM32MP13x lines
[edit source]
The QUADSPI is a secure peripheral (under ETZPC control).
2.2.2. On STM32MP15x lines
[edit source]
The QUADSPI is a non secure peripheral.
3. Using the peripheral - associated software[edit source]
3.1. Boot time[edit source]
QUADSPI instance is boot device that support serial boot for Flash programming with STM32CubeProgrammer.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The QUADSPI instances can be allocated to:
- the Arm® Cortex®-A7 secure context, on STM32MP13x lines
only, but this is not supported in OpenSTLinux.
- the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the MTD framework
- the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by QUADSPI HAL driver
Chapter #Peripheral assignment describes which peripheral instances can be assigned to which context.
3.2.2. Software frameworks[edit source]
3.2.2.1. On STM32MP13x lines
[edit source]
Domain | Peripheral | Software components | Comment | |
---|---|---|---|---|
OP-TEE | Linux | |||
Mass storage | QUADSPI | Linux MTD framework |
3.2.2.2. On STM32MP15x lines
[edit source]
Internal peripherals software table template
| Mass storage | QUADSPI | | Linux MTD framework | STM32Cube QUADSPI driver | |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
For Linux kernel configuration, please refer to QUADSPI device tree configuration.
3.2.4. Peripheral assignment[edit source]
3.2.4.1. On STM32MP13x lines
[edit source]
Click on the right to expand the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP13 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Mass storage | QUADSPI | QUADSPI | ⬚ | ☐ | Assignment (single choice) |
3.2.4.2. On STM32MP15x lines
[edit source]
Internal peripherals assignment table template
| rowspan="1" | Mass storage | rowspan="1" | QUADSPI | QUADSPI | | ☐ | ☐ | Assignment (single choice) |-
|}
4. How to go further[edit source]
5. References[edit source]