STM32MP15 ETZPC internal peripheral

Revision as of 10:11, 10 September 2021 by Registered User
Applicable for STM32MP15x lines

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the ETZPC peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how it can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the ETZPC peripheral.

2. Peripheral overview[edit source]

The ETZPC peripheral is used to configure TrustZone security in a SoC having bus masters and slaves with programmable-security attributes (securable resources) such as:

  • on-chip RAM/ROM with programmable secure region size
  • AHB and APB peripherals to be made secure
  • AHB masters to be granted secure rights

The ETZPC peripheral also allows peripheral isolation. With MCU isolation, some peripherals can be assigned to Cortex-M4 context execution only. Those peripherals will not be accessible for Cortex-A7 contexts (secure and non-secure).

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2. Security support[edit source]

The ETZPC is a secure peripheral.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The ETZPC is configured at boot time to setup the platform security.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The ETZPC is a system peripheral and is controlled by the Arm® Cortex®-A7 secure.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Security
| ETZPC
| TF-A(BL32) or OP-TEE ETZPC driver Read/Write access
| U-Boot
Read only access | Resource Manager Utility Read only access | Configuration made by A7 secure.
U-Boot updates the Linux device tree. |- |}

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in a secure context.

This configuration is done in TF-A(BL32) or OP-TEE, through device tree (see ETZPC device tree configuration).

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Security
| rowspan="1" | ETZPC
| ETZPC
| 
| 
| 
| 
|-
|}

4. How to go further[edit source]

The ETZPC is an STMicroelectronics extension of the Arm® peripheral: TrustZone Protection Controller[1]

5. References[edit source]