This article provides basic information about the DMA engine and how STM32 DMA, DMAMUX and MDMA drivers are plugged into it.
1. Framework purpose[edit source]
This article provides basic information about the DMA framework. However it is worth browsing the Kernel documentation related to DMA concept[1].
The direct memory access (DMA) is a feature that allows some hardware subsystems to access memory independently from the central processing unit (CPU).
The DMA can transfer data between peripherals and memory or between memory and memory.
2. System overview[edit source]
![](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/3/36/DMA_schemas.png)
2.1. Component description[edit source]
- Peripheral DMA client drivers:
DMA clients are drivers that are mapped on the DMA API[2].
- DMA engine:
The DMA engine is the engine core on which all clients rely.
Refer to DMA provider[1] for useful information on DMA internal behaviour.
- Virtual DMA channel support:
The virtual DMA channel support manages virtual DMA channels and DMA requests queues. This layer is no used by DMA clients.
- STM32 xDMA driver:
The STM32 xDMA driver is used to develop the DMA engine API.
- STM32 DMAMUX driver:
The STM32 DMAMUX driver request multiplexer allows routing DMA request lines between the device peripherals and the DMA controllers.
- DMAMUX, DMA and MDMA IP controller:
This is the STM32 DMA controller that handles data transfers between peripherals and memories or memory and memory connected to the same bus.
DMAMUX (DMA request router): DMAMUX internal peripheral
DMA: DMA internal peripheral
MDMA : MDMA internal peripheral
- Peripheral clients:
Peripheral clients are peripherals where at least one DMA request line is mapped on DMAMUX.
- Memories:
Memories can be either internal (e.g. SRAM, RETRAM or BCKRAM) or external (DDR).
2.2. APIs description[edit source]
Please refer to DMA Engine API Guide[3] for a clear description of the DMA framework API.
In addition, going through Dynamic API[4] provides insight on the DMA memory allocation API. The client has to rely on this API to properly allocate DMA buffers so that they are processed by the DMA engine without any trouble.
The document Dynamic DMA mapping Guide[5] can be read in conjunction with the previous one.
It presents some examples and usecases.
3. Configuration[edit source]
3.1. Kernel Configuration[edit source]
The DMA engine and driver are enabled throughout menu config (see Menuconfig or how to configure kernel):
For DMA:
Device Drivers -> [*] DMA Engine support -> [*] STMicroelectronics STM32 DMA support
For DMAMUX:
Device Drivers ->
[*] DMA Engine support ->
[*] STMicroelectronics STM32 dma multiplexer support
For MDMA
Device Drivers ->
[*] DMA Engine support ->
[*] STMicroelectronics STM32 master dma support
3.2. Device Tree configuration[edit source]
The DT configuration can be done using the STM32CubeMX.
Refer to the following articles for a description of the DT configuration:
- For DMA: DMA device tree configuration
- For DMAMUX: DMAMUX device tree configuration
- For MDMA: MDMA device tree configuration
4. How to trace and debug the framework[edit source]
4.1. How to trace[edit source]
Through menuconfig, enable DMA engine debugging and DMA engine verbose debugging (including STM32 drivers):
Device Drivers -> [*] DMA Engine support -> [*] DMA Engine debugging [*] DMA Engine verbose debugging (NEW)
4.2. How to debug[edit source]
4.2.1. devfs[edit source]
sysfs entry can be used to browse for available DMA channels.
More information can be found in sysfs.
The following command lists all the registered DMA channels:
Board $> ls /sys/class/dma/ dma0chan0 dma0chan13 dma0chan18 dma0chan22 dma0chan27 dma0chan31 dma0chan8 dma1chan3 dma2chan0 dma2chan5 dma0chan1 dma0chan14 dma0chan19 dma0chan23 dma0chan28 dma0chan4 dma0chan9 dma1chan4 dma2chan1 dma2chan6 dma0chan10 dma0chan15 dma0chan2 dma0chan24 dma0chan29 dma0chan5 dma1chan0 dma1chan5 dma2chan2 dma2chan7 dma0chan11 dma0chan16 dma0chan20 dma0chan25 dma0chan3 dma0chan6 dma1chan1 dma1chan6 dma2chan3 dma0chan12 dma0chan17 dma0chan21 dma0chan26 dma0chan30 dma0chan7 dma1chan2 dma1chan7 dma2chan4
Each channel is expanded as follows:
Board $> ls -la /sys/class/dma/dma0chan0/ total 0 drwxr-xr-x 3 root root 0 Jun 7 21:22 . drwxr-xr-x 34 root root 0 Jun 7 21:22 .. -r--r--r-- 1 root root 4096 Jun 9 13:11 bytes_transferred lrwxrwxrwx 1 root root 0 Jun 9 13:11 device -> ../../../58000000.dma -r--r--r-- 1 root root 4096 Jun 9 13:11 in_use -r--r--r-- 1 root root 4096 Jun 9 13:11 memcpy_count drwxr-xr-x 2 root root 0 Jun 9 13:11 power lrwxrwxrwx 1 root root 0 Jun 9 13:11 subsystem -> ../../../../../../class/dma -rw-r--r-- 1 root root 4096 Jun 7 21:22 uevent
device indicates which DMA driver manages the channel.
echoing in_use indicates whether the channel has been allocated or not.
Board $> cat /sys/class/dma/dma0chan0/in_use 1
4.2.2. Debugfs[edit source]
debugfs entries are available. They are documented in Part III - Debug drivers use of the DMA-API[4].
4.2.3. dmatest[edit source]
dmatest can be used to validate or debug DMA engine and driver without using client devices. This module is more a test than a debug module. It performs a memory-to-memory copy using standard DMA engine API.
For details on how to use this kernel module, refer to [6].
5. Source code location[edit source]
DMA: drivers/dma/stm32-dma.c
MDMA: drivers/dma/stm32-mdma.c
DMAMUX: drivers/dma/stm32-dmamux.c
DMA engine:
- Engine: drivers/dma/dmaengine.c
- Virtual channel support: drivers/dma/virt-dma.c
6. To go further[edit source]
Very useful documentation can be found at DMAEngine documentation
7. References[edit source]
- ↑ 1.0 1.1 DMA provider
- ↑ DMA API
- ↑ DMA Engine API Guide
- ↑ 4.0 4.1 core-api/dma-api.html Dynamic DMA mapping using the generic device Cite error: Invalid
<ref>
tag; name "Documentation API" defined multiple times with different content - ↑ core-api/dma-api-howto.html Dynamic DMA mapping Guide
- ↑ driver-api/dmaengine/dmatest.html