X-NUCLEO-NFC05A1 expansion board

Revision as of 16:43, 12 December 2019 by Registered User

1. Article Purpose[edit source]

The purpose of this article is to explain how to integrate the NFC05A1 expansion board with STM32MP157C-DK2, Software will run on Linux on Cortex®-A7. NFC05A1 board is a NFC card reader expansion board based on ST25R3911B for STM32 and STM8 Nucleos.

2. Prerequisites[edit source]

All the dependencies as per the LINK:Getting_started/STM32MP1_boards/STM32MP157C-DK2 should be installed

  • SDK must be installed and also enabled. [[1]]
  • Starter Package must be flashed onto SD-Card and board should boot up successfully.


2.1. Hardware Prerequisites[edit source]

  • STM32MP157C-DK2 Discovery Kit
  • X-NUCLEO-NFC05A1
  • 8 GB micro SD card to boot the STM32MP157C-DK2
  • SD card reader OR LAN connectivity
STM32MP157C-DK2

For more information about the STM32 discovery board and how to start it up, jump to this section Getting_started/STM32MP1_boards/STM32MP157C-DK2

  • NFC05A1 expansion board
File:X-nucleo-nfc05a1.jpg
X_NUCLEO-NFC05A1 board


2.2. Software prerequisites[edit source]

  • Linux PC with Ubuntu 16.04 LTS installed
  • The STM32MP157C-DK2 board must be downloaded with appropriate software in order to support NFC05A1 expansion board. For proceeding, follow the step-by-step instructions provided at STM32MP157C-DK2 Let's start.


3. Hardware setup - connections explained[edit source]

The X-NUCLEO-NFC005A1 is docked on to the Arduino connector present on the bottom side of the STM32MP157C-DK2 board as shown in below figure -

File:NFC05A1 and STM32MP157C-DK2 connection.png
Location of Arduino Connectors on both boards
File:NFC05A1 and STM32MP157C-DK2 dock.png
NFC05A1 docks over STM32MP157C-DK2


4. Software setup, build and run[edit source]

4.1. Booting STM32MP157C-DK2 with Starter Package[edit source]

Please refer to section Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let's_start/Populate_the_target_and_boot_the_image to know instructions for Booting the board using Starter Package.

4.2. Software platform configuration for running the application[edit source]

Before running the application, platform configuration needs to be updated. User need to download Developer Package and update device tree for enabling the relevant peripherals. For quick evaluation of the software user can refer to section 3.2.1 and use the pre-built images and easily have the application running on discovery kit. In case the user wants a full-fledged development environment, detailed description of how to modify the device tree and build updated kernel images is mentioned in section 3.2.2

Note: In this document, we will access the Discovery Kit from host PC via TCP/IP network (using ssh and scp commands). Another method to access the board could be through serial link (UART / USB) using tools such as ‘minicom’ (on Linux PC) or ‘Tera-term’ (on Windows PC). . Section 4 explains how to transfer file using Tera-Term . For more details, please refer to wiki page: How to get Terminal.

4.2.1. Steps for quick evaluation of software[edit source]

In order to speed-up the development process and quickly evaluate the software, please follow below mentioned steps–

  • Please follow intsructions in the link : STM32MP157C-DK2 Let's start. to flash the Starter Package on the SD Card.
  • Boot the board with Starter Package.
  • Connect Ethernet LAN cable to CN8 of discovery kit. If LAN is not available, please see page 'How to transfer files using ‘Tera Term’: Windows PC to Discovery Kit '.
  • Connect a USB Keyboard to the discovery kit.
  • Open terminal and get the IP address of the board using below command on board
Board $> ifconfig | more
  • Download pre-built images - [[2]]
  • Use below commands to copy the boot images, device tree blobs & lib modules on to the board and re-initialize the board –
PC $> unzip install_artifact.zip
PC $> cd install_artifact
PC $> scp ./boot/* root@<ip address of board>:/boot/
PC $> scp –r ./lib/modules root@<ip address of board>:/lib/modules/
PC $> ssh root@<ip address of board>
Board $> /sbin/depmod –a  
Board $> sync
Board $> reboot

Note: Incase network connectivity is not available, please refer to section: 'How to transfer files using ‘Tera Term’: Windows PC to Discovery Kit' for doing file transfer locally.

  • After the board boots up, copy the application binary and the shared lib to discovery board –
PC $> unzip install_artifact.zip
PC $> cd install_artifact
PC $> scp nfcPoller_st25r3911 root@<ip address of board>:/usr/local
PC $> ssh root@<ip address of board>
Board $> cd /usr/local
Board $> export LD_LIBRARY_PATH=/usr/local/:$LD_LIBRARY_PATH
Board $> chmod +x nfc_poller_st25r3911
Board $> ./nfc_poller_st25r3911

The application will start running once the above mentioned commands are executed. Below picture shows the application running on the discovery board.

4.2.2. Updating platform configuration in developer package[edit source]

In order to set up the development platform, please follow below mentioned steps –

PC $> cd stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0 
PC $> tar xvf linux-4.19.9.tar.xz
  • Apply the ST patches
PC $> cd linux-4.19.9
PC $> for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
  • Apply fragments
PC $> cd linux-4.19.9
PC $> mkdir -p ../build
PC $> make ARCH=arm O="$PWD/../build" multi_v7_defconfig fragment*.config
PC $> scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config ../fragment-03-systemd.config
PC $> scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config ../fragment-04-optee.config
PC $> scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config ../fragment-05-modules.config
PC $> yes  | make oldconfig

Note: Commands mentioned in this document are intended to compile the kernel in a separate directory (named ‘build’). Please refer to Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm®_Cortex®-A7/Modify,_rebuild_and_reload_the_Linux®_kernel for more details

  • Open the device tree file ‘arch/arm/boot/dts/stm32mp157c-dk2.dts’ and add below code snippet to the file.
&pinctrl{
	spi4_pins_a: spi4-0 {
			pins1 {
				pinmux = <STM32_PINMUX('E', 12, AF5)>, /* SPI4_SCK */
				<STM32_PINMUX('E', 14, AF5)>; /* SPI4_MOSI */
				bias-disable;
				drive-push-pull;
				slew-rate = <1>;
			};

			pins2 {
				pinmux = <STM32_PINMUX('E', 13, AF5)>; /* SPI4_MISO */
				bias-disable;
			};
	};
	spi4_sleep_pins_a: spi4-sleep-0 {
			pins {
				pinmux = <STM32_PINMUX('E', 12, ANALOG)>, /* SPI4_SCK */
				<STM32_PINMUX('E', 13, ANALOG)>, /* SPI4_MISO */
				<STM32_PINMUX('E', 14, ANALOG)>; /* SPI4_MOSI */
			};
	};
};
&spi4 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi4_pins_a>;
	pinctrl-1 = <&spi4_sleep_pins_a>;
	/*status = "disabled";*/
	cs-gpios = <&gpioe 11 0>;
	status = "okay";

	spidev@0x00 {
		compatible = "semtech,sx1301";
		spi-max-frequency = <5000000>;		
		reg = <0>;
	};
};
  • Build the Linux® kernel source and copy the updated images onto the discovery kit. Please refer to section 4 of this wiki page :: “Build the Linux® kernel source code for the first time”.

4.2.3. Build the RFAL Linux application code[edit source]

The user needs to have SDK installed on the Linux machine to compile the application code for STM32MP157. The below steps need to be followed to build the application -

  • Download and install the SDK. Please refer wiki page link for details. This should already be in place if you executed step #1 of section 3.2.2
  • SET the cross compiler(SDK) environment: If default folder structure is used then below command should work –
PC $> source $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
  • Download the application from the link: [[3]]
  • Extract the RFAL_st25r3911_v2.0.10.zip package
 unzip Linux_RFAL_st25r3911_v2.1.0.zip
 sudo apt-get install cmake
 cd Linux_RFAL_st25r3911_v2.1.0/linux_demo/build
 rm –rf *
 cmake ..
 make
  • The above-mentioned commands would build following files –

The example application: "Linux_RFAL_st25r3911_v2.0.4/linux_demo/build/nfc_poller/nfc_poller_st25r3911" Shared lib : "Linux_RFAL_st25r3911_v2.0.4/linux_demo/build/rfal/st25r3911/librfal_st25r3911.so"

4.2.4. RUN the RFAL Linux application on STM32MP157C-DK2[edit source]

Copy generated binaries onto the Discovery Kit using below commands

 scp Linux_RFAL_st25r3911_v2.0.10/linux_demo/build/nfc_poller/nfc_poller_st25r3911 root@<board ip address>:/usr/local
 scp Linux_RFAL_st25r3911_v2.0.10/linux_demo/build/rfal/st25r3911/librfal_st25r3911.so root@<board ip address>:/usr/local

Open terminal on the Discovery Kit board or use ssh login and run the application using below commands.

 ssh root@<board ip address>

Export the shared lib to the environment

 export LD_LIBRARY_PATH=/usr/local:$LD_LIBRARY_PATH 

Enter the directory where binaries were copied

 cd /usr/local 

RUN the application

 ./nfc_poller_st25r3911

The user will see the below message on the screen:

“Welcome to the ST25R3911B NFC Poller Demo on Linux. 
Scanning for NFC Technologies ...........”


When a NFC tag is brought near the reader antenna, the communication takes place between the tag and reader and the UID is displayed on the screen. Snapshot below [ upload snapshot pic]