Template:ArticleFirstDraftVersion
1. Article purpose[edit source]
This article provides basic information to start using the Linux tool: sysdig[1].
2. Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||||
---|---|---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package | ||
sysdig | Monitoring tools | sysdig[1] is a tool for system troubleshooting, analysis and exploration. It can be used to capture, filter and decode system calls and other OS events. | ![]() |
![]() |
![]() |
|
sysdig can be both used to inspect live systems or to generate trace files that can be analyzed at a later stage.
It includes a powerul filtering language, has customizable output, and can be extended through Lua scripts, called chisels.
sysdig aims to replace a collection of tools, as lsof, strace, iostat, ps, etc...
3. Installing the trace and debug tool on your target board[edit source]
sysdig is a user space application which is not part of the standard STM32MPU Embedded Software distribution image and Packages. It has to be integrated as an external component.
Linux kernel configuration must also enable CONFIG_TRACEPOINTS and CONFIG_HAVE_SYSCALL_TRACEPOINTS:
Symbol: TRACEPOINTS [=y] Selected by: TRACING [=y] || BLK_DEV_IO_TRACE [=n] && TRACING_SUPPORT [=y] && FTRACE [=y] && SYSFS [=y] && BLOCK [=y] Symbol: HAVE_SYSCALL_TRACEPOINTS [=y] Selected by: ARM [=y]
3.1. Using STM32MPU Embedded Software distribution[edit source]
On STM32MPU Embedded Software distribution(weston), Linux kernel configuration already enable the required configuration options.
3.1.1. Developer Package[edit source]
There are too many dependencies for building sysdig application and kernel driver, that's the reason why this is recommended to use the Distribution package to integrate this tool.
3.1.2. Distribution Package[edit source]
Yocto recipes for building sysdig are part of the OpenSTLinux distribution.
Following steps to be done to enable sysdig and add it to the st-image-weston image:
- Add sysdig package install for the image
echo 'IMAGE_INSTALL_append += "sysdig"' >> layer/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend echo 'IMAGE_INSTALL_append += "sysdig-driver"' >> layer/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend
- Regenerate the image file:
bitbake st-image-weston
- Update your board with the new image. See Flashing the built image.
3.2. Using STM32MPU Embedded Software distribution for Android™[edit source]
![]() |
Coming soon |
4. Getting started[edit source]
Below some basics commands extracted from official sysdig website[1]:
5. To go further[edit source]
![]() |
Coming soon |
6. References[edit source]
Document link | Document Type | Description |
---|---|---|
sysdig manpage | Standard | Man page from Official github |
sysdig wiki documentation | User Guide | Documentation from Official github |