How to use TTY with User Terminal

Revision as of 15:11, 19 February 2019 by Registered User

Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Purpose[edit source]

This article describes how to use TTY with a user terminal. The TTY overview is described in Serial TTY overview article.

The use case of the following examples is a data transfer between a STM32 MPU board and PC, over a USB to a RS232 adapter cable.
The setup of this use case is described in details in the How to get Terminal article.


For the following examples:

  • uart4 is activated by default (for the Linux console)
  • usart3 is enabled by device tree
  • The usart3 pins are connected to a RS232 card
  • The RS232 card is connected to the PC over the USB to RS232 adapter cable.

Note: Some TTY tools are used in this article. A list of TTY tools is defined a dedicated article [TTY Tools ].

2. Print the file name of the terminal connected to standard input (with tty tool)[edit source]

 tty
/* The console is connected to uart4 (aka ttySTM0) */
/dev/ttySTM0

3. Change serial port configuration (with stty tool)[edit source]

Many serial port properties can be displayed and changed with the stty tool. The full feature list is available in stty user manual pages [1] .

 stty --help
  • Display the current configuration:
 stty -a -F /dev/ttySTM1
/* Display the configuration of uart3 (aka ttySTM1) */
speed 115200 baud; rows 45; columns 169; line = 0;
  • Display only the current baud rate:
 stty -F /dev/ttySTM1 speed
/* uart3 (aka ttySTM1) baud rate is set to 115200 bps */
115200
  • Change the baud rate:

stty -F /dev/ttySTMx EXPECTED_BAUDRATE

Example: change the baud rate to 19200

/* Change uart3 (aka ttySTM1) baud rate to 19200 bps */
 stty -F /dev/ttySTM1 19200

The stty tool proposes many arguments allowing many operations on a tty terminal, such as:

  • special settings (various arguments such as speed, line discipline, minimum number of characters for a completed read, size, timeout, etc...)
  • control settings
  • input settings
  • output settings
  • local settings
  • combination settings


Note: If you want to go further, an interesting tutorial describes termios and stty [2].

4. Send / Receive data (with stty, minicom, echo and cat tools)[edit source]

4.1. Default configuration (8 data bits frame, no parity errors detection, no framing errors detection)[edit source]

Sending data can be simply done by opening the device as a file and writing data to it.

  • Configure a port on ttySTM1 (aka usart3)
 stty -F /dev/ttySTM1 115200 -echo
  • Display the current configuration on ttySTM1 (usart3):
/* display the configuration of uart3 (aka ttySTM1) */
 stty -a -F /dev/ttySTM1
speed 115200 baud; rows 45; columns 169; line = 0;
  • Open a port on ttySTM1 (usart3) to receive data
 cat /dev/ttySTM1 &
  • On the remote PC, identify the tty terminal associated to RS232 card connected on STM32MPU USART3 pins
/* Command to execute from host terminal */
 ls /dev/ttyUSB*

/dev/ttyUSB0

  • Open a minicom in a second terminal on the remote device connected on USART3 pins
 minicom -D /dev/ttyUSB0
  • Display the current configuration on ttyUSB0 (remote device):
/* Display the configuration of host uart (aka ttyUSB0) */
 stty -a -F /dev/ttyUSB0
speed 115200 baud; rows 45; columns 169; line = 0;
  • Send data from remote PC to STM32MPU over USART3 with default termios configuration (8 frames length, no parity)
/* Execute this command from host terminal */
 echo "HELLO" > /dev/ttyUSB0
  • send data from STM32MPU to remote PC over USART3 with default termios configuration (8 frames length, no parity)
/* Execute this command from STM32 terminal */
 echo "HELLO" > /dev/ttySTM1

4.2. Parity errors detection[edit source]

Some additional termios funtions allow to enable parity errors detection:

  • parenb: Parity enable.
  • parodd: Odd parity else even.
  • inpck: Enable input parity check.


Exemples:

  • Configure a port on ttySTM1 (usart3) with even parity enabling
/* STM32 parity enabling */
 stty -F /dev/ttySTM1 115200 -echo parenb -parodd inpck
  • Open a port on ttySTM1 (usart3) to receive data
 cat /dev/ttySTM1 &
Open a minicom in a second terminal on the remote device connected on USART3 pins
 minicom -D /dev/ttyUSB0
  • Configure a port on ttyUSB0 (remote device) with even parity enabling:
/* Remote device parity enabling */
 stty -a -F /dev/ttyUSB0 115200 -echo parenb -parodd inpck
speed 115200 baud; rows 45; columns 169; line = 0;
  • Send data from remote PC to STM32MPU over USART3 with default termios configuration (8 frames length, no parity)
/* Execute this command from host terminal */
 echo "HELLO" > /dev/ttyUSB0
  • send data from STM32MPU to remote PC over USART3 with default termios configuration (8 frames length, no parity)
/*  Execute this command from STM32 terminal */
 echo "HELLO" > /dev/ttySTM1


4.3. Framing errors detection[edit source]

Some additional termios funtions allow to enable framing errors detection:

  • csize: Number of bits per byte (CS5, CS6, CS7, or CS8).
  • inpck: Enable input framing check.


Exemples:

  • Configure a port on ttySTM1 (usart3) with framing check enabling and 7 data bits length frames
/* STM32 framing enabling */
 stty -F /dev/ttySTM1 115200 -echo cs7 inpck
  • Open a port on ttySTM1 (usart3) to receive data
 cat /dev/ttySTM1 &
Open a minicom in a second terminal on the remote device connected on USART3 pins
 minicom -D /dev/ttyUSB0
  • Configure a port on ttyUSB0 (remote device) with framing check enabling and 7 data bits length frames
/* Remote device parity enabling */
 stty -a -F /dev/ttyUSB0 115200 -echo cs7 inpck
speed 115200 baud; rows 45; columns 169; line = 0;
  • Send data from remote PC to STM32MPU over USART3 with default termios configuration (8 frames length, no parity)
/* Execute this command from host terminal*/
 echo "HELLO" > /dev/ttyUSB0
  • send data from STM32MPU to remote PC over USART3 with default termios configuration (8 frames length, no parity)
/* Execute this command from STM32 terminal */
 echo "HELLO" > /dev/ttySTM1

5. Identify processes using a tty serial device (with fuser tool)[edit source]

 fuser /dev/ttySTM0
/* The process numbered 395, 691 and 3872 are using a tty serial device*/
395 691 3872

6. Link a tty serial device with a line discipline (with ldattach tool)[edit source]

Attach ttySTM1 with line discipline number n :

 ldattach n /dev/ttySTM1

7. File transfer over serial console[edit source]

Please see the dedicated article How to transfer a file over serial console.

8. References[edit source]