Last edited 2 years ago

MB1263

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


1. Board overview[edit source]

Daughterboard MB1263 (STM32MP157C 18x18 with PMIC and DDR3), revision C: part of the STM32MP157C-EV1 Evaluation board

Template:ImageMap

Details of some LEDs:

  • LD1: green if power connection established
  • LD6: red flashing if ST-LINK/V2-1 connection not established, else green
  • LD2, LD3, LD4, LD5: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the LEDs and buttons on STM32 MPU boards article

Template:ImageMap

2. Links[edit source]

MB1263 schematics